This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Edge AI : Int8 Compilied model is taking more time on the EVM during inference

Part Number: TDA4VM

Tool/software:

Hello Champs , 

I am having a custom model which i am able to complie and run it on the TDA4 EVM board but the issue with the timings ie the performance , the inference is taking Sum of Layer Cycles 67089796 for  a 1 single input data below are the details and the model 

Settings 

Edgeai : 9.27 / 10.07

Tensor Bits : int8 

Can you please let us knw if there are any solution to reduce the timing taken to run by the model modified_modified_dd3d_fnc_4cam_vtow_ped_v5_pruned.zip