This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6747: Calculating T_RAS_MAX

Part Number: TMS320C6747


Tool/software:

I have a SDRAM on the EMIFB and the refresh rate is 16 ms and 4096 rows.

The tRAS_MAx is 120k ns, and I viewing Table 19-22 in document SPRUH91D–March 2013–Revised September 2016

The formula for T_RAS_MAX for EMIFB.SDTIM2 bits 30-27 (4 bits wide) is:

T_RAS_MAX = (tRAS_Max / SDRAM refresh rate) -1

I'm using 16ms/4096 for the SDRAM refresh rate = 3.90625 us. 

T_RAS_MAX = (120 us / 3.90625 us ) -1 = 29.72  a number too big for the 4 bit field.

Any suggestions?

Thank you, Tony