Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi Team,
Yocto-SDK: "09_01_00"
MCU-SDK: "mcu_plus_sdk_am62ax_09_02_00_38"
EVM: SK-AM62A-LP
Questions related HW-Watchdog in MCU-R5.
1) Does MCU-R5 support the HW watchdog ?
2) how do we configure the HW-Watchdog in the MCU-R5 fw using SysConfig and FreeRTOS APIs ?
3) Is there any sample example available to use the HW-Watchdog in MCU-R5 and test ?
Note: We are running applications on the MCU-R5 core, along with Linux running on the A-53 core.
Link:- software-dl.ti.com/.../DRIVERS_WATCHDOG_PAGE.html
Thanks,
Nisarg