Tool/software:
I am using TMS320VC5507PGE.
I am using it with CVDD = 1.62 V (196.608 MHz).
16.384MHz is multiplied by 12 inside the DSP to get 196.608MHz.
(1) What is the allowable ripple for CVDD?
The following is stated for USBPLLVDD. Please provide a similar value for CVDD.
[†USB PLL is susceptible to power supply ripple. The maximum allowable supply ripple is 1% for 1 Hz to 5 kHz; 1.5% for 5 kHz to 10 MHz; 3% for 10 MHz to 100 MHz, and less than 5% for 100 MHz or greater.]
(2) Is it okay to use 1.60V for CVDD when using 196.608MHz?
Since it is 1.60V at 200MHz, would it be 1.58V at 196.608MHz?
(3) Based on a. through d. below, can we understand it as follows?
"When the noise level (or ripple level) exceeds CVDD±3%V, the DPLL inside the DSP malfunctions, and the multiplication frequency fluctuates. If it is within the range of CVDD±3%, it will not malfunction.
If it is within CVDD±3%, the noise frequency, impulse noise, and other noise shapes are not relevant.
This noise (ripple) tolerance changes depending on the DSP temperature and DSP pressure.
Noise (ripple) tolerance differs between individual DSPs."
=========================================================
When the 1.6V power supply noise is large,
a. The multiplied frequency of 196.608MHz drops by about -0.2%.
b. It is temperature dependent, and this phenomenon occurs when the DSP surface temperature is around 32.5°C.
c. This phenomenon also occurs when pressing or bending the DSP.
d. Even with the same noise level, there are some DSPs for which the phenomenon occurs and some for which it does not.
========================================================
Please answer questions (1) to (3) above.
Thank you in advance.