Other Parts Discussed in Thread: TMS320DM365
Hi All:
I have some questions about the Face Detection on DM365:
1. Does the FD only support the input YUV420SP with resolution 320x192, or any resolution which less than 320x240??
2. How about the FD(Don't include Face Recognize) performance? From the debug message, seems it cost about 200 milliseconds, but from the spec, we can find "It takes 15 milli sec to detect multiple faces of size of 20x20 in a 320x192 input image", which one is correct??
Now I have tried the open the FD in AV_SERVER, but it can't detect any face, any comments?
Thanks.