Hi guys!!
I am using the DSPLINK package (version 1.65) in order to communicate ARM & DSP in the beagleboard platform and CCSv5.1 like IDE (OS Linux). I am building the executables for DSP with the makefile provided for DSPLINK. I want to modify some includes of the project, but I do not know where I have to make it (CCS? ,makefile structure? dsplinkcfg written in perl). I have already built the dsplink module and I have modified the files of configuration of DSP (c64xxp_5.xx_linux.mk).
For instance, I have a builded project in CCSv5.1 with some defines and includes that I can see in the console of CCS. Where and how can I add more options? Options like more paths, more defines, whatever...One solution could be modifing perl file or modifing some parameter of some makefile structure of dsplink? Any suggestions?? Thanks in advance.
Regards
Óscar