Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TS3A27518E-Q1
Tool/software:
Debugging Diagnostics Traces
Hello team
I would like to know if the MUX MODE [4] can be changed "on the fly" or Jacinto would need to be flashed
here is the scenario
let say that for a "Instrumented" ECU I'll use Traces from TRC_DATA0 to TRC_DATA03 for debugging
after debugging / diagnostic the port used previously as Trace will be used as CAN signal, to switch signal I'm using a TS3A27518E-Q1 the COMM pin is connected to Jacinto NO and NC will switch between signals
To talk about a specific example:
Ball number Port
AF33 for debugging diagnostics it needs to be assigned as MUX Mode [4] = 10 TRC Data1
after that
AF33 port will be assigned as Mux Mode [4] = 0 MCAN13_TX
the question is:
Can it be done on the fly or 2 DTSI files should be created then the specific file should be flashed ??
regards