This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62B-P1: HUK Trusted Keys

Part Number: SK-AM62B-P1


Tool/software:

I'm trying to setup automatic partition encryption/decryption using OPTEE trusted keys, but I have been unsuccessful at enabling this feature.

The following command I am trying fails:

root@v1:~$ keyctl add trusted kmk "new 32" @s
add_key: No such device

I'm building from Yocto Scarthgap and have verified the version of ti-fs-firmware-am62x-hs-enc.bin used is 10.01.00.10 (according to git log the commit pulled is 1eaf07dc).

All testing is done on an SK-AM62B-P1 devboard that has been configured as HS-SE.

The keyutil package has been added to my Yocto recipe to enable using keyctl.

The TRUSTED_KEYS, TPM-based trusted keys, and TEE-based trusted keys have been configured in menuconfig.

I've verified the menuconfig has propagated into the kernel by dumping the running /proc/config.gz and I verified I see:

CONFIG_TRUSTED_KEYS=y
CONFIG_TRUSTED_KEYS_TPM=y
CONFIG_TRUSTED_KEYS_TEE=y

I also tried building these as modules and installing them using "modprobe trustedkeys" but the keyctl command still failed.

Any ideas on what to further investigate are greatly appreciated!

Thanks,