This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

"nand_bbt: ECC error while reading bad block table" when Kernel loads



The following is a brief on Configuration used:

Processor : DM365

U-Boot (April 2010 release)  (Configuration : davinci_dm365_ipnc_config)

Linux Kernel version: 2.6.18

 

"nand_bbt: ECC error while reading bad block table" started coming when the Flash Size was increased from 32M to 64M

On 32M flash this error was never seen. Any help on this would be appreciated.

Thanks in Advance...