Other Parts Discussed in Thread: ADS1158
Hi
I'm not sure if this is really a boot issue, but since it only occurs during boot I hope it gives one of the gurus here a clue:
I have a custom C6742 board which uses SPI1 and UART0. I have a test application that flashes some leds, and this application works fine both when I run it from the debugger and when I program it into the flash chip and boot from SPI1 flash.
I have the real application that collects samples from an ADC on SPI1 and sends processed data out over UART0. This application works fine if I run it from the debugger. However, when I boot this program from the flash chip, it does collect data from the ADC, but will not transmit over UART0. Strange thing is, if I connect the debugger and restart the processor (without changing any settings), it does transmit over UART0.
Both the test application and the real application run from mDDR2 memory.
My AISgen configuration file is here:
Boot Mode=SPI1 Flash Boot Speed=5 Flash Width=0 Flash Timing=3ffffffc Configure Peripheral=True Configure PLL0=True Configure SDRAM=False Configure PLL1=True Configure DDR2=True Configure LPSC=True Configure Pinmux=False Enable CRC=False Specify Entrypoint=False Enable Sequential Read=False Use 4.5 Clock Divider=False Use DDR2 Direct Clock=False Use mDDR=True ROM ID=2 Device Type=1 Input Clock Speed=24 Clock Type=0 PLL0 Pre Divider=1 PLL0 Multiplier=25 PLL0 Post Divider=3 PLL0 Div1=1 PLL0 Div3=2 PLL0 Div7=6 PLL1 Multiplier=25 PLL1 Post Divider=4 PLL1 Div1=1 PLL1 Div2=2 PLL1 Div3=3 Entrypoint=c0000000 SDRAM SDBCR=0 SDRAM SDTMR=0 SDRAM SDRSRPDEXIT=0 SDRAM SDRCR=0 DDR2 PHY=84 DDR2 SDCR=134621 DDR2 SDCR2=0 DDR2 SDTIMR=16923209 DDR2 SDTIMR2=3d0cc722 DDR2 SDRCR=492 LPSC0 Enable=3+4+5+6+9+10+11+12+ LPSC0 Disable= LPSC0 SyncRst= LPSC1 Enable=1+2+3+4+5+7+9+10+11+12+13+14+15+16+17+18+19+ LPSC1 Disable= LPSC1 SyncRst= Pinmux=0:44000000+4:11441100+5:111111+8:88800+10:8000000+14:8+18:800+19:88800+ App File String=U:\Projects\PJ0095_-_Metatronics_-_Motion9\FLled\Debug\FLled.out AIS File Name=U:\Projects\PJ0095_-_Metatronics_-_Motion9\FLled\Debug\FLled4.bin
Does anyone have a clue what could be going on here? Is it perhaps a timing issue?
And any ideas how to solve it? Should I (re-)enable UART0 in software? How?
Best regards
Admar