When configuring shared memory regions on a 6472, do all of the meta entries on each core need to be the same? For example, do all the cores need to have the cache enable set the same? or can only the core which have cache turned on set the share mem region cashe enable to true, and the others to false?
Thanks