This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BUG in local_bh_enable at kernel/softirq.c

hi

i am trying to do the setup for DM365IPNC by APPRO using ipnc2.6.0

i am following the steps given in Users_Guide_IPNC_DM365_.pdf. and i met some problem while starting the DM365 ipnc from appro, could you help me ?

i just coppied the message from console.

----------------------------------------------

U-Boot 1.3.4 (Dec  9 2010 - 17:45:52) DM365-IPNC-1.0.1                                                                                                                           
                                                                                                                                                                                 
I2C:   ready                                                                                                                                                                     
DRAM:  128 MB                                                                                                                                                                    
NAND:  NAND device: Manufacturer ID: 0xec, Chip ID: 0x75 (Samsung NAND 32MiB 3,3V 8-bit)                                                                                         
Bad block table found at page 65504, version 0x00                                                                                                                                
Bad block table found at page 65472, version 0x00                                                                                                                                
32 MiB                                                                                                                                                                           
In:    serial                                                                                                                                                                    
Out:   serial                                                                                                                                                                    
Err:   serial                                                                                                                                                                    
ARM Clock :- 297MHz                                                                                                                                                              
DDR Clock :- 270MHz                                                                                                                                                              
Ethernet PHY: GENERIC @ 0x01                                                                                                                                                     
Hit any key to stop autoboot:  0                                                                                                                                                 
DM365 IPNC :>set bootcmd 'nand read 0x82000000 0x400000 0xe00000;nboot 0x80700000 0 0x200000;bootm 0x80700000'                                                                   
DM365 IPNC :>set bootargs 'mem=48M console=ttyS1,115200n8 root=/dev/ram0 rw initrd=0x82000000,14M ip=192.168.5.158:192.168.5.79:192.168.5.1:255.255.254.0:::off eth=00:11:22:33:4'
DM365 IPNC :>boot                                                                                                                                                                
                                                                                                                                                                                 
NAND read: device 0 offset 0x400000, size 0xe00000                                                                                                                               
 14680064 bytes read: OK                                                                                                                                                         
                                                                                                                                                                                 
Loading from NAND 32MiB 3,3V 8-bit, offset 0x200000                                                                                                                              
   Image Name:   Linux-2.6.18_pro500-davinci_IPNC                                                                                                                                
   Image Type:   ARM Linux Kernel Image (uncompressed)                                                                                                                           
   Data Size:    1809444 Bytes =  1.7 MB                                                                                                                                         
   Load Address: 80008000                                                                                                                                                        
   Entry Point:  80008000                                                                                                                                                        
## Booting kernel from Legacy Image at 80700000 ...                                                                                                                              
   Image Name:   Linux-2.6.18_pro500-davinci_IPNC                                                                                                                                
   Image Type:   ARM Linux Kernel Image (uncompressed)                                                                                                                           
   Data Size:    1809444 Bytes =  1.7 MB                                                                                                                                         
   Load Address: 80008000                                                                                                                                                        
   Entry Point:  80008000                                                                                                                                                        
   Verifying Checksum ... OK                                                                                                                                                     
   Loading Kernel Image ... OK                                                                                                                                                   
OK                                                                                                                                                                               
                                                                                                                                                                                 
Starting kernel ...                                                                                                                                                              
                                                                                                                                                                                 
Linux version 2.6.18_pro500-davinci_IPNC_DM365_2.6.0 (root@rockingblue-G41MT-S2) (gcc 版本 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Fri Nov 11 16:38:52   1
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177                                                                                                                    
Machine: DaVinci DM365 IPNC                                                                                                                                                      
Memory policy: ECC disabled, Data cache writeback                                                                                                                                
DaVinci DM0365 variant 0x8                                                                                                                                                       
PLL0: fixedrate: 24000000, commonrate: 135000000, vpssrate: 270000000                                                                                                            
PLL0: vencrate_sd: 27000000, ddrrate: 270000000 mmcsdrate: 49090909                                                                                                              
PLL1: armrate: 297000000, voicerate: 118800000, vencrate_hd: 74250000                                                                                                            
CPU0: D VIVT write-back cache                                                                                                                                                    
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets                                                                                                             
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets                                                                                                               
Built 1 zonelists.  Total pages: 12288                                                                                                                                           
Kernel command line: mem=48M console=ttyS1,115200n8 root=/dev/ram0 rw initrd=0x82000000,14M ip=192.168.5.158:192.168.5.79:192.168.5.1:255.255.254.0:::off eth=00:11:22:33:46:01  
PID hash table entries: 256 (order: 8, 1024 bytes)                                                                                                                               
Clock event device timer0_0 configured with caps set: 07                                                                                                                         
Console: colour dummy device 80x30                                                                                                                                               
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)                                                                                                                    
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)                                                                                                                     
Memory: 48MB = 48MB total                                                                                                                                                        
Memory: 30360KB available (3101K code, 643K data, 176K init)                                                                                                                     
Security Framework v1.0.0 initialized                                                                                                                                            
Capability LSM initialized                                                                                                                                                       
Mount-cache hash table entries: 512                                                                                                                                              
CPU: Testing write buffer coherency: ok                                                                                                                                          
checking if image is initramfs...it isn't (bad gzip magic numbers); looks like an initrd                                                                                         
Freeing initrd memory: 14336K                                                                                                                                                    
NET: Registered protocol family 16                                                                                                                                               
DaVinci: 104 gpio irqs                                                                                                                                                           
MUX: initialized GPIO20                                                                                                                                                          
MUX: initialized I2C_SCL                                                                                                                                                         
Generic PHY: Registered new driver                                                                                                                                               
ch0 default output "COMPOSITE", mode "NTSC"                                                                                                                                      
VPBE Encoder Initialized                                                                                                                                                         
SCSI subsystem initialized                                                                                                                                                       
NET: Registered protocol family 2                                                                                                                                                
IP route cache hash table entries: 512 (order: -1, 2048 bytes)                                                                                                                   
TCP established hash table entries: 2048 (order: 1, 8192 bytes)                                                                                                                  
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)                                                                                                                         
TCP: Hash tables configured (established 2048 bind 1024)                                                                                                                         
TCP reno registered                                                                                                                                                              
VFS: Disk quotas dquot_6.5.1                                                                                                                                                     
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)                                                                                                                       
squashfs: version 3.1 (2006/08/19) Phillip Lougher                                                                                                                               
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.                                                                                                                            
yaffs Nov 11 2011 16:37:01 Installing.                                                                                                                                           
SGI XFS with no debug enabled                                                                                                                                                    
Initializing Cryptographic API                                                                                                                                                   
io scheduler noop registered                                                                                                                                                     
io scheduler anticipatory registered (default)                                                                                                                                   
LTT : ltt-facilities init                                                                                                                                                        
LTT : ltt-facility-core init in kernel                                                                                                                                           
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec                                                                                                                            
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled                                                                                                        
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A                                                                                                  
serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A                                                                                                  
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize                                                                                                            
Linux video capture interface: v2.00                                                                                                                                             
Trying to register davinci display video device.                                                                                                                                 
layer=c2dbba00,layer->video_dev=c2dbbb60                                                                                                                                         
Trying to register davinci display video device.                                                                                                                                 
layer=c2dbb800,layer->video_dev=c2dbb960                                                                                                                                         
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded                                                                                                                             
i2c /dev entries driver                                                                                                                                                          
nand_davinci nand_davinci.0: Using 4-bit hardware ECC                                                                                                                            
NAND device: Manufacturer ID: 0xec, Chip ID: 0x75 (Samsung NAND 32MiB 3,3V 8-bit)                                                                                                
Creating 5 MTD partitions on "nand_davinci.0":                                                                                                                                   
0x00000000-0x00080000 : "bootloader"                                                                                                                                             
0x00080000-0x00200000 : "params"                                                                                                                                                 
0x00200000-0x00400000 : "kernel"                                                                                                                                                 
0x00400000-0x01c00000 : "filesystem1"                                                                                                                                            
0x01c00000-0x02000000 : "filesystem2"                                                                                                                                            
nand_davinci nand_davinci.0: hardware revision: 2.3                                                                                                                              
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: proc                                                                                                                            
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: dev (254:0)                                                                                                                     
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc core: registered rtc_davinci_dm365 as rtc0                                                                                            
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).                                                                                       
ASoC version 0.13.1                                                                                                                                                              
CQ0093 Voice Codec 0.1                                                                                                                                                           
asoc: cq93vc <-> davinci-vcif mapping ok                                                                                                                                         
ALSA device list:                                                                                                                                                                
  #0: On-chip voice codec (cq93vc)                                                                                                                                               
IPv4 over IPv4 tunneling driver                                                                                                                                                  
TCP bic registered                                                                                                                                                               
NET: Registered protocol family 1                                                                                                                                                
NET: Registered protocol family 17                                                                                                                                               
rtc_davinci_dm365 rtc_davinci_dm365.0: setting the system clock to 2011-11-16 07:31:26 (1321428686)                                                                              
Time: timer0_1 clocksource has been installed.                                                                                                                                   
Clock event device timer0_0 configured with caps set: 08                                                                                                                         
Switched to high resolution mode on CPU 0                                                                                                                                        
IP-Config: No network devices available.                                                                                                                                         
RAMDISK: cramfs filesystem found at block 0                                                                                                                                      
RAMDISK: Loading 13960KiB [1 disk] into ram disk... done.                                                                                                                        
VFS: Mounted root (cramfs filesystem) readonly.                                                                                                                                  
Freeing init memory: 176K                                                                                                                                                        
INIT: version 2.86 booting                                                                                                                                                       
0                                                                                                                                                                                
mkdir: Cannot create directory `/dev/.test': Read-only file system                                                                                                               
Starting the hotplug events dispatcher: udevd.                                                                                                                                   
Synthesizing the initial hotplug events...done.                                                                                                                                  
Waiting for /dev to be fully populated...done.                                                                                                                                   
0                                                                                                                                                                                
CSL: Module install successful, device major num = 253                                                                                                                           
CSL: Module version 0.10.00, built on Nov 11 2011 16:40:33                                                                                                                       
I2C: Module install successful, device major num = 252                                                                                                                           
DMA: Module install successful, device major num = 251                                                                                                                           
DRV: Module install successful                                                                                                                                                   
DRV: Module built on Nov 11 2011 16:40:35                                                                                                                                        
DRV: EDMACC.QUEPRI  = 00000777                                                                                                                                                   
DRV: SYSTEM.MSTPRI0 = 00440022                                                                                                                                                   
DRV: SYSTEM.MSTPRI1 = 00000244                                                                                                                                                   
DRV: ISP.BCR        = 00000002                                                                                                                                                   
DRV: SYSTEM.MISC    = 00000399                                                                                                                                                   
CMEMK module: built on Nov 11 2011 at 16:40:13                                                                                                                                   
  Reference Linux version 2.6.18                                                                                                                                                 
  File /home/appro/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c                                                                        
allocated heap buffer 0xc4000000 of size 0x5000000                                                                                                                               
CMEM Range Overlaps Kernel Physical - allowing overlap                                                                                                                           
CMEM phys_start (0x1000) overlaps kernel (0x80000000 -> 0x83000000)                                                                                                              
cmemk initialized                                                                                                                                                                
EDMAK module: built on Nov 11 2011 at 16:40:15                                                                                                                                   
  Reference Linux version 2.6.18                                                                                                                                                 
  File /home/appro/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/edma/src/module/edmak.c                                                                        
IRQK module: built on Nov 11 2011 at 16:40:16                                                                                                                                    
  Reference Linux version 2.6.18                                                                                                                                                 
  File /home/appro/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/irq/src/module/irqk.c                                                                          
irqk initialized                                                                                                                                                                 
Creat queue id:0                                                                                                                                                                 
queue id:0                                                                                                                                                                       
FileMngThread created                                                                                                                                                            
Creat queue id:32769                                                                                                                                                             
queue id:32769                                                                                                                                                                   
queue id:32769                                                                                                                                                                   
AlramThread created                                                                                                                                                              
Share memory init success                                                                                                                                                        
IPNC_DM365_2.6.0 (root@rockingblue-G41MT-S2) (gcc 版本 4.2.0                                                                                                                     
Creat queue id:65538                                                                                                                                                             
queue id:65538                                                                                                                                                                   
queue id:65538                                                                                                                                                                   
Creat queue id:98307                                                                                                                                                             
queue id:98307                                                                                                                                                                   
                                                                                                                                                                                 
CPU is DM365                                                                                                                                                                     
./av_server.out DM365 NTSC APPRO2A AEWB 720P H264 5000000 VBR AUTO MENUOFF &                                                                                                     
Check_device_version : DEVICE VER = 0 !!                                                                                                                                         
Starting mounting local filesystems: CPU CurrentStatus is = 0                                                                                                                    
mount none on /dev/shm type tmpfs (rw,size=5M)                                                                                                                                   
none on /var/run type tmpfs (rw)                                                                                                                                                 
none on /tmp type tmpfs (rw,sync)                                                                                                                                                
                                                                                                                                                                                 
AVSERVER UI: Initializing.                                                                                                                                                       
Setting up networking ...rm: unable to remove `/etc/network/run': Read-only file system                                                                                          
ApproDrvInit: 7                                                                                                                                                                  
Creat queue id:131076                                                                                                                                                            
queue id:131076                                                                                                                                                                  
                                                                                                                                                                                 
 CLK Hz,                                                                                                                                                                         
 ARM   Hz =  297000000                                                                                                                                                           
 DDR   Hz =  270000000                                                                                                                                                           
 VPSS  Hz =  270000000                                                                                                                                                           
 IMCOP Hz =  270000000                                                                                                                                                           
                                                                                                                                                                                 
 [OSA_FILE ] Reading file [/mnt/nand/IMG_Paramset.bin] ... ERROR                                                                                                                 
IMAGE TUNE: Paramset File is not available..... Setting DEFAULT parameter                                                                                                        
Starting hotplug subsystem:                                                                                                                                                      
   pci                                                                                                                                                                           
                                                                                                                                                                                 
CONFIGURING AVSERVER FOR DM365 .....                                                                                                                                             
queue id:65538                                                                                                                                                                   
SENSOR FPS VALUE = 30                                                                                                                                                            
   pci      [success]                                                                                                                                                            
DavinciDisplay DavinciDisplay.1: Before finishing with S_FMT:                                                                                                                    
layer.pix_fmt.bytesperline = 640,                                                                                                                                                
 layer.pix_fmt.width = 640,                                                                                                                                                      
 layer.pix_fmt.height = 480,                                                                                                                                                     
 layer.pix_fmt.sizeimage =460800                                                                                                                                                 
DavinciDisplay DavinciDisplay.1: pixfmt->width = 640,                                                                                                                            
 layer->layer_info.config.line_length= 640                                                                                                                                       
                                                                                                                                                                                 
                                                                                                                                                                                 
 FR : 0 users registered from exsiting face album                                                                                                                                
IPNC_DM365_2.6.0 (root@rockingblue-G41MT-S2) (gcc 版本 4.2.0                                                                                                                     
IPNC AUTO_IRIS = 1                                                                                                                                                               
   usb                                                                                                                                                                           
APPRO AEW TRIAL VERSION !!!                                                                                                                                                      
APPRO AEW DATE LINE 2011/12                                                                                                                                                      
   usb      [success]                                                                                                                                                            
   isapnp                                                                                                                                                                        
   isapnp   [success]                                                                                                                                                            
Simple mixer control 'PGA',0                                                                                                                                                     
  Capabilities: cvolume                                                                                                                                                          
  Capture channels: Mono                                                                                                                                                         
  Limits: Capture 0 - 3                                                                                                                                                          
  Mono: Capture 2 [67%]                                                                                                                                                          
Simple mixer control 'Mono DAC',0                                                                                                                                                
  Capabilities: pvolume pvolume-joined                                                                                                                                           
  Playback channels: Mono                                                                                                                                                        
  Limits: Playback 0 - 63                                                                                                                                                        
  Mono: Playback 47 [75%]                                                                                                                                                        
SystemInit success                                                                                                                                                               
Schedule manager init success                                                                                                                                                    
   ide                                                                                                                                                                           
   ide      [success]                                                                                                                                                            
   input                                                                                                                                                                         
   input    [success]                                                                                                                                                            
   scsi                                                                                                                                                                          
   scsi     [success]                                                                                                                                                            
done.                                                                                                                                                                            
Starting portmap daemon: portmap.                                                                                                                                                
Starting internet superserver: inetd.                                                                                                                                            
io scheduler deadline registered                                                                                                                                                 
io scheduler cfq registered                                                                                                                                                      
TI DaVinci EMAC: kernel boot params Ethernet address: 00:11:22:33:46:01                                                                                                          
 sbulla: unknown partition table                                                                                                                                                 
Installing knfsd (copyright (C) 1996 okir@monad.swb.de).                                                                                                                         
loop: loaded (max 8 devices)                                                                                                                                                     
tun: Universal TUN/TAP device driver, 1.6                                                                                                                                        
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>                                                                                                                           
CSLIP: code copyright 1989 Regents of the University of California                                                                                                               
netconsole: not configured, aborting                                                                                                                                             
PPP generic driver version 2.4.2                                                                                                                                                 
PPP Deflate Compression module registered                                                                                                                                        
Davinci EMAC MII Bus: probed                                                                                                                                                     
MAC address is 00:11:22:33:46:01                                                                                                                                                 
TI DaVinci EMAC Linux version updated 4.0                                                                                                                                        
davinci-mmc davinci-mmc.0: Supporting 4-bit mode                                                                                                                                 
davinci-mmc davinci-mmc.0: Using DMA mode                                                                                                                                        
usbcore: registered new driver usbfs                                                                                                                                             
usbcore: registered new driver hub                                                                                                                                               
musb_hdrc: version 6.0, cppi-dma, peripheral, debug=0                                                                                                                            
musb_hdrc musb_hdrc: No DMA interrupt line                                                                                                                                       
musb_hdrc: USB Peripheral mode controller at c38f8000 using DMA, IRQ 12                                                                                                          
Loading iSCSI transport class v1.1-646.<5>iscsi: registered transport (tcp)                                                                                                      
 sbulla: unknown partition table                                                                                                                                                 
mkdosfs 3.0.6 (04 Oct 2009)                                                                                                                                                      
unable to get drive geometry, using default 255/63                                                                                                                               
/dev/sbulla has 255 heads and 63 sectors per track,                                                                                                                              
logical sector size is 512,                                                                                                                                                      
using 0xf8 media descriptor, with 1024 sectors;                                                                                                                                  
file system has 2 12-bit FATs and 4 sectors per cluster.                                                                                                                         
FAT size is 1 sector, and provides 247 clusters.                                                                                                                                 
Root directory contains 512 slots.                                                                                                                                               
Volume ID is 6e067d05, no volume label.                                                                                                                                          
queue id:0                                                                                                                                                                       
umount: /mnt/mmc: not mounted                                                                                                                                                    
killall: dhcpcd: no process killed                                                                                                                                               
rm: cannot remove `/var/run/dhcpcd-eth0.pid': No such file or directory                                                                                                          
net_search_gateway:eth0, 4A8C0, 0, 1                                                                                                                                             
dns=192.168.5.1                                                                                                                                                                  
net_search_gateway:eth0, 4A8C0, 0, 1                                                                                                                                             
net_search_gateway:eth0, 0, 105A8C0, 3                                                                                                                                           
dns=192.168.5.1                                                                                                                                                                  
ERROR: Module g_file_storage does not exist in /proc/modules                                                                                                                     
g_file_storage gadget: File-backed Storage Gadget, version: 28 November 2005                                                                                                     
g_file_storage gadget: Number of LUNs=1                                                                                                                                          
g_file_storage gadget-lun0: ro=0, file: /dev/sbulla                                                                                                                              
system_server/512[CPU#0]: BUG in local_bh_enable at kernel/softirq.c:196                                                                                                         
ApproDrvInit: 9                                                                                                                                                                  
queue id:131076                                                                                                                                                                  
Initializing...                                                                                                                                                                  
...done initializing                                                                                                                                                             
ApproDrvInit: 8                                                                                                                                                                  
queue id:131076                                                                                                                                                                  
Initializing...                                                                                                                                                                  
...done initializing                                                                                                                                                             
ApproDrvInit: 6                                                                                                                                                                  
queue id:131076                                                                                                                                                                  
Initializing...                                                                                                                                                                  
...done initializing                                                                                                                                                             
ApproDrvInit: 10                                                                                                                                                                 
queue id:131076                                                                                                                                                                  
Initializing...                                                                                                                                                                  
...done initializing                                                                                                                                                             
Play this stream using the URL:                                                                                                                                                  
        rtsp://192.168.5.158:8555/PSIA/Streaming/channels/0?videoCodecType=MJPEG                                                                                                 
Play this stream using the URL:                                                                                                                                                  
        rtsp://192.168.5.158:8557/PSIA/Streaming/channels/2?videoCodecType=H.264                                                                                                 
Play this stream using the URL:                                                                                                                                                  
        rtsp://192.168.5.158:8554/PSIA/Streaming/channels/1?videoCodecType=MPEG4                                                                                                 
Play this stream using the URL:                                                                                                                                                  
        rtsp://192.168.5.158:8556/PSIA/Streaming/channels/2?videoCodecType=H.264                                                                                                 
ApproDrvInit: 3                                                                                                                                                                  
queue id:131076                                                                                                                                                                  
queue id:0                                                                                                                                                                       
queue id:32769                                                                                                                                                                   
ApproDrvInit: 2                                                                                                                                                                  
queue id:131076                                                                                                                                                                  
Initializing...                                                                                                                                                                  
...done initializing                                                                                                                                                             
Play this stream using the URL:                                                                                                                                                  
        rtsp://192.168.5.158:8553/PSIA/Streaming/channels/1?videoCodecType=MPEG4                                                                                                 
queue id:0                                                                                                                                                                       
[16/Nov/2011:07:31:47 +0000] boa: server version Boa/0.94.13                                                                                                                     
[16/Nov/2011:07:31:47 +0000] boa: server built Nov 11 2011 at 16:41:51.                                                                                                          
[16/Nov/2011:07:31:47 +0000] boa: starting server pid=792, port 80                                                                                                               
UDPString=uuid:Upnp-TVEmulator-1_0-00_0006303610</UDN>                                                                                                                           
                                                                                                                                                                                 
INIT: Entering runlevel: 3                                                                                                                                                       
error code = 0                                                                                                                                                                   
device advertisement succeed.                                                                                                                                                    
                                                                                                                                                                                 
MontaVista(R) Linux(R) Professional Edition 5.0.0 (0702774)                                                                                                                      
                                                                                                                                                                                 
DM365_IPNC login:

----------------------------------------

I just want to know why did it happen? ( system_server/512[CPU#0]: BUG in local_bh_enable at kernel/softirq.c:196 )  and how do i resolve it ?

please help me,thank you very much