Tool/software:
Hello,
I'm working on secure boot with the SK-AM62X and I have a few questions about the keywriter:
- Is it possible to boot from the keywriter (kw-tiboot3.bin) on an SD card (backup boot mode)? In the AM62X_OTP_Keywriter_User_Guide, it mentions that the keywriter application has only been validated with UART, OSPI and USB-DFU boot modes.
- Is it necessary to use the flashwriter to flash the regular tiboot3.bin? After writing the keys, can I boot a signed firmware from the SD card and flash the eMMC (primary boot media) from the SD?
Thank you in advance for your help!