This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

loading programs to DM36x on the evaluation board

I've just got TMS320DM36x DVEVM and there are 2 simple questions:

1. How should I program the processor? I have a SD-card shipped with the board. It contains Linux and bootloader. Now there are some demo programs on the card. Which file from a project need I write and where? As I got, <file_name>.hex to the folder "BOOT", but I want to clarify.

2. Is there a kind of  "hello world" program available for this?

 

Thanks in advance!!!

  • Hi,

    Using the TI dvsdk (based on Linux) package you could find a lot of demos programs, e.g. to encode/decode video/audio.
    Moreover, you would find bootloaders, kernel and filesystem images to re-initialize your processor boot and linux system architecture (the way is UBL --> u-boot --> kernel --> FS).

    When you are writting your own programs and want to test, you can transfer them into your board thanks to USB for example. Another way is to use a NFS if you built it yet...
    I do not remember well if it contains a default "hello world" program to begin, but in the provided Software Developers Guide, you have a very easy process to follow to build your own "hello world" app ;)

    PS/ I noticed this post is pretty old, hope it could helps somebody in the same case...