This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x EVM Ethernet Connectivity

Other Parts Discussed in Thread: TMDXEVM3358

 

Hello,

 

We are going to purchase AM335x EVM TMDXEVM3358. We need to test the Gbit ethernet ports(x2).

 

The features mentioned on the EVM's product folder says "10/100 Ethernet (1)".

But I believe its a TYPO and it would be 10/100/1000.

 

In our case, we need to evaluate two ethernet ports,

if the EVM has only one ethernet port, is there any option to connect another port to this EVM?

 

Please let me know if there are any daughter card we need to buy for ethernet dual ports,

and also will the "Ethernet Driver" or StarterWare from TI support Dual ehternet/Dual MAC mode?

 

 

Regards

Ayus.