Hi
We recently switched nand chip on our product (from 48nm [MT29F2G08AADWP-ET:D] to 34nm [MT29F2G08ABAEAWP-IT]) and we have been seeing some weird issues. There were regular crashes and there were a couple times where the uboot param partition got erase all by itself.
We are using u-boot 2009.03 and linux kernel 2.6.32.17.
Below is a table of the differences of the 2 Nand chip from Micron:
Micron TN-29-52: Migrating 1Gb 48nm and 2Gb/4Gb 57nm SLC NAND Flash Memory to 34nm
| Feature | 1Gb 48nm, 2Gb/4Gb 57nm | 1Gb, 2Gb, 4Gb 34nm |
| ECC | 1 bit per 528 bytes | 4 bits per 528 bytes or on-die ECC |
| Vendor ID | 20h | 2Ch |
| RC/WC | 25ns (3V), 45ns (1.8V) | 20ns (3V), 25ns (1.8V) |
| BERS | 1Gb: 1500µs (TYP) 2Gb: 2000µs (TYP) | 700µs (TYP) |
| Command set | ONFI and legacy | ONFI |
| Block0 | Valid at shipment 1 bit/528 bytes ECC | Valid at shipment, 1 bit/528 bytes ECC up to 1K PROGRAM/ERASE cycles |
| RESET at power-on | Not required | Required |
One thing I am wondering is if we are doing the "RESET at power-on" . So which part of the dm365 is supposed to do that? How do I verify that it is doing it?
Any other ideas on how to make sure things are compatible??
Thanks!!
Roy