Part Number: AM625
Other Parts Discussed in Thread: AM62A7
Tool/software:
We have a custom AM625 board driving a RGB LCD in 565 mode.
The first text page it displays is OK - thereafter it seems that half the pixels are missing?
I have modified 'k3-am625-beagleplay.dts' to remove the HDMI and replace it with the following snippets:
panel {
compatible = "winstar,wf50fswagdnn0";
port {
panel_in: endpoint {
remote-endpoint = <&dpi1_out>;
};
};
};
&dss {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&dss0_pins_default>;
};
&dss_ports {
/* VP2: DPI Output */
port@1 {
reg = <1>;
dpi1_out: endpoint {
remote-endpoint = <&panel_in>;
};
};
};
Also added the following to panel-simple.c:
static const struct drm_display_mode winstar_wf50fswagdnn0_mode = {
.clock = 24750,
.hdisplay = 800,
.hsync_start = 800 + 54,
.hsync_end = 800 + 54 + 2,
.htotal = 800 + 54 + 2 + 44,
.vdisplay = 480,
.vsync_start = 480 + 49,
.vsync_end = 480 + 49 + 2,
.vtotal = 480 + 49 + 2 + 22,
.flags = DRM_MODE_FLAG_NVSYNC | DRM_MODE_FLAG_NHSYNC,
};
static const struct panel_desc winstar_wf50fswagdnn0 = {
.modes = &winstar_wf50fswagdnn0_mode,
.num_modes = 1,
.bpc = 8,
.size = {
.width = 152,
.height = 91,
},
.bus_flags = DRM_BUS_FLAG_DE_HIGH |
DRM_BUS_FLAG_PIXDATA_SAMPLE_NEGEDGE |
DRM_BUS_FLAG_SYNC_SAMPLE_NEGEDGE,
.bus_format = MEDIA_BUS_FMT_RGB565_1X16,
// .bus_format = MEDIA_BUS_FMT_RGB888_1X24,
.connector_type = DRM_MODE_CONNECTOR_DPI,
};
It does not seem to be a synchronization problem as the display is stable - just missing pixels as in the attached Video:
Thanks in advance.