Part Number: AM62A7
Tool/software:
Hi supporter,
Related to thread AM62A7: GPIO interrupt number and event id on C75 I want to ask more because seem the thing is not clear to me.
Let me ask more detail question.
1. If I want to use MCU_GPIO0_6 as input interrupt, I will use WKUP_MCU_GPIOMUX_INTROUTER0 source, right? Can I use the same interrupt number 21 fỏ this GPIO?
2. In the example for gpio1_22, even id is defined as : CSLR_C7X256V0_CLEC_GIC_SPI_MAIN_GPIOMUX_INTROUTER0_OUTP_15 + 256U. So what is this even id if I want to use MCU GPIO0_6?
3. Can I use MAIN_GPIOMUX_INTROUTER0_OUTP_14 for event id of Gpio1_22?
Best regards,
J