Hello,
I am trying to create DSP bios configuration file for my custom board, I have DSP bios 5.41.10.36 with CCS 5.1.0.07001.
When I add DSP bios configuraion file using custom "Platform.tci" with device name 5501(code snippet as follows) in configuration tool it recognize device C5502 instead C5501.
var params = {
clockRate: 200,
catalogName: "ti.catalog.c5500",
deviceName: "5501",
regs: device_regs,
mem: mem_ext
};
I am providing my platform configuration file in attachment, can someone try to recreate this problem to find if there is problem with bios.
6131.HD_Aud.zip
By the way when I try to connect to device on hardware though XDS100V2 it gives me Device ID not recognise.