This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6412: PCIe boot initialization time from reset

Part Number: AM6412

Tool/software:

Customer wants to make PCIe card with AM64x, as the RC computer need to configure EP within 200ms after send out PCIe reset signal, otherwise it can't recognize the device.

As AM64x has not PCIe module specific reset signal, the reset from RC should connect to AM64x warm reset.

Question:

#1. What is the initialization time of PCIe boot until RC can configure AM64x PCIe?

#2. The reset signa from RCl should connect to MCU_RESETz or main domain RESET_REQz?