This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: Configuring firewall for DMA buffer pool

Part Number: AM623


Tool/software:

Hello,

this is a direct follow up to https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1460476/am623-understanding-firewall-for-dma

At first the solution seemed to work, however with the development ongoing, we now discovered that this firewall configuration only applies to the descriptor ring.
It does not cover buffers allocated for frames, so the DMA is able to write receiving frames anywhere in memory without respecting the firewall configuration.

Is there an additional ID required to be blocked? Why is there a difference anyway, is there another hardware component involved which does the transaction of frames?

Thanks

  • Hello,

    I am not very familiar with the DMA architecture but the firewalls only cares about protecting a given memory address space. If there are multiple address spaces, like for descriptors and buffers as you said, associated with the DMA then you would need to firewall such address spaces.

    Regards,

    Prashant

  • Hello,

    my current firewall configuration is as you suggested:

    • Background region for the whole address space 0x80000000 - 0xe0000000 with these permissions:
      • Allow access to everyone using wildcard privid 0xC3.
      • Allow access to everyone using wildcard privid 0xC3 (redundant).
      • Block access to DMA (privid = 0).
    • Foreground regions 0xb0000000-0xb0200000 with the following three permission settings:
      • Allow access to everyone using wildcard privid 0xC3.
      • Allow access to everyone using wildcard privid 0xC3 (redundant).
      • Allow access to everyone using wildcard privid 0xC3 (redundant).

    The descriptor ring is located at 0xb0000000, frame buffers are allocated starting at 0xa0000000.

    From the Firewall config I would assume, that DMA should not be able to write at 0xa0000000, but it can. On the other hand when the foreground region is somewhere else, DMA no longer works because of missing access to 0xb0000000.

    So to me it looks like the Firewall does not properly protect memory accesses from DMA. I also tried adding priv ID 192 (DMA Reserved Priv-ID) to the blocked list, but without change.

    I noticed that the Frame buffers use ASEL (another system I do not fully understand) and the TRM states that the Firewall on DDR is not ASEL capable. 
    Could this be the problem here? Could you explain what ASEL is used for?

    Thanks

  • Hello,

    From the Firewall config I would assume, that DMA should not be able to write at 0xa0000000, but it can.

    It should unless the DMA transaction was tagged with another PRIVID.

    You could create another foreground regions for the frame buffers address space with the permissions to block access for everyone (0xC30000). Then, you can get the PRIVID from the firewall exception logging by SYSFW.

    Regards,

    Prashant

  • Hello,

    how can I enable firewall logging?

    Thanks

  • Hello,

    Please refer to the following guide for enabling TIFS logs:

    https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/10_01_10_04/exports/docs/linux/How_to_Guides/Host/SYSFW_Trace_Parser.html

    The TIFS logs, if enabled correctly, would come on the MAIN_UART1 instance.

    Regards,

    Prashant

  • Hello,

    thank you for the link. I need some time for this because on our board UART1 is not easily accessible externally.

  • Hello,

    The traces could also be collected from the memory buffer as described here:

    https://software-dl.ti.com/tisci/esd/latest/4_trace/trace.html#trace-memory-buffer-location

    However, since these buffers are circular ones, the traces captured may not be full and not provide the relevant information. But, it can be given a try if it's too much to enable UART1.

    Regards,

    Prashant

  • Hello,

    I managed to read the trace from the memory buffer.

    Here are my findings:

    Blocking the descriptor ring (priv-id 0, starting at 0xB0200000) :

    Because only priv-id 0 is blocked here, this should originate from the DMA.

    FWL Bit  0x1
    Exception addr  0x45B0000
    FWL Exception  0x1000100
     0x60000
     0xB0200000
     0x0
     0x821000
     0x8
    
    FWL Bit  0x1
    Exception addr  0x45B08000
    FWL Exception  0x1000100
     0x60000
     0xB02002C8
     0x0
     0x821000
     0x8
    
    FWL Bit  0x1
    Exception addr  0x45B08000
    FWL Exception  0x1000100
     0x60000
     0xB0200570
     0x0
     0x821000
     0x8

    Blocking the buffer ring (priv-id 0xc3, starting at 0x8FFF0000):

    Here the initiator should be the dma, because the address is not accessed before receiving data (AFAIK).

    FWL Bit  0x1
    Exception addr  0x45B08000
    FWL Exception  0x1000100
     0x70000
     0x8FFF2040
     0x0
     0x42201
     0x40
     
    FWL Bit  0x1
    Exception addr  0x45B08000
    FWL Exception  0x1000100
     0x70000
     0x8FFF4040
     0x0
     0x42201
     0x40
    
    FWL Bit 
    0x1
    Exception addr  0x45B08000
    FWL Exception  0x1000100
     0x70000
     0x8FFF5040
     0x0
     0x42201
     0x40
    
    FWL Bit  0x1
    Exception addr  0x45B08000
    FWL Exception  0x1000100
     0x70000
     0x8FFF6040
     0x0
     0x42201
     0x40
    
    FWL Bit  0x1
    Exception addr  0x45B08000
    FWL Except
    on  0x1000100
     0x70000
     0x8FFF7040
     0x0
     0x42201
     0x40

    Could you please help me understanding these logs?
    I can identify the accessed address and assume the FWL Bit being the firewall ID (1=DDR). How can I find the priv-id causing the transaction?

    Thanks.

  • Hello,

    According to the table "Table 3-5 Firewall Violation Parameters"

    https://www.ti.com/document-viewer/lit/html/SPRUIV7B#GUID-26BD43DA-22BA-4EC0-A0BA-0E6F7AD6EE27/TITLE-SPRUIM0INT_SPRUIM0_SA_00050

    The privid is part of the DATA2 register. In the logs, the second last value in the exception log is DATA2 register value. So,

    Blocking the buffer ring (priv-id 0xc3, starting at 0x8FFF0000):

    Those exceptions are for the write transactions from the privid 1.

    According to the following, the privid 1 is associated with the A53.

    https://software-dl.ti.com/tisci/esd/latest/5_soc_doc/am62x/firewalls.html#list-of-priv-ids

    Unless the DMA is inheriting the initiator privid, the write transaction could be originating from the Linux Kernel. Are you sure that no one except DMA is writing to those buffers?

    Regards,

    Prashant

  • Hello,

    indeed it looks like DMA is inheriting the A53 priv Id. After some more testing I identified that the required permission in the DMA buffer region is Non-Secure/User/Cache. If this is enabled, frames are properly received, but if it is disabled, neither DMA nor Linux can access the region. I tested it with only this single permission, which shows to me that it is also used by the DMA, otherwise it would trigger another exception. Also I do not see a write access to the RX buffers in the Linux code.

  • Hello Prashant,

    what could be the reason for DMA inheriting the A53 priv ID? Could the incoming transaction be handled by A53 after the descriptor was fetched?

    I see that ASEL is set to 15 for the buffer addresses, can this change the priv ID? But I am having issues, when I set it to 0 in the device tree.

    Thanks.

  • Hello ,

    Any update on this issue?

  • Hello,

    Apologies for the delayed response.

    I tested the UDMA_MEMCPY_POLLING example for A53 core from the MCU+ SDK. And I do not see DMA using different PrivIDs for descriptors and frame buffers.

    // Descriptor buffer
    FWL Bit  0x1
    Exception addr  0x45B08000
    FWL Exception  0x1000100
     0x60000
     0xA0000000
     0x0
     0x801000
     0x10
    
    // Tx and Rx buffers
    FWL Bit  0x1
    Exception addr  0x45B08000
    FWL Exception  0x1000100
     0x60000
     0xA0100000
     0x0
     0x801000
     0x40

    Can you share your current firewall configurations?

    Thanks!

  • Hello Prashant,

    thank you for the test. This gives me the hope that the hardware supports my goal and I might miss some configurations.

    Here is my current firewall configuration with some annotations:

    TI UDMA (INFO)>: fwl_id=1, region=0, n_permission_regs=3
    TI UDMA (INFO)>: control=0x11a
    TI UDMA (INFO)>: perm[0]=0xc3ffff
    TI UDMA (INFO)>: perm[1]=0xc3ffff
    TI UDMA (INFO)>: perm[2]=0x008888 <- Disallow UDMA
    TI UDMA (INFO)>: Range: 0x80000000 - 0xefffffff <- full memory range
    TI UDMA (INFO)>: fwl_id=1, region=1, n_permission_regs=3
    TI UDMA (INFO)>: control=0x1a
    TI UDMA (INFO)>: perm[0]=0xc3ffff
    TI UDMA (INFO)>: perm[1]=0xc3ffff
    TI UDMA (INFO)>: perm[2]=0xc3ffff
    TI UDMA (INFO)>: Range: 0xb0000000 - 0xb007ffff <- buffer descriptor ring
    TI UDMA (INFO)>: fwl_id=1, region=2, n_permission_regs=3
    TI UDMA (INFO)>: control=0x1a
    TI UDMA (INFO)>: perm[0]=0xc38888
    TI UDMA (INFO)>: perm[1]=0xc38888
    TI UDMA (INFO)>: perm[2]=0x018888 <- Kernel cannot boot
                             0x018c88 (user,nsec,cache) <- Kernel can boot and frames can be received
    TI UDMA (INFO)>: Range: 0xa0000000 - 0xa8000fff <- Linux Kernel + frame buffers

    With the last region I am experimenting to see what works and what not. I identified the cache permission flag to enable memory access from Linux. However, with this flag set, also DMA can write to memory. Maybe there is some cache configuration missing?

    Thanks and regards

  • Hello Prashant,

    any remarks on my firewall configuration?

    I have now figured out that with setting the cache bit in control register (0x200) I can get some better control over the access and the read/write permissions perform more like I expected.

    However, I still only catch accesses to the frame buffers with priv-id 1. 

    What could be the reason for DMA inheriting the A53 priv ID? Could the incoming transaction be handled by A53 after the descriptor was fetched?

    I see that ASEL is set to 15 for the buffer addresses, can this change the priv ID?

    Thanks.