Other Parts Discussed in Thread: DM3730
Hi all,
I have a Beagle board xM Rev.C on to which DVSDK 4.01 is ported. I decoded the demo video(davincieffect.mpeg4) using ti-dmai applications as given below.
root@beagleboard-dvsdk:/usr/share/ti/ti-dmai-apps# ./video_decode_io2_dm3730.x47
0MV -c mpeg4dec -i /usr/share/ti/data/videos/davincieffect.mpeg4 -o /media/sda1/
raw.yuv
Starting application...
Loader created and primed, entering main loop..
Loaded Frame 1: frame size 9967
Display Frame 1: Wrote UYVY frame size 1843200 (1280x720) to disk
Loaded Frame 2: frame size 491
Display Frame 2: Wrote UYVY frame size 1843200 (1280x720) to disk
Loaded Frame 3: frame size 19
Display Frame 3: Wrote UYVY frame size 1843200 (1280x720) to disk
Loaded Frame 4: frame size 19
Display Frame 4: Wrote UYVY frame size 1843200 (1280x720) to disk
Loaded Frame 5: frame size 491
Display Frame 5: Wrote UYVY frame size 1843200 (1280x720) to disk