Other Parts Discussed in Thread: OMAP-L138, OMAPL138
I have the LogicPD board, and from u-boot doing a USB reset, with a usb flash drive plugged into either/or/both the OTG USB2.0 and the USB1.1 ports on the board, only the OTG port is recognized... is there a way to boot from the 1.1 port?
Also I'm using the UBL/u-boot from EVM 4.02 (03.20.00.14) and I noticed that in the next release 03.21.00.04, the release notes don't mention booting from USB at all, has that been removed?