This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO: Does the armcl compiler support Cmake?

Part Number: CCSTUDIO

Tool/software:

Hi TI guys,

I use the ti-cgt-arm_20.2.0.LTS/bin/armclto compile in the CmakeLists.txt, but it reports the following error:

CMake Error at /usr/share/cmake-3.25/Modules/CMakeTestCXXCompiler.cmake:63 (message):
is not able to compile a simple test program.
It fails with the following output:
***
CMakeFiles/cmTC_27091.dir/build.make:99: recipe for target 'cmTC_27091' failed..

The CMakeLists.txt as follow:

`option(UNDER_ARM "ARM toolchain compile" ON)
if(UNDER_ARM)
set(CMAKE_SYSTEM_PROCESSOR arm)
set(CMAKE_CXX_COMPILER /home/xiejieying/rtos_sdk_7.1/ti-cgt-arm_20.2.0.LTS/bin/armcl)
set(CMAKE_C_COMPILER /home/xiejieying/rtos_sdk_7.1/ti-cgt-arm_20.2.0.LTS/bin/armcl)
message("CMAKE_CXX_COMPILER_VERSION: ${CMAKE_CXX_COMPILER_VERSION}")
endif()

project(integrator)`

Best regard