Part Number: PROCESSOR-SDK-J784S4
Tool/software:
Hello everyone,
I'm trying to test external watchdog by using GPIO API on TDA4.
Here's the relevant code which I based off of the code I've seen in other thread here on the forum:
#define PADCONFIG_34 0x0011C088
#define WKUP_PADCONFIG_23 0x4301C05C
#define WKUP_PADCONFIG_41 0x4301C0A4
#define MCU_WDT_WDI_PIN (38U)
#define MCU_WDT_WDO_PIN (34U)
#define SYS_MCU_PWRDN_PIN (55U)
static void watchdog_isr(void)
{
App_ConsolePrintf("Watchdog triggered!\n");
// Make rising edge on SYS_MCU_PWRDN pin
GPIOPinWrite_v0(CSL_WKUP_GPIO0_BASE, SYS_MCU_PWRDN_PIN, GPIO_PIN_LOW);
GPIOPinWrite_v0(CSL_WKUP_GPIO0_BASE, SYS_MCU_PWRDN_PIN, GPIO_PIN_HIGH);
}
GPIO_PinConfig gpioPinConfigs[] = {
GPIO_DEVICE_CONFIG(0, MCU_WDT_WDO_PIN) |
GPIO_CFG_IN_INT_FALLING | GPIO_CFG_INPUT,
GPIO_DEVICE_CONFIG(0, MCU_WDT_WDI_PIN) |
GPIO_CFG_OUTPUT,
GPIO_DEVICE_CONFIG(0, SYS_MCU_PWRDN_PIN) |
GPIO_CFG_OUTPUT
};
GPIO_CallbackFxn callbacks[] = {
watchdog_isr,
NULL,
NULL
};
GPIO_v0_Config GPIO_v0_config = {
gpioPinConfigs,
callbacks,
sizeof(gpioPinConfigs) / sizeof(gpioPinConfigs[0]),
sizeof(callbacks) / sizeof(callbacks[0]),
~0
};
void AppGPIOPadConfig()
{
*(uint32_t*)PADCONFIG_34 = 0x00060007;
*(uint32_t*)WKUP_PADCONFIG_23 = 0x00010007;
*(uint32_t*)WKUP_PADCONFIG_41 = 0x00010007;
}
///////////////////////////////////////////////////////////
GPIO_v0_HwAttrs gpio_cfg;
GPIO_socGetInitCfg(0, &gpio_cfg);
gpio_cfg.baseAddr = CSL_WKUP_GPIO0_BASE;
(gpio_cfg.intCfg[0]).intcMuxNum = INVALID_INTC_MUX_NUM;
(gpio_cfg.intCfg[0]).intcMuxInEvent = 0;
(gpio_cfg.intCfg[0]).intcMuxOutEvent = 0;
GPIO_socSetInitCfg(0, &gpio_cfg);
GPIO_init();
//GPIO_setCallback(0, watchdog_isr);
GPIO_enableInt(0);
AppGPIOPadConfig();
GPIOSetDirMode_v0(CSL_WKUP_GPIO0_BASE, MCU_WDT_WDI_PIN, GPIO_DIRECTION_OUTPUT);
GPIOPinWrite_v0(CSL_WKUP_GPIO0_BASE, MCU_WDT_WDI_PIN, GPIO_PIN_HIGH);
//GPIOSetDirMode_v0(CSL_WKUP_GPIO0_BASE, MCU_WDT_WDO_PIN, GPIO_DIRECTION_INPUT);
GPIOSetDirMode_v0(CSL_WKUP_GPIO0_BASE, SYS_MCU_PWRDN_PIN, GPIO_DIRECTION_OUTPUT);
// Attempt to activate callback manually
GPIO_toggle(0);
Osal_delay(20);
GPIO_toggle(0);
for (uint32_t i = 0; i < 20; i++)
{
App_ConsolePrintf("\nNotifying watchdog...\n");
// Make a falling edge on WDI and assert it back
GPIOPinWrite_v0(CSL_WKUP_GPIO0_BASE, MCU_WDT_WDI_PIN, GPIO_PIN_LOW);
GPIOPinWrite_v0(CSL_WKUP_GPIO0_BASE, MCU_WDT_WDI_PIN, GPIO_PIN_HIGH);
Osal_delay(1000);
}
App_ConsolePrintf("\nStopped notifications. Waiting for watchog to trigger.\n");
GPIOPinWrite_v0(CSL_WKUP_GPIO0_BASE, SYS_MCU_PWRDN_PIN, GPIO_PIN_LOW);
Osal_delay(50);
GPIOPinWrite_v0(CSL_WKUP_GPIO0_BASE, SYS_MCU_PWRDN_PIN, GPIO_PIN_HIGH);
The issue is that watchdog_isr callback never gets called even when using GPIO_toggle to manually trigger it.
I also took a look at SYS_MCU_PWRD pin with oscilloscope and there weren't any changes.
Any help would be appreciated.