Other Parts Discussed in Thread: AM1808, OMAP-L138
Hi -
I want to connect an AM1808 Zoom DK running Linux to a PC and have it show up on the PC as a mass storage device (USB thumb drive). I tried using a USB cable with miniB plug on one end and full-size A plug on the other end to connect the DK board to the PC. I connected the miniB end of the cable to J6 (miniAB socket) on the Zoom DK board and full-size A plug end of the cable to a USB host port on my PC. The AM1808 Zoom DK board was running the standard Linux build that came with the DK board. When I plugged the cable into the PC, the host port of the PC did not detect any USB device connection. Basically nothing happened.
Question - How can I configure / create a Linux build or the AM1808 Zoom development kit that has support for USB mass storage device mode? I am a Linux nubie so detailed instructions are greatly appreciated.
Thanks,
Doug