This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM62L ( AM62L32 , AM62L31 ) Custom board hardware design – I2C interface

Part Number: AM62L

Tool/software:

Hi TI Experts,

I have the below queries regarding the I2C interface

  1. Need information on the number of I2C interfaces available
  2. Termination of I2C interfaces when used as I2C interface and not used as I2C interface.
  3. Any additional recommendations / Guidelines
  4. Any concerns on Interfacing SoC Non-Failsafe I2C to devices that are powered before the SoC- Ex PMIC
  5. Any exception that are required to be considered when using the I2C interfaces. 
  6. Can the I2C interface be used to interface with devices supporting SMBus or PMBus 

Let me know your thoughts.

Unused iOs connection

(+) [FAQ] What should be done with unused I/O pins of the level translator devices? - Logic forum - Logic - TI E2E support forums