This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: can control 3mega resolution(2560x1440) 6CH camera at the same time?

Other Parts Discussed in Thread: TDA4VH

hello, Ti team

i want to control 6ch(2560x1440) cameras at the same time

we need to get 6ch images from cameras and make images for surround view image (SVM)

it's possible by using TDA4VH?

when i checked on datasheet i get information like a below

Video acceleration: • H.264/H.265 Encode/Decode, up to 960MP/s (TDA4xH) or 480MP/s (TDA4xP)

please check

thanks,

  • Hello,

    I apologize for the delay in response. Yes, 6x 3MP cameras are supported on TDA4VH. A 12-camera application has been validated on TDA4VH using imx390 sensors (2MP) split across 2 VISS via Fusion 2 (FPDLink IV). The constraints to keep in mind are as follows:

    CSI bandwidth: 2.5 Gbps per lane (1, 2, 3 or 4 data lane mode supported)

    The ISP (i.e. VISS) bandwidth: 720 Mpixels/sec (576 Mpixels/sec considering SW overhead) and there are 2 such VISS ISPs present

    Thank you,

    Fabiana