Other Parts Discussed in Thread: AM3359, , TPS65217, TPS65910
Tool/software:
Dear colleagues,
Our product based on AM335x (in most case AM3352/AM3359) CPUs.
Like operation system we use our own Linux based on Yocto build system. In current solution for our custom board we use u-boot 2018.01 without any issue.
For some technical reason we decided to upgrade our OS system. Now we are going to use modern u-boot 2024.04 and linux kernel 6.6.x with Yocto 5.0.X and gcc 13
Unfortunately during migration we faced with a problem of launch U-Boot 2024.04.
Boot logs:
U-Boot SPL 2024.04-ti-g29d0c23d67ee (Feb 23 2025 - 19:32:46 +0000) Trying to boot from MMC1 VI_DEBUG: spl: mmc boot mode: fs VI_DEBUG: spl_mmc_do_fs_boot executing spl_start_uboot VI_DEBUG: spl_start_uboot ENTER VI_DEBUG: spl_start_uboot VI_DEBUG: spl_start_uboot sdram_init_done = 0 VI_DEBUG: spl_start_uboot board_init_f_state = 2 VI_DEBUG: spl_start_uboot gd->ram_size 0x20000000 VI_DEBUG: bd_info size = 92 VI_DEBUG: bd_info stack = 96 VI_DEBUG: env_load CFG_SYS_SDRAM_BASE 0x80000000 0x80000000 VI_DEBUG: spl_start_uboot env_get_yesno NO VI_DEBUG: spl_mmc_do_fs_boot executing spl_load_image_fat spl_load_image_fat: fat_size, file u-boot.img size - 0 VI_DEBUG: _spl_load ENTER VI_DEBUG: _spl_load info->priv u-boot.img VI_DEBUG: _spl_load loading hdr from 0x0 to 807fffc0 VI_DEBUG: fat_read_file reading u-boot.img at pos 0x0 VI_DEBUG: _spl_load FDT_MAGIC branch VI_DEBUG: _spl_load activated SPL_LOAD_FIT VI_DEBUG: spl_load_simple_fit ENTER VI_DEBUG: fat_read_file reading u-boot.img at pos 0x0 VI_DEBUG: load_simple_fit ENTER VI_DEBUG: fat_read_file reading u-boot.img at pos 0x0 VI_DEBUG load_simple_fit External data: dst=80800000, offset=fc8, size=3cec4 VI_DEBUG: load_simple_fit NO_COMPRESS length = 249540 VI_DEBUG: spl_load_simple_fit load_simple_fit ret 0 VI_DEBUG: load_simple_fit ENTER VI_DEBUG: fat_read_file reading u-boot.img at pos 0x0 VI_DEBUG load_simple_fit External data: dst=8083cf00, offset=3de8c, size=15f10 VI_DEBUG: load_simple_fit NO_COMPRESS length = 89872 VI_DEBUG: _spl_load spl_image load_addr 0x80800000 entry_point 0x80800000 VI_DEBUG: _spl_load spl_image offset 0x0 VI_DEBUG: _spl_load spl_image size 249540 VI_DEBUG: _spl_load spl_image flags 2 VI_DEBUG: spl_load_image_fat spl_load done sdram_init_done = 0 VI_DEBUG spl_load_image_fat: return 0 VI_DEBUG: spl_mmc_do_fs_boot executing spl_load_image_fat ret = 0 VI_DEBUG: spl_mmc_load spl_mmc_do_fs_boot err=0 VI_DEBUG: image entry point: 0x80800000 b8 0 0 ea 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5
The situation looks like MLO start properly but u-boot.img doesn't start. VI_DEBUG - it's prefix our additional prefix for logs
MLO has achieved image entery point:
VI_DEBUG: image entry point: 0x80800000 b8 0 0 ea 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5
The first 32 bytes started from address 0x80800000 is:
b8 0 0 ea 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5 14 f0 9f e5
My jump_to_image_no_args looks like:
void __noreturn jump_to_image_no_args(struct spl_image_info *spl_image)
{
typedef void __noreturn (*image_entry_noargs_t)(u32 *);
int i;
image_entry_noargs_t image_entry =
(image_entry_noargs_t) spl_image->entry_point;
u32 boot_params = *((u32 *)OMAP_SRAM_SCRATCH_BOOT_PARAMS);
debug("image entry point: 0x%lX\n", spl_image->entry_point);
printf("VI_DEBUG: image entry point: 0x%x\n", spl_image->entry_point);
uint8_t * entry_data = (uint8_t *) spl_image->entry_point;
for(i = 0; i < 32; i++)
{
printf(" %x", (int)entry_data[i]);
}
printf("\n");
/* Pass the saved boot_params from rom code */
image_entry((u32 *)boot_params);
}
Bytes from console matches the u-boot.img content:

From my side I can made the conclusion that u-boot.img was load correctly and DDR is work (settings for DDR the same like on 2018.01)
My part of u-boot configuration:
CONFIG_ARM=y CONFIG_ARCH_CPU_INIT=y CONFIG_ARCH_OMAP2PLUS=y CONFIG_TARGET_AM335X_WECAT3D=y CONFIG_MEL_COMMON_CMD_OPTIONS=y CONFIG_HAS_CUSTOM_SYS_INIT_SP_ADDR=y CONFIG_CUSTOM_SYS_INIT_SP_ADDR=0x4030ff00 CONFIG_SF_DEFAULT_SPEED=24000000 CONFIG_DEFAULT_DEVICE_TREE="am335x-mlsl-v11" CONFIG_AM33XX=y CONFIG_CLOCK_SYNTHESIZER=y CONFIG_TIMESTAMP=y CONFIG_SPL_LOAD_FIT=y CONFIG_SYS_BOOTM_LEN=0x1000000 CONFIG_DISTRO_DEFAULTS=y CONFIG_OF_BOARD_SETUP=y CONFIG_LOGLEVEL=7 CONFIG_SYS_EXTRA_OPTIONS="EMMC_BOOT" CONFIG_BOOTCOMMAND="run findfdt; run init_console; run finduuid; run distro_bootcmd" CONFIG_SYS_CONSOLE_INFO_QUIET=y CONFIG_ARCH_MISC_INIT=y CONFIG_SPL_SYS_MALLOC=y CONFIG_SPL_SYS_MALLOC_SIZE=0x800000 CONFIG_SPL_FIT_IMAGE_TINY=y CONFIG_SPL_ETH=y CONFIG_SPL_FS_LOAD_PAYLOAD_NAME="u-boot.img" CONFIG_VERSION_VARIABLE=y CONFIG_SPL=y CONFIG_SPL_OS_BOOT=y CONFIG_AUTOBOOT_KEYED=y CONFIG_AUTOBOOT_PROMPT="Press SPACE to abort autoboot in %d seconds\n" CONFIG_AUTOBOOT_DELAY_STR="d" CONFIG_AUTOBOOT_STOP_STR=" " #CONFIG_FASTBOOT=y CONFIG_CMD_SPL=y CONFIG_ISO_PARTITION=y CONFIG_MMC_OMAP_HS=y CONFIG_SPI_FLASH=y CONFIG_SPI_FLASH_SST=y CONFIG_SPI_FLASH_STMICRO=y CONFIG_PHYLIB=y CONFIG_SYS_NS16550=y CONFIG_DRIVER_TI_CPSW=y CONFIG_DM_PMIC=y CONFIG_PMIC_TPS65217=y CONFIG_SPL_POWER_TPS65910=y CONFIG_SPI=y CONFIG_DM_SPI=y CONFIG_OMAP3_SPI=y CONFIG_LZO=y CONFIG_SHOW_ERRORS=y CONFIG_SYS_I2C_SPEED=100000 CONFIG_SYS_I2C_SLAVE=0x1 CONFIG_DM_I2C=y CONFIG_OF_LIBFDT=y CONFIG_OF_LIBFDT_OVERLAY=y CONFIG_ENV_IS_IN_FAT=y CONFIG_OF_CONTROL=y CONFIG_OF_LIST="am335x-evm am335x-bone am335x-sancloud-bbe am335x-sancloud-bbe-lite am335x-sancloud-bbe-extended-wifi am335x-boneblack am335x-evmsk am335x-bonegreen am335x-icev2 am335x-pocketbeagle am335x-mlsl-v11" CONFIG_ENV_OVERWRITE=y CONFIG_SYS_RELOC_GD_ENV_ADDR=y CONFIG_SPL_ENV_IS_NOWHERE=y CONFIG_OF_EMBED=y CONFIG_ENV_FAT_FILE="uEnv.txt" CONFIG_LOG=y CONFIG_SPL_LOG=y CONFIG_SPL_PAYLOAD="u-boot.img" CONFIG_CC_OPTIMIZE_FOR_DEBUG=y
Full u-boot config in attach.
I kindly ask you to provide any ideas and suggestions for understanding the reason of this behavior of u-boot_2024.
Thanks in advance!
# # Automatically generated file; DO NOT EDIT. # U-Boot 2024.04 Configuration # # # Compiler: arm-we-linux-gnueabi-gcc (GCC) 13.3.0 # CONFIG_CREATE_ARCH_SYMLINK=y CONFIG_SYS_CACHE_SHIFT_6=y CONFIG_SYS_CACHELINE_SIZE=64 CONFIG_LINKER_LIST_ALIGN=4 # CONFIG_ARC is not set CONFIG_ARM=y # CONFIG_M68K is not set # CONFIG_MICROBLAZE is not set # CONFIG_MIPS is not set # CONFIG_NIOS2 is not set # CONFIG_PPC is not set # CONFIG_RISCV is not set # CONFIG_SANDBOX is not set # CONFIG_SH is not set # CONFIG_X86 is not set # CONFIG_XTENSA is not set CONFIG_SYS_ARCH="arm" CONFIG_SYS_CPU="armv7" CONFIG_SYS_SOC="am33xx" CONFIG_SYS_VENDOR="wenglorMEL" CONFIG_SYS_BOARD="weCat3D" CONFIG_SYS_CONFIG_NAME="am335x_weCat3D" # # Skipping low level initialization functions # # CONFIG_SKIP_LOWLEVEL_INIT is not set # CONFIG_SPL_SKIP_LOWLEVEL_INIT is not set # CONFIG_TPL_SKIP_LOWLEVEL_INIT is not set # CONFIG_SKIP_LOWLEVEL_INIT_ONLY is not set # CONFIG_SPL_SKIP_LOWLEVEL_INIT_ONLY is not set # CONFIG_SYS_ICACHE_OFF is not set # CONFIG_SPL_SYS_ICACHE_OFF is not set # CONFIG_SYS_DCACHE_OFF is not set # CONFIG_SPL_SYS_DCACHE_OFF is not set # # ARM architecture # CONFIG_COUNTER_FREQUENCY=0 # CONFIG_POSITION_INDEPENDENT is not set # CONFIG_SPL_USE_SEPARATE_FAULT_HANDLERS is not set # CONFIG_GIC_V3_ITS is not set CONFIG_HAS_VBAR=y CONFIG_HAS_THUMB2=y CONFIG_GPIO_EXTRA_HEADER=y CONFIG_ARM_ASM_UNIFIED=y CONFIG_SYS_ARM_CACHE_CP15=y CONFIG_SYS_ARM_MMU=y # CONFIG_SYS_ARM_MPU is not set CONFIG_ARM_CORTEX_A8_CVE_2017_5715=y CONFIG_CPU_V7A=y CONFIG_SYS_ARM_ARCH=7 CONFIG_SYS_ARM_CACHE_WRITEBACK=y # CONFIG_SYS_ARM_CACHE_WRITETHROUGH is not set # CONFIG_SYS_ARM_CACHE_WRITEALLOC is not set CONFIG_ARCH_CPU_INIT=y # CONFIG_SYS_ARCH_TIMER is not set # CONFIG_ARM_SMCCC is not set CONFIG_SYS_THUMB_BUILD=y CONFIG_SPL_SYS_THUMB_BUILD=y # CONFIG_SYS_L2_PL310 is not set # CONFIG_SPL_SYS_L2_PL310 is not set # CONFIG_SYS_L2CACHE_OFF is not set # CONFIG_ENABLE_ARM_SOC_BOOT0_HOOK is not set CONFIG_USE_ARCH_MEMCPY=y CONFIG_SPL_USE_ARCH_MEMCPY=y CONFIG_USE_ARCH_MEMSET=y CONFIG_SPL_USE_ARCH_MEMSET=y # CONFIG_ARCH_AT91 is not set # CONFIG_ARCH_DAVINCI is not set # CONFIG_ARCH_HISTB is not set # CONFIG_ARCH_KIRKWOOD is not set # CONFIG_ARCH_MVEBU is not set # CONFIG_ARCH_ORION5X is not set # CONFIG_TARGET_STV0991 is not set # CONFIG_ARCH_BCM283X is not set # CONFIG_ARCH_BCMSTB is not set # CONFIG_ARCH_BCMBCA is not set # CONFIG_TARGET_VEXPRESS_CA9X4 is not set # CONFIG_TARGET_BCMNS is not set # CONFIG_TARGET_BCMNS2 is not set # CONFIG_TARGET_BCMNS3 is not set # CONFIG_ARCH_EXYNOS is not set # CONFIG_ARCH_S5PC1XX is not set # CONFIG_ARCH_HIGHBANK is not set # CONFIG_ARCH_INTEGRATOR is not set # CONFIG_ARCH_IPQ40XX is not set # CONFIG_ARCH_KEYSTONE is not set # CONFIG_ARCH_K3 is not set CONFIG_ARCH_OMAP2PLUS=y # CONFIG_ARCH_MESON is not set # CONFIG_ARCH_MEDIATEK is not set # CONFIG_ARCH_LPC32XX is not set # CONFIG_ARCH_IMX8 is not set # CONFIG_ARCH_IMX8M is not set # CONFIG_ARCH_IMX8ULP is not set # CONFIG_ARCH_IMX9 is not set # CONFIG_ARCH_IMXRT is not set # CONFIG_ARCH_MX23 is not set # CONFIG_ARCH_MX28 is not set # CONFIG_ARCH_MX31 is not set # CONFIG_ARCH_MX7ULP is not set # CONFIG_ARCH_MX7 is not set # CONFIG_ARCH_MX6 is not set # CONFIG_ARCH_MX5 is not set # CONFIG_ARCH_NEXELL is not set # CONFIG_ARCH_NPCM is not set # CONFIG_ARCH_APPLE is not set # CONFIG_ARCH_OWL is not set # CONFIG_ARCH_QEMU is not set # CONFIG_ARCH_RENESAS is not set # CONFIG_ARCH_SNAPDRAGON is not set # CONFIG_ARCH_SOCFPGA is not set # CONFIG_ARCH_SUNXI is not set # CONFIG_ARCH_U8500 is not set # CONFIG_ARCH_VERSAL is not set # CONFIG_ARCH_VERSAL_NET is not set # CONFIG_ARCH_VF610 is not set # CONFIG_ARCH_ZYNQ is not set # CONFIG_ARCH_ZYNQMP_R5 is not set # CONFIG_ARCH_ZYNQMP is not set # CONFIG_ARCH_TEGRA is not set # CONFIG_ARCH_VEXPRESS64 is not set # CONFIG_TARGET_CORSTONE1000 is not set # CONFIG_TARGET_TOTAL_COMPUTE is not set # CONFIG_TARGET_LS2080A_EMU is not set # CONFIG_TARGET_LS1088AQDS is not set # CONFIG_TARGET_LS2080AQDS is not set # CONFIG_TARGET_LS2080ARDB is not set # CONFIG_TARGET_LS2081ARDB is not set # CONFIG_TARGET_LX2160ARDB is not set # CONFIG_TARGET_LX2160AQDS is not set # CONFIG_TARGET_LX2162AQDS is not set # CONFIG_TARGET_HIKEY is not set # CONFIG_TARGET_HIKEY960 is not set # CONFIG_TARGET_POPLAR is not set # CONFIG_TARGET_LS1012AQDS is not set # CONFIG_TARGET_LS1012ARDB is not set # CONFIG_TARGET_LS1012A2G5RDB is not set # CONFIG_TARGET_LS1012AFRWY is not set # CONFIG_TARGET_LS1012AFRDM is not set # CONFIG_TARGET_LS1028AQDS is not set # CONFIG_TARGET_LS1028ARDB is not set # CONFIG_TARGET_LS1088ARDB is not set # CONFIG_TARGET_LS1021AQDS is not set # CONFIG_TARGET_LS1021ATWR is not set # CONFIG_TARGET_PG_WCOM_SELI8 is not set # CONFIG_TARGET_PG_WCOM_EXPU1 is not set # CONFIG_TARGET_LS1021ATSN is not set # CONFIG_TARGET_LS1021AIOT is not set # CONFIG_TARGET_LS1043AQDS is not set # CONFIG_TARGET_LS1043ARDB is not set # CONFIG_TARGET_LS1046AQDS is not set # CONFIG_TARGET_LS1046ARDB is not set # CONFIG_TARGET_LS1046AFRWY is not set # CONFIG_TARGET_SL28 is not set # CONFIG_TARGET_TEN64 is not set # CONFIG_ARCH_UNIPHIER is not set # CONFIG_ARCH_SYNQUACER is not set # CONFIG_ARCH_STM32 is not set # CONFIG_ARCH_STI is not set # CONFIG_ARCH_STM32MP is not set # CONFIG_ARCH_ROCKCHIP is not set # CONFIG_ARCH_OCTEONTX is not set # CONFIG_ARCH_OCTEONTX2 is not set # CONFIG_TARGET_THUNDERX_88XX is not set # CONFIG_ARCH_ASPEED is not set # CONFIG_TARGET_DURIAN is not set # CONFIG_TARGET_POMELO is not set # CONFIG_TARGET_PE2201 is not set # CONFIG_TARGET_PRESIDIO_ASIC is not set # CONFIG_TARGET_XENGUEST_ARM64 is not set # CONFIG_ARCH_GXP is not set # CONFIG_SUPPORT_PASSING_ATAGS is not set # CONFIG_STATIC_MACH_TYPE is not set # CONFIG_TI_SECURE_DEVICE is not set CONFIG_TEXT_BASE=0x80800000 CONFIG_SYS_MALLOC_LEN=0x2000000 CONFIG_SYS_MALLOC_F_LEN=0x2000 CONFIG_SPL_GPIO=y CONFIG_SPL_LIBCOMMON_SUPPORT=y CONFIG_SPL_LIBGENERIC_SUPPORT=y CONFIG_NR_DRAM_BANKS=4 CONFIG_SPL_LDSCRIPT="arch/arm/mach-omap2/u-boot-spl.lds" CONFIG_ENV_SOURCE_FILE="" CONFIG_HAS_CUSTOM_SYS_INIT_SP_ADDR=y CONFIG_CUSTOM_SYS_INIT_SP_ADDR=0x4030ff00 CONFIG_ENV_SIZE=0x20000 CONFIG_DM_GPIO=y # CONFIG_SPL_DM_SPI is not set CONFIG_DEFAULT_DEVICE_TREE="am335x-mlsl-v11" CONFIG_SPL_TEXT_BASE=0x402F0400 # CONFIG_OMAP34XX is not set # CONFIG_OMAP44XX is not set # CONFIG_OMAP54XX is not set # CONFIG_AM43XX is not set CONFIG_AM33XX=y CONFIG_SYS_MPUCLK=500 # CONFIG_TARGET_AM335X_EVM is not set CONFIG_TARGET_AM335X_WECAT3D=y # CONFIG_TARGET_AM335X_BALTOS is not set # CONFIG_TARGET_AM335X_IGEP003X is not set # CONFIG_TARGET_AM335X_SHC is not set # CONFIG_TARGET_AM335X_GUARDIAN is not set # CONFIG_TARGET_AM335X_SL50 is not set # CONFIG_TARGET_BRXRE1 is not set # CONFIG_TARGET_BRSMARC1 is not set # CONFIG_TARGET_BRPPT1 is not set # CONFIG_TARGET_CHILIBOARD is not set # CONFIG_TARGET_ETAMIN is not set # CONFIG_TARGET_PCM051 is not set # CONFIG_TARGET_PHYCORE_AM335X_R2 is not set # CONFIG_TARGET_PXM2 is not set # CONFIG_TARGET_RASTABAN is not set # CONFIG_TARGET_RUT is not set # CONFIG_TARGET_THUBAN is not set # CONFIG_TARGET_PDU001 is not set CONFIG_CLOCK_SYNTHESIZER=y CONFIG_CLK_SYNTHESIZER_I2C_ADDR=0x65 CONFIG_PUB_ROM_DATA_SIZE=0x8400 CONFIG_CONS_INDEX=1 CONFIG_MEL_COMMON_CMD_OPTIONS=y CONFIG_OF_LIBFDT_OVERLAY=y CONFIG_MULTI_DTB_FIT_UNCOMPRESS_SZ=0x8000 # CONFIG_DM_RESET is not set CONFIG_SYS_MONITOR_LEN=0 CONFIG_SPL_MMC=y CONFIG_SPL_SERIAL=y # CONFIG_SPL_DRIVERS_MISC is not set CONFIG_SPL_STACK_R_ADDR=0x82000000 CONFIG_SPL_SYS_MALLOC_F=y CONFIG_SPL_SYS_MALLOC_F_LEN=0x2000 CONFIG_ERR_PTR_OFFSET=0x0 CONFIG_SPL_SIZE_LIMIT=0x0 CONFIG_SPL=y CONFIG_BOOTSTAGE_STASH_ADDR=0x0 CONFIG_IDENT_STRING="" CONFIG_SYS_CLK_FREQ=0 # CONFIG_CHIP_DIP_SCAN is not set CONFIG_SPL_FS_FAT=y CONFIG_SPL_LIBDISK_SUPPORT=y # CONFIG_SPL_SPI is not set # CONFIG_HAS_ARMV7_SECURE_BASE is not set # CONFIG_ARMV7_LPAE is not set # CONFIG_CMD_DEKBLOB is not set # CONFIG_IMX_CAAM_DEK_ENCAP is not set # CONFIG_IMX_OPTEE_DEK_ENCAP is not set # CONFIG_IMX_SECO_DEK_ENCAP is not set # CONFIG_IMX_ELE_DEK_ENCAP is not set # CONFIG_CMD_HDMIDETECT is not set CONFIG_IMX_DCD_ADDR=0x00910000 CONFIG_SYS_MEM_TOP_HIDE=0x0 CONFIG_SYS_LOAD_ADDR=0x82000000 # # ARM debug # # CONFIG_DEBUG_LL is not set CONFIG_SPL_PAYLOAD="u-boot.img" CONFIG_BUILD_TARGET="" # CONFIG_PCI is not set CONFIG_FWU_NUM_BANKS=2 CONFIG_FWU_NUM_IMAGES_PER_BANK=2 # CONFIG_DEBUG_UART is not set # CONFIG_AHCI is not set # CONFIG_OF_BOARD_FIXUP is not set # # Functionality shared between NXP SoCs # # CONFIG_NXP_ESBC is not set # # General setup # CONFIG_LOCALVERSION="" CONFIG_LOCALVERSION_AUTO=y CONFIG_CC_IS_GCC=y CONFIG_GCC_VERSION=130300 CONFIG_CLANG_VERSION=0 # CONFIG_CC_OPTIMIZE_FOR_SIZE is not set # CONFIG_CC_OPTIMIZE_FOR_SPEED is not set CONFIG_CC_OPTIMIZE_FOR_DEBUG=y # CONFIG_OPTIMIZE_INLINING is not set # CONFIG_SPL_OPTIMIZE_INLINING is not set CONFIG_ARCH_SUPPORTS_LTO=y # CONFIG_LTO is not set CONFIG_CC_HAS_ASM_INLINE=y CONFIG_ENV_VARS_UBOOT_CONFIG=y # CONFIG_SYS_BOOT_GET_CMDLINE is not set # CONFIG_SYS_BOOT_GET_KBD is not set CONFIG_SYS_MALLOC_F=y # CONFIG_VALGRIND is not set CONFIG_EXPERT=y CONFIG_SYS_MALLOC_CLEAR_ON_INIT=y CONFIG_SPL_SYS_MALLOC_CLEAR_ON_INIT=y # CONFIG_SYS_MALLOC_DEFAULT_TO_INIT is not set # CONFIG_TOOLS_DEBUG is not set # CONFIG_PHYS_64BIT is not set # CONFIG_FDT_64BIT is not set CONFIG_SPL_IMAGE="spl/u-boot-spl.bin" # CONFIG_REMAKE_ELF is not set # CONFIG_HAS_BOARD_SIZE_LIMIT is not set # CONFIG_SYS_CUSTOM_LDSCRIPT is not set CONFIG_PLATFORM_ELFENTRY="_start" CONFIG_STACK_SIZE=0x1000000 CONFIG_SYS_SRAM_BASE=0x0 CONFIG_SYS_SRAM_SIZE=0x0 # CONFIG_MP is not set CONFIG_HAVE_TEXT_BASE=y # CONFIG_HAVE_SYS_UBOOT_START is not set CONFIG_SYS_UBOOT_START=0x80800000 # CONFIG_DYNAMIC_SYS_CLK_FREQ is not set # CONFIG_API is not set # # Boot options # # # Boot images # # CONFIG_ANDROID_BOOT_IMAGE is not set CONFIG_TIMESTAMP=y CONFIG_FIT=y CONFIG_FIT_EXTERNAL_OFFSET=0x0 CONFIG_FIT_FULL_CHECK=y # CONFIG_FIT_SIGNATURE is not set # CONFIG_FIT_CIPHER is not set # CONFIG_FIT_VERBOSE is not set # CONFIG_FIT_BEST_MATCH is not set CONFIG_FIT_PRINT=y CONFIG_SPL_FIT=y # CONFIG_SPL_FIT_PRINT is not set # CONFIG_SPL_FIT_FULL_CHECK is not set # CONFIG_SPL_FIT_SIGNATURE is not set CONFIG_SPL_LOAD_FIT=y CONFIG_SPL_LOAD_FIT_ADDRESS=0x0 # CONFIG_SPL_LOAD_FIT_APPLY_OVERLAY is not set # CONFIG_SPL_LOAD_FIT_FULL is not set # CONFIG_SPL_FIT_IMAGE_POST_PROCESS is not set CONFIG_SPL_FIT_SOURCE="" # CONFIG_USE_SPL_FIT_GENERATOR is not set CONFIG_PXE_UTILS=y CONFIG_BOOT_DEFAULTS_FEATURES=y CONFIG_BOOT_DEFAULTS_CMDS=y CONFIG_BOOT_DEFAULTS=y CONFIG_BOOTSTD=y # CONFIG_BOOTSTD_FULL is not set # CONFIG_BOOTSTD_DEFAULTS is not set # CONFIG_BOOTSTD_BOOTCOMMAND is not set CONFIG_BOOTMETH_GLOBAL=y # CONFIG_BOOTMETH_ANDROID is not set # CONFIG_BOOTMETH_CROS is not set CONFIG_BOOTMETH_EXTLINUX=y CONFIG_BOOTMETH_EXTLINUX_PXE=y CONFIG_BOOTMETH_EFILOADER=y CONFIG_BOOTMETH_VBE=y # CONFIG_SPL_BOOTMETH_VBE is not set CONFIG_BOOTMETH_VBE_REQUEST=y # CONFIG_SPL_BOOTMETH_VBE_REQUEST is not set CONFIG_BOOTMETH_VBE_SIMPLE=y CONFIG_BOOTMETH_VBE_SIMPLE_OS=y # CONFIG_SPL_BOOTMETH_VBE_SIMPLE is not set # CONFIG_BOOTMETH_SCRIPT is not set CONFIG_LEGACY_IMAGE_FORMAT=y CONFIG_SYS_BOOTM_LEN=0x1000000 CONFIG_SUPPORT_RAW_INITRD=y # CONFIG_CHROMEOS is not set # CONFIG_CHROMEOS_VBOOT is not set # CONFIG_RAMBOOT_PBL is not set CONFIG_SYS_BOOT_RAMDISK_HIGH=y CONFIG_DISTRO_DEFAULTS=y # # Boot timing # # CONFIG_BOOTSTAGE is not set CONFIG_BOOTSTAGE_STASH_SIZE=0x1000 # CONFIG_SHOW_BOOT_PROGRESS is not set # CONFIG_SPL_SHOW_BOOT_PROGRESS is not set # # Boot media # # CONFIG_NAND_BOOT is not set # CONFIG_ONENAND_BOOT is not set # CONFIG_QSPI_BOOT is not set # CONFIG_SATA_BOOT is not set # CONFIG_SD_BOOT is not set # CONFIG_SD_BOOT_QSPI is not set # CONFIG_SPI_BOOT is not set # # Autoboot options # CONFIG_AUTOBOOT=y CONFIG_BOOTDELAY=2 CONFIG_AUTOBOOT_KEYED=y # CONFIG_AUTOBOOT_FLUSH_STDIN is not set CONFIG_AUTOBOOT_PROMPT="Press SPACE to abort autoboot in %d seconds\n" # CONFIG_AUTOBOOT_ENCRYPTION is not set CONFIG_AUTOBOOT_DELAY_STR="d" CONFIG_AUTOBOOT_STOP_STR=" " # CONFIG_AUTOBOOT_KEYED_CTRLC is not set # CONFIG_BOOT_RETRY is not set # # Image support # # CONFIG_IMAGE_PRE_LOAD is not set # # Devicetree fixup # # CONFIG_OF_ENV_SETUP is not set CONFIG_OF_BOARD_SETUP=y # CONFIG_OF_SYSTEM_SETUP is not set # CONFIG_OF_STDOUT_VIA_ALIAS is not set # CONFIG_FDT_FIXUP_PARTITIONS is not set CONFIG_ARCH_FIXUP_FDT_MEMORY=y # CONFIG_USE_BOOTARGS is not set # CONFIG_BOOTARGS_SUBST is not set CONFIG_USE_BOOTCOMMAND=y CONFIG_BOOTCOMMAND="run findfdt; run init_console; run finduuid; run distro_bootcmd" # CONFIG_USE_PREBOOT is not set CONFIG_DEFAULT_FDT_FILE="" # CONFIG_SAVE_PREV_BL_FDT_ADDR is not set # CONFIG_SAVE_PREV_BL_INITRAMFS_START_ADDR is not set # # Configuration editor # # # Console # CONFIG_MENU=y # CONFIG_CONSOLE_RECORD is not set CONFIG_SYS_CBSIZE=1024 CONFIG_SYS_PBSIZE=1044 # CONFIG_DISABLE_CONSOLE is not set CONFIG_LOGLEVEL=7 CONFIG_SPL_LOGLEVEL=7 # CONFIG_SILENT_CONSOLE is not set # CONFIG_SPL_SILENT_CONSOLE is not set # CONFIG_TPL_SILENT_CONSOLE is not set # CONFIG_PRE_CONSOLE_BUFFER is not set CONFIG_CONSOLE_FLUSH_SUPPORT=y # CONFIG_CONSOLE_FLUSH_ON_NEWLINE is not set # CONFIG_CONSOLE_MUX is not set # CONFIG_SYS_CONSOLE_IS_IN_ENV is not set # CONFIG_SYS_CONSOLE_OVERWRITE_ROUTINE is not set CONFIG_SYS_CONSOLE_INFO_QUIET=y # CONFIG_SYS_STDIO_DEREGISTER is not set # CONFIG_SPL_SYS_STDIO_DEREGISTER is not set # CONFIG_SYS_DEVICE_NULLDEV is not set # # Logging # CONFIG_LOG=y CONFIG_LOG_MAX_LEVEL=6 CONFIG_LOG_DEFAULT_LEVEL=6 CONFIG_LOG_CONSOLE=y # CONFIG_LOGF_FILE is not set # CONFIG_LOGF_LINE is not set # CONFIG_LOGF_FUNC is not set CONFIG_LOGF_FUNC_PAD=20 # CONFIG_LOG_SYSLOG is not set CONFIG_SPL_LOG=y CONFIG_SPL_LOG_MAX_LEVEL=3 CONFIG_SPL_LOG_CONSOLE=y # CONFIG_LOG_ERROR_RETURN is not set # # Init options # # CONFIG_BOARD_TYPES is not set CONFIG_DISPLAY_CPUINFO=y CONFIG_DISPLAY_BOARDINFO=y # CONFIG_DISPLAY_BOARDINFO_LATE is not set # # Start-up hooks # # CONFIG_CYCLIC is not set CONFIG_EVENT=y CONFIG_EVENT_DYNAMIC=y # CONFIG_EVENT_DEBUG is not set CONFIG_ARCH_MISC_INIT=y # CONFIG_BOARD_EARLY_INIT_F is not set # CONFIG_BOARD_EARLY_INIT_R is not set # CONFIG_BOARD_POSTCLK_INIT is not set CONFIG_BOARD_LATE_INIT=y # CONFIG_CLOCKS is not set # CONFIG_HWCONFIG is not set CONFIG_LAST_STAGE_INIT=y # CONFIG_MISC_INIT_R is not set # CONFIG_SYS_MALLOC_BOOTPARAMS is not set # CONFIG_ID_EEPROM is not set # CONFIG_RESET_PHY_R is not set # # Security support # CONFIG_HASH=y CONFIG_SPL_HASH=y # CONFIG_STACKPROTECTOR is not set # CONFIG_BOARD_RNG_SEED is not set # # Update support # # CONFIG_UPDATE_TFTP is not set # CONFIG_ANDROID_AB is not set # # Blob list # # CONFIG_BLOBLIST is not set CONFIG_SUPPORT_SPL=y # # SPL configuration options # CONFIG_SPL_FRAMEWORK=y # CONFIG_SPL_FRAMEWORK_BOARD_INIT_F is not set CONFIG_SPL_MAX_SIZE=0x1b000 CONFIG_SPL_PAD_TO=0x1b000 CONFIG_SPL_HAS_BSS_LINKER_SECTION=y CONFIG_SPL_BSS_START_ADDR=0x80a00000 # CONFIG_SPL_NO_BSS_LIMIT is not set CONFIG_SPL_BSS_LIMIT=y # CONFIG_SPL_FOOTPRINT_LIMIT is not set CONFIG_SPL_BSS_MAX_SIZE=0x80000 CONFIG_SPL_SYS_STACK_F_CHECK_BYTE=0xaa # CONFIG_SPL_SYS_REPORT_STACK_F_USAGE is not set # CONFIG_SPL_SHOW_ERRORS is not set CONFIG_SPL_BOARD_INIT=y CONFIG_SPL_LOAD_BLOCK=y # CONFIG_SPL_BOOTROM_SUPPORT is not set # CONFIG_SPL_BOOTCOUNT_LIMIT is not set CONFIG_SPL_RAW_IMAGE_SUPPORT=y # CONFIG_SPL_LEGACY_IMAGE_FORMAT is not set # CONFIG_SPL_LOAD_IMX_CONTAINER is not set CONFIG_SPL_SYS_MALLOC_SIMPLE=y CONFIG_SPL_SHARES_INIT_SP_ADDR=y CONFIG_SPL_STACK_R=y CONFIG_SPL_STACK_R_MALLOC_SIMPLE_LEN=0x100000 CONFIG_SPL_SEPARATE_BSS=y CONFIG_SPL_SYS_MALLOC=y # CONFIG_SPL_HAS_CUSTOM_MALLOC_START is not set CONFIG_SPL_SYS_MALLOC_SIZE=0x800000 CONFIG_SPL_BANNER_PRINT=y # CONFIG_SPL_EARLY_BSS is not set # CONFIG_SPL_DISPLAY_PRINT is not set CONFIG_SPL_SYS_MMCSD_RAW_MODE=y CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_USE_SECTOR=y CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_SECTOR=0x300 CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_DATA_PART_OFFSET=0x0 # CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_USE_PARTITION is not set CONFIG_SPL_FIT_IMAGE_TINY=y # CONFIG_SPL_CACHE is not set # CONFIG_SPL_CPU is not set # CONFIG_SPL_CRYPTO is not set # CONFIG_SPL_DMA is not set CONFIG_SPL_ENV_SUPPORT=y # CONFIG_SPL_SAVEENV is not set CONFIG_SPL_FS_EXT4=y # CONFIG_SPL_FS_SQUASHFS is not set CONFIG_SPL_FS_FAT_DMA_ALIGN=y CONFIG_SPL_FS_LOAD_PAYLOAD_NAME="u-boot.img" CONFIG_SPL_FS_LOAD_KERNEL_NAME="uImage" CONFIG_SPL_FS_LOAD_ARGS_NAME="args" # CONFIG_SPL_FAT_WRITE is not set # CONFIG_SPL_FPGA is not set CONFIG_SPL_I2C=y # CONFIG_SPL_DM_MAILBOX is not set # CONFIG_SPL_MEMORY is not set CONFIG_SYS_MMCSD_FS_BOOT=y CONFIG_SYS_MMCSD_FS_BOOT_PARTITION=1 # CONFIG_SPL_MMC_TINY is not set # CONFIG_SPL_MMC_WRITE is not set # CONFIG_SPL_MPC8XXX_INIT_DDR is not set # CONFIG_SPL_MTD is not set # CONFIG_SPL_MUSB_NEW is not set # CONFIG_SPL_NAND_SUPPORT is not set # CONFIG_SPL_NAND_DRIVERS is not set # CONFIG_SPL_NAND_ECC is not set # CONFIG_SPL_NAND_SIMPLE is not set # CONFIG_SPL_UBI is not set # CONFIG_SPL_DM_SPI_FLASH is not set # CONFIG_SPL_NET is not set # CONFIG_SPL_NOR_SUPPORT is not set # CONFIG_SPL_XIP_SUPPORT is not set # CONFIG_SPL_ONENAND_SUPPORT is not set CONFIG_SPL_OS_BOOT=y CONFIG_SPL_PAYLOAD_ARGS_ADDR=0x88000000 # CONFIG_SPL_FALCON_BOOT_MMCSD is not set # CONFIG_SPL_PCI is not set # CONFIG_SPL_PCH is not set # CONFIG_SPL_POST_MEM_SUPPORT is not set # CONFIG_SPL_DM_RESET is not set CONFIG_SPL_POWER=y # CONFIG_SPL_POWER_DOMAIN is not set # CONFIG_SPL_RAM_SUPPORT is not set # CONFIG_SPL_REMOTEPROC is not set # CONFIG_SPL_RTC is not set # CONFIG_SPL_SATA is not set # CONFIG_SPL_NVME is not set # CONFIG_SPL_THERMAL is not set CONFIG_SPL_WATCHDOG=y CONFIG_SPL_YMODEM_SUPPORT=y CONFIG_SPL_AM33XX_ENABLE_RTC32K_OSC=y # CONFIG_SPL_OPTEE_IMAGE is not set CONFIG_SPL_TARGET="" # CONFIG_VPL is not set CONFIG_CMDLINE=y CONFIG_HUSH_PARSER=y # # Hush flavor to use # CONFIG_HUSH_OLD_PARSER=y # CONFIG_HUSH_MODERN_PARSER is not set CONFIG_CMDLINE_EDITING=y # CONFIG_CMDLINE_PS_SUPPORT is not set CONFIG_AUTO_COMPLETE=y CONFIG_SYS_LONGHELP=y CONFIG_SYS_PROMPT="=> " CONFIG_SYS_PROMPT_HUSH_PS2="> " CONFIG_SYS_MAXARGS=64 CONFIG_SYS_XTRACE=y # # Commands # # # Info commands # CONFIG_CMD_BDI=y # CONFIG_CMD_BDINFO_EXTRA is not set # CONFIG_CMD_CONFIG is not set CONFIG_CMD_CONSOLE=y # CONFIG_CMD_HISTORY is not set # CONFIG_CMD_LICENSE is not set # CONFIG_CMD_PMC is not set # CONFIG_CMD_SMBIOS is not set # # Boot commands # CONFIG_CMD_BOOTD=y CONFIG_CMD_BOOTM=y # CONFIG_CMD_BOOTDEV is not set CONFIG_CMD_BOOTFLOW=y # CONFIG_CMD_BOOTMETH is not set CONFIG_BOOTM_EFI=y CONFIG_CMD_BOOTZ=y CONFIG_BOOTM_LINUX=y CONFIG_BOOTM_NETBSD=y # CONFIG_BOOTM_OPENRTOS is not set # CONFIG_BOOTM_OSE is not set CONFIG_BOOTM_PLAN9=y CONFIG_BOOTM_RTEMS=y # CONFIG_CMD_VBE is not set CONFIG_BOOTM_VXWORKS=y CONFIG_CMD_BOOTEFI=y CONFIG_CMD_BOOTEFI_BINARY=y CONFIG_CMD_BOOTEFI_BOOTMGR=y CONFIG_CMD_BOOTEFI_HELLO_COMPILE=y # CONFIG_CMD_BOOTEFI_HELLO is not set # CONFIG_CMD_BOOTEFI_SELFTEST is not set # CONFIG_CMD_BOOTMENU is not set # CONFIG_CMD_ADTIMG is not set CONFIG_CMD_ELF=y CONFIG_CMD_FDT=y CONFIG_SUPPORT_EXTENSION_SCAN=y # CONFIG_CMD_EXTENSION is not set CONFIG_CMD_GO=y CONFIG_CMD_RUN=y CONFIG_CMD_IMI=y # CONFIG_CMD_IMLS is not set CONFIG_CMD_XIMG=y CONFIG_SYS_XIMG_LEN=0x800000 CONFIG_CMD_SPL=y CONFIG_CMD_SPL_WRITE_SIZE=0x2000 # CONFIG_CMD_ZBOOT is not set # # Environment commands # CONFIG_CMD_ASKENV=y CONFIG_CMD_EXPORTENV=y CONFIG_CMD_IMPORTENV=y CONFIG_CMD_EDITENV=y # CONFIG_CMD_GREPENV is not set CONFIG_CMD_SAVEENV=y # CONFIG_CMD_ERASEENV is not set CONFIG_CMD_ENV_EXISTS=y # CONFIG_CMD_ENV_CALLBACK is not set # CONFIG_CMD_ENV_FLAGS is not set # CONFIG_CMD_NVEDIT_EFI is not set # CONFIG_CMD_NVEDIT_INDIRECT is not set # CONFIG_CMD_NVEDIT_INFO is not set # CONFIG_CMD_NVEDIT_LOAD is not set # CONFIG_CMD_NVEDIT_SELECT is not set # # Memory commands # # CONFIG_CMD_BINOP is not set # CONFIG_CMD_BLOBLIST is not set CONFIG_CMD_CRC32=y # CONFIG_CRC32_VERIFY is not set # CONFIG_CMD_EEPROM is not set CONFIG_SYS_EEPROM_PAGE_WRITE_DELAY_MS=0 # CONFIG_LOOPW is not set # CONFIG_CMD_MD5SUM is not set # CONFIG_CMD_MEMINFO is not set CONFIG_CMD_MEMORY=y # CONFIG_CMD_MEM_SEARCH is not set # CONFIG_CMD_MX_CYCLIC is not set CONFIG_CMD_RANDOM=y # CONFIG_CMD_MEMTEST is not set # CONFIG_CMD_SHA1SUM is not set # CONFIG_CMD_STRINGS is not set # # Compression commands # # CONFIG_CMD_LZMADEC is not set # CONFIG_CMD_UNLZ4 is not set # CONFIG_CMD_UNZIP is not set # CONFIG_CMD_ZIP is not set # # Device access commands # # CONFIG_CMD_ARMFLASH is not set # CONFIG_CMD_BCB is not set # CONFIG_CMD_BIND is not set # CONFIG_CMD_CLK is not set # CONFIG_CMD_DEMO is not set # CONFIG_CMD_DFU is not set # CONFIG_CMD_DM is not set # CONFIG_CMD_FPGAD is not set # CONFIG_CMD_FUSE is not set CONFIG_CMD_GPIO=y # CONFIG_CMD_GPIO_READ is not set CONFIG_CMD_GPT=y # CONFIG_CMD_GPT_RENAME is not set # CONFIG_CMD_IDE is not set # CONFIG_CMD_IO is not set # CONFIG_CMD_IOTRACE is not set CONFIG_CMD_I2C=y CONFIG_CMD_LOADB=y # CONFIG_CMD_LOADM is not set CONFIG_CMD_LOADS=y # CONFIG_LOADS_ECHO is not set # CONFIG_CMD_SAVES is not set # CONFIG_SYS_LOADS_BAUD_CHANGE is not set CONFIG_CMD_LOADXY_TIMEOUT=90 # CONFIG_CMD_LSBLK is not set # CONFIG_CMD_MBR is not set CONFIG_CMD_MMC=y # CONFIG_CMD_BKOPS_ENABLE is not set # CONFIG_CMD_MMC_REG is not set # CONFIG_CMD_MMC_SWRITE is not set # CONFIG_CMD_CLONE is not set # CONFIG_CMD_OSD is not set CONFIG_CMD_PART=y # CONFIG_CMD_PCI is not set # CONFIG_CMD_POWEROFF is not set # CONFIG_CMD_READ is not set # CONFIG_CMD_SATA is not set # CONFIG_CMD_SDRAM is not set CONFIG_CMD_SPI=y CONFIG_DEFAULT_SPI_BUS=0 CONFIG_DEFAULT_SPI_MODE=0x0 # CONFIG_CMD_TSI148 is not set # CONFIG_CMD_UNIVERSE is not set # CONFIG_CMD_USB_SDP is not set # CONFIG_CMD_RKMTD is not set # CONFIG_CMD_WRITE is not set # # Shell scripting commands # # CONFIG_CMD_CAT is not set CONFIG_CMD_ECHO=y CONFIG_CMD_ITEST=y CONFIG_CMD_SOURCE=y # CONFIG_CMD_SETEXPR is not set # CONFIG_CMD_XXD is not set # # Android support commands # CONFIG_CMD_NET=y CONFIG_CMD_BOOTP=y CONFIG_CMD_DHCP=y # CONFIG_BOOTP_MAY_FAIL is not set CONFIG_BOOTP_BOOTPATH=y # CONFIG_BOOTP_VENDOREX is not set # CONFIG_BOOTP_BOOTFILESIZE is not set CONFIG_BOOTP_DNS=y # CONFIG_BOOTP_DNS2 is not set CONFIG_BOOTP_GATEWAY=y CONFIG_BOOTP_HOSTNAME=y # CONFIG_BOOTP_PREFER_SERVERIP is not set CONFIG_BOOTP_SUBNETMASK=y # CONFIG_BOOTP_NISDOMAIN is not set # CONFIG_BOOTP_NTPSERVER is not set # CONFIG_CMD_PCAP is not set CONFIG_BOOTP_PXE=y CONFIG_BOOTP_PXE_CLIENTARCH=0x15 # CONFIG_BOOTP_PXE_DHCP_OPTION is not set CONFIG_BOOTP_VCI_STRING="U-Boot.armv7" CONFIG_CMD_TFTPBOOT=y # CONFIG_CMD_TFTPPUT is not set # CONFIG_CMD_TFTPSRV is not set CONFIG_NET_TFTP_VARS=y # CONFIG_CMD_RARP is not set # CONFIG_CMD_NFS is not set # CONFIG_SYS_DISABLE_AUTOLOAD is not set # CONFIG_CMD_WGET is not set CONFIG_CMD_MII=y CONFIG_CMD_MDIO=y CONFIG_CMD_PING=y # CONFIG_CMD_CDP is not set # CONFIG_CMD_SNTP is not set # CONFIG_CMD_DNS is not set # CONFIG_CMD_LINK_LOCAL is not set # CONFIG_CMD_ETHSW is not set CONFIG_CMD_PXE=y # CONFIG_CMD_WOL is not set # # Misc commands # # CONFIG_CMD_2048 is not set # CONFIG_CMD_BSP is not set CONFIG_CMD_BLOCK_CACHE=y # CONFIG_CMD_CACHE is not set # CONFIG_CMD_CONITRACE is not set # CONFIG_CMD_CLS is not set # CONFIG_CMD_EFIDEBUG is not set CONFIG_CMD_EFICONFIG=y # CONFIG_CMD_EXCEPTION is not set # CONFIG_CMD_INI is not set # CONFIG_CMD_DATE is not set CONFIG_CMD_TIME=y # CONFIG_CMD_GETTIME is not set # CONFIG_CMD_PAUSE is not set CONFIG_CMD_SLEEP=y # CONFIG_CMD_TIMER is not set CONFIG_CMD_SYSBOOT=y # CONFIG_CMD_QFW is not set # CONFIG_CMD_PSTORE is not set # CONFIG_CMD_TERMINAL is not set # CONFIG_CMD_UUID is not set # # TI specific command line interface # # CONFIG_CMD_DDRSS is not set # # Power commands # CONFIG_CMD_PMIC=y # # Security commands # # CONFIG_CMD_AES is not set # CONFIG_CMD_BLOB is not set # CONFIG_CMD_HASH is not set # # Firmware commands # # # Filesystem commands # # CONFIG_CMD_BTRFS is not set # CONFIG_CMD_EROFS is not set CONFIG_CMD_EXT2=y CONFIG_CMD_EXT4=y CONFIG_CMD_EXT4_WRITE=y CONFIG_CMD_FAT=y # CONFIG_CMD_SQUASHFS is not set CONFIG_CMD_FS_GENERIC=y # CONFIG_CMD_FS_UUID is not set # CONFIG_CMD_JFFS2 is not set # CONFIG_CMD_REISER is not set # CONFIG_CMD_ZFS is not set # # Debug commands # # CONFIG_CMD_DIAG is not set # CONFIG_CMD_EVENT is not set # CONFIG_CMD_LOG is not set # CONFIG_CMD_UBI is not set # CONFIG_MMC_SPEED_MODE_SET is not set # # Partition Types # CONFIG_PARTITIONS=y CONFIG_SPL_PARTITIONS=y # CONFIG_MAC_PARTITION is not set # CONFIG_SPL_MAC_PARTITION is not set CONFIG_DOS_PARTITION=y CONFIG_SPL_DOS_PARTITION=y CONFIG_ISO_PARTITION=y # CONFIG_SPL_ISO_PARTITION is not set # CONFIG_AMIGA_PARTITION is not set # CONFIG_SPL_AMIGA_PARTITION is not set CONFIG_EFI_PARTITION=y CONFIG_EFI_PARTITION_ENTRIES_NUMBERS=128 CONFIG_EFI_PARTITION_ENTRIES_OFF=0 CONFIG_SPL_EFI_PARTITION=y CONFIG_PARTITION_UUIDS=y CONFIG_SPL_PARTITION_UUIDS=y # CONFIG_PARTITION_TYPE_GUID is not set # CONFIG_SPL_PARTITION_TYPE_GUID is not set CONFIG_SUPPORT_OF_CONTROL=y # # Device Tree Control # CONFIG_OF_CONTROL=y CONFIG_OF_REAL=y # CONFIG_SPL_OF_CONTROL is not set # CONFIG_OF_LIVE is not set # CONFIG_OF_SEPARATE is not set CONFIG_OF_EMBED=y # CONFIG_OF_BOARD is not set # CONFIG_OF_OMIT_DTB is not set CONFIG_DEVICE_TREE_INCLUDES="" CONFIG_OF_LIST="am335x-evm am335x-bone am335x-sancloud-bbe am335x-sancloud-bbe-lite am335x-sancloud-bbe-extended-wifi am335x-boneblack am335x-evmsk am335x-bonegreen am335x-icev2 am335x-pocketbeagle am335x-mlsl-v11" # CONFIG_MULTI_DTB_FIT is not set CONFIG_OF_TAG_MIGRATE=y # CONFIG_OF_DTB_PROPS_REMOVE is not set # # Environment # CONFIG_ENV_SUPPORT=y CONFIG_SAVEENV=y CONFIG_ENV_OVERWRITE=y CONFIG_ENV_MIN_ENTRIES=64 CONFIG_ENV_MAX_ENTRIES=512 # CONFIG_ENV_IS_NOWHERE is not set # CONFIG_ENV_IS_IN_EEPROM is not set CONFIG_ENV_IS_IN_FAT=y # CONFIG_ENV_IS_IN_EXT4 is not set # CONFIG_ENV_IS_IN_FLASH is not set # CONFIG_ENV_IS_IN_MMC is not set # CONFIG_ENV_IS_IN_NAND is not set # CONFIG_ENV_IS_IN_NVRAM is not set # CONFIG_ENV_IS_IN_ONENAND is not set # CONFIG_ENV_IS_IN_REMOTE is not set # CONFIG_SYS_REDUNDAND_ENVIRONMENT is not set CONFIG_ENV_FAT_INTERFACE="mmc" CONFIG_ENV_FAT_DEVICE_AND_PART="0:1" CONFIG_ENV_FAT_FILE="uEnv.txt" CONFIG_SYS_RELOC_GD_ENV_ADDR=y CONFIG_SYS_MMC_ENV_DEV=0 CONFIG_SYS_MMC_ENV_PART=0 # CONFIG_USE_DEFAULT_ENV_FILE is not set # CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG is not set # CONFIG_ENV_IMPORT_FDT is not set # CONFIG_ENV_APPEND is not set # CONFIG_ENV_WRITEABLE_LIST is not set # CONFIG_ENV_ACCESS_IGNORE_FORCE is not set CONFIG_SPL_ENV_IS_NOWHERE=y # CONFIG_USE_BOOTFILE is not set # CONFIG_USE_ETHPRIME is not set # CONFIG_USE_HOSTNAME is not set CONFIG_VERSION_VARIABLE=y CONFIG_NET=y CONFIG_ARP_TIMEOUT=5000 CONFIG_NET_RETRY_COUNT=5 # CONFIG_PROT_UDP is not set CONFIG_BOOTDEV_ETH=y # CONFIG_BOOTP_SEND_HOSTNAME is not set # CONFIG_NET_RANDOM_ETHADDR is not set # CONFIG_NETCONSOLE is not set # CONFIG_IP_DEFRAG is not set # CONFIG_SYS_FAULT_ECHO_LINK_DOWN is not set CONFIG_TFTP_BLOCKSIZE=1468 # CONFIG_TFTP_PORT is not set CONFIG_TFTP_WINDOWSIZE=1 CONFIG_TFTP_TSIZE=y # CONFIG_SERVERIP_FROM_PROXYDHCP is not set CONFIG_SERVERIP_FROM_PROXYDHCP_DELAY_MS=100 # CONFIG_KEEP_SERVERADDR is not set # CONFIG_UDP_CHECKSUM is not set # CONFIG_BOOTP_SERVERIP is not set CONFIG_BOOTP_MAX_ROOT_PATH_LEN=64 # CONFIG_USE_GATEWAYIP is not set # CONFIG_USE_IPADDR is not set # CONFIG_USE_NETMASK is not set # CONFIG_USE_ROOTPATH is not set # CONFIG_USE_SERVERIP is not set # CONFIG_PROT_TCP is not set # CONFIG_IPV6 is not set CONFIG_SYS_RX_ETH_BUFFER=4 # # Device Drivers # # # Generic Driver Options # CONFIG_DM=y CONFIG_SPL_DM=y # CONFIG_DM_WARN is not set # CONFIG_SPL_DM_WARN is not set # CONFIG_DM_DEBUG is not set # CONFIG_DM_STATS is not set # CONFIG_SPL_DM_STATS is not set CONFIG_DM_DEVICE_REMOVE=y CONFIG_DM_EVENT=y # CONFIG_SPL_DM_DEVICE_REMOVE is not set CONFIG_DM_STDIO=y CONFIG_DM_SEQ_ALIAS=y CONFIG_SPL_DM_SEQ_ALIAS=y CONFIG_SPL_DM_INLINE_OFNODE=y # CONFIG_DM_DMA is not set # CONFIG_REGMAP is not set # CONFIG_SPL_REGMAP is not set # CONFIG_DEVRES is not set CONFIG_SIMPLE_BUS=y # CONFIG_SIMPLE_BUS_CORRECT_RANGE is not set CONFIG_OF_TRANSLATE=y # CONFIG_TRANSLATION_OFFSET is not set CONFIG_DM_DEV_READ_INLINE=y # CONFIG_OFNODE_MULTI_TREE is not set # CONFIG_BOUNCE_BUFFER is not set # CONFIG_ADC is not set # CONFIG_ADC_EXYNOS is not set # CONFIG_ADC_SANDBOX is not set # CONFIG_SARADC_MESON is not set # CONFIG_SARADC_ROCKCHIP is not set # CONFIG_SATA is not set # CONFIG_SCSI_AHCI is not set # # SATA/SCSI device support # # CONFIG_AXI is not set # # Bus devices # CONFIG_TI_SYSC=y # CONFIG_SPL_TI_SYSC is not set CONFIG_BLK=y CONFIG_SPL_LEGACY_BLOCK=y CONFIG_SPL_BLK=y CONFIG_BLOCK_CACHE=y # CONFIG_BLKMAP is not set # CONFIG_SPL_BLOCK_CACHE is not set # CONFIG_EFI_MEDIA is not set # CONFIG_SPL_BLK_FS is not set # CONFIG_IDE is not set # CONFIG_LBA48 is not set # CONFIG_SYS_64BIT_LBA is not set # CONFIG_RKMTD is not set # CONFIG_BOOTCOUNT_LIMIT is not set # # Button Support # # CONFIG_BUTTON is not set # # Cache Controller drivers # # CONFIG_CACHE is not set # CONFIG_L2X0_CACHE is not set # CONFIG_V5L2_CACHE is not set # CONFIG_NCORE_CACHE is not set # CONFIG_SIFIVE_CCACHE is not set # CONFIG_SIFIVE_PL2 is not set # # Clock # # CONFIG_CLK is not set # CONFIG_SPL_CLK_CCF is not set # CONFIG_CLK_CCF is not set # CONFIG_CLK_RCAR is not set # CONFIG_CLK_RCAR_CPG_LIB is not set # CONFIG_CPU is not set # # Hardware crypto devices # # CONFIG_DM_HASH is not set # CONFIG_FSL_CAAM is not set # CONFIG_SYS_FSL_SEC_BE is not set # CONFIG_SYS_FSL_SEC_LE is not set # CONFIG_NPCM_AES is not set # CONFIG_NPCM_SHA is not set # CONFIG_DDR_SPD is not set # CONFIG_IMX_SNPS_DDR_PHY is not set # # Demo for driver model # # CONFIG_DM_DEMO is not set # # DFU support # # # DMA Support # # CONFIG_DMA is not set # CONFIG_DMA_LPC32XX is not set # CONFIG_TI_EDMA3 is not set # CONFIG_DMA_LEGACY is not set # # Extcon Support # # CONFIG_EXTCON is not set # # Fastboot support # # CONFIG_UDP_FUNCTION_FASTBOOT is not set # CONFIG_TCP_FUNCTION_FASTBOOT is not set # CONFIG_FIRMWARE is not set # CONFIG_ZYNQMP_FIRMWARE is not set # CONFIG_DM_FUZZING_ENGINE is not set # # FPGA support # # CONFIG_FPGA_ALTERA is not set # CONFIG_FPGA_SOCFPGA is not set # CONFIG_FPGA_LATTICE is not set # CONFIG_FPGA_XILINX is not set # CONFIG_DM_FPGA is not set # CONFIG_FWU_MDATA is not set CONFIG_GPIO=y CONFIG_SPL_DM_GPIO=y # CONFIG_GPIO_HOG is not set # CONFIG_SPL_GPIO_HOG is not set # CONFIG_DM_GPIO_LOOKUP_LABEL is not set # CONFIG_SPL_DM_GPIO_LOOKUP_LABEL is not set # CONFIG_ALTERA_PIO is not set # CONFIG_BCM2835_GPIO is not set # CONFIG_DWAPB_GPIO is not set # CONFIG_AT91_GPIO is not set # CONFIG_ATMEL_PIO4 is not set # CONFIG_ASPEED_GPIO is not set # CONFIG_DA8XX_GPIO is not set # CONFIG_FXL6408_GPIO is not set # CONFIG_HIKEY_GPIO is not set # CONFIG_INTEL_BROADWELL_GPIO is not set # CONFIG_INTEL_GPIO is not set # CONFIG_INTEL_ICH6_GPIO is not set # CONFIG_IMX_RGPIO2P is not set # CONFIG_IPROC_GPIO is not set # CONFIG_HSDK_CREG_GPIO is not set # CONFIG_KIRKWOOD_GPIO is not set # CONFIG_LPC32XX_GPIO is not set # CONFIG_MAX7320_GPIO is not set # CONFIG_MCP230XX_GPIO is not set # CONFIG_MSM_GPIO is not set # CONFIG_MXC_GPIO is not set # CONFIG_MXS_GPIO is not set # CONFIG_NPCM_GPIO is not set CONFIG_OMAP_GPIO=y # CONFIG_CMD_PCA953X is not set # CONFIG_PCF8575_GPIO is not set # CONFIG_ROCKCHIP_GPIO is not set # CONFIG_XILINX_GPIO is not set # CONFIG_TCA642X is not set # CONFIG_TEGRA_GPIO is not set # CONFIG_TEGRA186_GPIO is not set # CONFIG_VYBRID_GPIO is not set # CONFIG_SIFIVE_GPIO is not set # CONFIG_ZYNQ_GPIO is not set # CONFIG_DM_74X164 is not set # CONFIG_DM_PCA953X is not set # CONFIG_SPL_DM_PCA953X is not set # CONFIG_PCA953X is not set # CONFIG_MPC8XXX_GPIO is not set # CONFIG_MPC8XX_GPIO is not set # CONFIG_NX_GPIO is not set # CONFIG_NOMADIK_GPIO is not set # CONFIG_ZYNQMP_GPIO_MODEPIN is not set # CONFIG_SLG7XL45106_I2C_GPO is not set # CONFIG_TURRIS_OMNIA_MCU is not set # CONFIG_FTGPIO010 is not set # CONFIG_ADP5585_GPIO is not set # # Hardware Spinlock Support # # CONFIG_DM_HWSPINLOCK is not set CONFIG_I2C=y CONFIG_DM_I2C=y CONFIG_SPL_DM_I2C=y # CONFIG_I2C_SET_DEFAULT_BUS_NUM is not set # CONFIG_DM_I2C_GPIO is not set # CONFIG_SYS_I2C_IPROC is not set # CONFIG_SYS_I2C_FSL is not set # CONFIG_SYS_I2C_CADENCE is not set # CONFIG_SYS_I2C_DW is not set # CONFIG_SYS_I2C_INTEL is not set # CONFIG_SYS_I2C_IMX_LPI2C is not set # CONFIG_SYS_I2C_MTK is not set # CONFIG_SYS_I2C_MICROCHIP is not set # CONFIG_SYS_I2C_MXC is not set # CONFIG_SYS_I2C_NEXELL is not set # CONFIG_SYS_I2C_NPCM is not set # CONFIG_SYS_I2C_OCORES is not set CONFIG_SYS_I2C_OMAP24XX=y # CONFIG_SYS_I2C_ROCKCHIP is not set # CONFIG_SYS_I2C_SOFT is not set # CONFIG_SYS_I2C_MV is not set # CONFIG_SYS_I2C_MVTWSI is not set CONFIG_SYS_I2C_BUS_MAX=3 # CONFIG_SYS_I2C_XILINX_XIIC is not set # CONFIG_SYS_I2C_IHS is not set # CONFIG_I2C_MUX is not set CONFIG_INPUT=y # CONFIG_SPL_INPUT is not set # CONFIG_DM_KEYBOARD is not set # CONFIG_SPL_DM_KEYBOARD is not set # CONFIG_CROS_EC_KEYB is not set # CONFIG_TEGRA_KEYBOARD is not set # CONFIG_TWL4030_INPUT is not set # # IOMMU device drivers # # CONFIG_IOMMU is not set # # LED Support # # CONFIG_LED is not set # CONFIG_SPL_LED is not set # CONFIG_LED_STATUS is not set # # Mailbox Controller Support # # CONFIG_DM_MAILBOX is not set # # Memory Controller drivers # # CONFIG_MEMORY is not set # CONFIG_ATMEL_EBI is not set # CONFIG_MFD_ATMEL_SMC is not set # # Multifunction device drivers # # CONFIG_MISC is not set # CONFIG_SPL_MISC is not set # CONFIG_NVMEM is not set # CONFIG_SPL_NVMEM is not set # CONFIG_SMSC_LPC47M is not set # CONFIG_SMSC_SIO1007 is not set # CONFIG_CROS_EC is not set # CONFIG_DS4510 is not set # CONFIG_FSL_SEC_MON is not set # CONFIG_IRQ is not set # CONFIG_NUVOTON_NCT6102D is not set # CONFIG_PWRSEQ is not set # CONFIG_PCA9551_LED is not set # CONFIG_TEST_DRV is not set # CONFIG_USB_HUB_USB251XB is not set # CONFIG_TWL4030_LED is not set # CONFIG_WINBOND_W83627 is not set # CONFIG_FS_LOADER is not set # CONFIG_SPL_FS_LOADER is not set # CONFIG_ESM_PMIC is not set # CONFIG_SL28CPLD is not set # # MMC Host controller Support # CONFIG_MMC=y CONFIG_MMC_WRITE=y # CONFIG_MMC_BROKEN_CD is not set CONFIG_DM_MMC=y CONFIG_SPL_DM_MMC=y # CONFIG_MMC_SPI is not set # CONFIG_ARM_PL180_MMCI is not set CONFIG_MMC_QUIRKS=y CONFIG_SYS_MMC_MAX_BLK_COUNT=65535 CONFIG_MMC_HW_PARTITIONING=y # CONFIG_SUPPORT_EMMC_RPMB is not set # CONFIG_SUPPORT_EMMC_BOOT is not set # CONFIG_MMC_IO_VOLTAGE is not set # CONFIG_SPL_MMC_IO_VOLTAGE is not set # CONFIG_MMC_HS400_ES_SUPPORT is not set # CONFIG_SPL_MMC_HS400_ES_SUPPORT is not set # CONFIG_MMC_HS400_SUPPORT is not set # CONFIG_SPL_MMC_HS400_SUPPORT is not set # CONFIG_MMC_HS200_SUPPORT is not set # CONFIG_SPL_MMC_HS200_SUPPORT is not set CONFIG_MMC_VERBOSE=y # CONFIG_MMC_TRACE is not set # CONFIG_MMC_DW is not set # CONFIG_MMC_MXC is not set CONFIG_MMC_OMAP_HS=y # CONFIG_MMC_OMAP_HS_ADMA is not set # CONFIG_HSMMC2_8BIT is not set # CONFIG_MMC_SDHCI is not set # CONFIG_MMC_PITON is not set # CONFIG_STM32_SDMMC2 is not set # CONFIG_FTSDC010 is not set # CONFIG_FSL_ESDHC is not set # CONFIG_FSL_ESDHC_IMX is not set # # MTD Support # # CONFIG_MTD is not set # # Multiplexer drivers # # CONFIG_MULTIPLEXER is not set # CONFIG_BITBANGMII is not set # CONFIG_MV88E6352_SWITCH is not set CONFIG_PHYLIB=y # CONFIG_PHY_ADDR_ENABLE is not set # CONFIG_B53_SWITCH is not set # CONFIG_MV88E61XX_SWITCH is not set # CONFIG_PHYLIB_10G is not set # CONFIG_PHY_ADIN is not set # CONFIG_PHY_AQUANTIA is not set # CONFIG_PHY_ATHEROS is not set # CONFIG_SPL_PHY_ATHEROS is not set # CONFIG_PHY_BROADCOM is not set # CONFIG_PHY_CORTINA is not set # CONFIG_PHY_DAVICOM is not set # CONFIG_PHY_ET1011C is not set # CONFIG_PHY_LXT is not set # CONFIG_PHY_MARVELL is not set # CONFIG_PHY_MARVELL_10G is not set # CONFIG_PHY_MESON_GXL is not set # CONFIG_PHY_MICREL is not set # CONFIG_PHY_MOTORCOMM is not set # CONFIG_PHY_MSCC is not set # CONFIG_PHY_NATSEMI is not set # CONFIG_PHY_NXP_C45_TJA11XX is not set # CONFIG_PHY_NXP_TJA11XX is not set # CONFIG_PHY_REALTEK is not set # CONFIG_PHY_SMSC is not set # CONFIG_PHY_TERANETICS is not set # CONFIG_PHY_TI is not set # CONFIG_PHY_TI_DP83867 is not set # CONFIG_PHY_TI_DP83869 is not set # CONFIG_PHY_TI_GENERIC is not set # CONFIG_PHY_VITESSE is not set # CONFIG_PHY_XILINX is not set # CONFIG_PHY_XILINX_GMII2RGMII is not set # CONFIG_PHY_XWAY is not set # CONFIG_PHY_ETHERNET_ID is not set # CONFIG_PHY_FIXED is not set # CONFIG_PHY_NCSI is not set # CONFIG_FSL_MEMAC is not set CONFIG_PHY_RESET_DELAY=0 # CONFIG_FSL_PFE is not set CONFIG_ETH=y CONFIG_DM_ETH=y # CONFIG_DM_MDIO is not set # CONFIG_DM_ETH_PHY is not set CONFIG_NETDEVICES=y # CONFIG_PHY_GIGE is not set # CONFIG_ALTERA_TSE is not set # CONFIG_BCM_SF2_ETH is not set # CONFIG_BCMGENET is not set # CONFIG_BNXT_ETH is not set # CONFIG_CALXEDA_XGMAC is not set # CONFIG_DRIVER_DM9000 is not set # CONFIG_DWC_ETH_QOS is not set # CONFIG_EEPRO100 is not set # CONFIG_ETH_DESIGNWARE is not set # CONFIG_ETH_DESIGNWARE_MESON8B is not set # CONFIG_ETHOC is not set # CONFIG_FMAN_ENET is not set # CONFIG_FTMAC100 is not set # CONFIG_FTGMAC100 is not set # CONFIG_MCFFEC is not set # CONFIG_KS8851_MLL is not set # CONFIG_LITEETH is not set # CONFIG_MACB is not set # CONFIG_NET_NPCM750 is not set # CONFIG_PCH_GBE is not set # CONFIG_RGMII is not set # CONFIG_MII is not set # CONFIG_RMII is not set # CONFIG_PCNET is not set # CONFIG_QE_UEC is not set # CONFIG_RTL8139 is not set # CONFIG_SMC911X is not set # CONFIG_SUN7I_GMAC is not set # CONFIG_SUN4I_EMAC is not set # CONFIG_SUN8I_EMAC is not set # CONFIG_SH_ETHER is not set CONFIG_DRIVER_TI_CPSW=y # CONFIG_DRIVER_TI_EMAC is not set # CONFIG_DRIVER_TI_KEYSTONE_NET is not set # CONFIG_TULIP is not set # CONFIG_XILINX_AXIEMAC is not set # CONFIG_VSC7385_ENET is not set # CONFIG_XILINX_EMACLITE is not set # CONFIG_ZYNQ_GEM is not set # CONFIG_SYS_DPAA_QBMAN is not set # CONFIG_TSEC_ENET is not set # CONFIG_MEDIATEK_ETH is not set # CONFIG_HIFEMAC_ETH is not set # CONFIG_HIGMACV300_ETH is not set # CONFIG_NVME is not set # CONFIG_NVME_APPLE is not set # # PCI Endpoint # # CONFIG_PCI_ENDPOINT is not set # CONFIG_X86_PCH7 is not set # CONFIG_X86_PCH9 is not set # # PHY Subsystem # # CONFIG_PHY is not set # CONFIG_SPL_PHY is not set # CONFIG_MIPI_DPHY_HELPERS is not set # # Rockchip PHY driver # # CONFIG_MVEBU_COMPHY_SUPPORT is not set # # Pin controllers # # CONFIG_PINCTRL is not set # CONFIG_SPL_PINCTRL is not set # CONFIG_PINCTRL_TEGRA is not set CONFIG_POWER=y # CONFIG_POWER_LEGACY is not set # CONFIG_SPL_POWER_LEGACY is not set # CONFIG_ACPI_PMC is not set # CONFIG_SPL_ACPI_PMC is not set # # Power Domain Support # # CONFIG_POWER_DOMAIN is not set CONFIG_DM_PMIC=y # CONFIG_SPL_DM_PMIC is not set CONFIG_PMIC_CHILDREN=y # CONFIG_PMIC_AB8500 is not set # CONFIG_PMIC_ACT8846 is not set # CONFIG_PMIC_AXP is not set # CONFIG_DM_PMIC_DA9063 is not set # CONFIG_PMIC_AS3722 is not set # CONFIG_DM_PMIC_BD71837 is not set # CONFIG_DM_PMIC_MP5416 is not set # CONFIG_DM_PMIC_PCA9450 is not set # CONFIG_DM_PMIC_PFUZE100 is not set # CONFIG_DM_PMIC_MAX77663 is not set # CONFIG_DM_PMIC_MAX77686 is not set # CONFIG_DM_PMIC_MAX8998 is not set # CONFIG_DM_PMIC_MC34708 is not set # CONFIG_PMIC_MAX8997 is not set # CONFIG_PMIC_QCOM is not set # CONFIG_PMIC_RK8XX is not set # CONFIG_PMIC_S2MPS11 is not set # CONFIG_DM_PMIC_SANDBOX is not set # CONFIG_PMIC_S5M8767 is not set # CONFIG_PMIC_RN5T567 is not set # CONFIG_PMIC_TPS65090 is not set # CONFIG_PMIC_PALMAS is not set # CONFIG_PMIC_LP873X is not set # CONFIG_PMIC_LP87565 is not set # CONFIG_DM_PMIC_TPS65910 is not set # CONFIG_DM_PMIC_TPS80031 is not set # CONFIG_PMIC_STPMIC1 is not set # CONFIG_PMIC_TPS65941 is not set # CONFIG_PMIC_TPS65219 is not set # CONFIG_PMIC_RAA215300 is not set CONFIG_PMIC_TPS65217=y # CONFIG_POWER_TPS65218 is not set # CONFIG_POWER_TPS62362 is not set # CONFIG_SPL_POWER_TPS62362 is not set CONFIG_SPL_POWER_TPS65910=y # CONFIG_DM_REGULATOR is not set # CONFIG_TPS6586X_POWER is not set # CONFIG_POWER_MT6323 is not set # CONFIG_DM_PWM is not set # CONFIG_PWM_IMX is not set # CONFIG_PWM_SANDBOX is not set # CONFIG_U_QE is not set # CONFIG_RAM is not set # # Reboot Mode Support # # CONFIG_DM_REBOOT_MODE is not set # # Remote Processor drivers # CONFIG_REMOTEPROC_MAX_FW_SIZE=0x10000 # # Reset Controller Support # # CONFIG_RESET_SCMI is not set # CONFIG_DM_RNG is not set # # Real Time Clock # # CONFIG_DM_RTC is not set # CONFIG_SPL_DM_RTC is not set # CONFIG_RTC_ENABLE_32KHZ_OUTPUT is not set # CONFIG_RTC_DS1337 is not set # CONFIG_RTC_DS1338 is not set # CONFIG_RTC_DS1374 is not set # CONFIG_RTC_DS3231 is not set # CONFIG_RTC_PCF8563 is not set # CONFIG_RTC_PT7C4338 is not set # CONFIG_RTC_PL031 is not set # CONFIG_RTC_S35392A is not set # CONFIG_RTC_MC13XXX is not set # CONFIG_RTC_MC146818 is not set # CONFIG_RTC_M41T62 is not set # CONFIG_RTC_DAVINCI is not set # CONFIG_SCSI is not set CONFIG_SERIAL=y CONFIG_BAUDRATE=115200 # CONFIG_OF_SERIAL_BAUD is not set # CONFIG_DEFAULT_ENV_IS_RW is not set CONFIG_REQUIRE_SERIAL_CONSOLE=y CONFIG_SPECIFY_CONSOLE_INDEX=y CONFIG_SERIAL_PRESENT=y CONFIG_SPL_SERIAL_PRESENT=y CONFIG_DM_SERIAL=y # CONFIG_SERIAL_RX_BUFFER is not set # CONFIG_SERIAL_PUTS is not set # CONFIG_SERIAL_SEARCH_ALL is not set # CONFIG_SERIAL_PROBE_ALL is not set CONFIG_SPL_DM_SERIAL=y # CONFIG_VPL_DM_SERIAL is not set # CONFIG_ALTERA_JTAG_UART is not set # CONFIG_ALTERA_UART is not set # CONFIG_ARC_SERIAL is not set # CONFIG_ARM_DCC is not set # CONFIG_ATMEL_USART is not set # CONFIG_BCM6345_SERIAL is not set # CONFIG_COREBOOT_SERIAL is not set # CONFIG_CORTINA_UART is not set # CONFIG_FSL_LINFLEXUART is not set # CONFIG_FSL_LPUART is not set # CONFIG_MVEBU_A3700_UART is not set # CONFIG_MCFUART is not set # CONFIG_NULLDEV_SERIAL is not set CONFIG_SYS_NS16550=y # CONFIG_NS16550_DYNAMIC is not set # CONFIG_SYS_NS16550_MEM32 is not set # CONFIG_SYS_NS16550_PORT_MAPPED is not set # CONFIG_PL01X_SERIAL is not set # CONFIG_ROCKCHIP_SERIAL is not set # CONFIG_XILINX_UARTLITE is not set # CONFIG_MSM_SERIAL is not set # CONFIG_MSM_GENI_SERIAL is not set # CONFIG_MXS_AUART_SERIAL is not set CONFIG_OMAP_SERIAL=y # CONFIG_SIFIVE_SERIAL is not set # CONFIG_ZYNQ_SERIAL is not set # CONFIG_MTK_SERIAL is not set # CONFIG_MT7620_SERIAL is not set # CONFIG_NPCM_SERIAL is not set # CONFIG_SM is not set # CONFIG_MESON_SM is not set # CONFIG_SMEM is not set # # Sound support # # CONFIG_SOUND is not set # # SOC (System On Chip) specific Drivers # # CONFIG_SOC_DEVICE is not set # CONFIG_SOC_SAMSUNG is not set # CONFIG_SOC_TI is not set CONFIG_SPI=y CONFIG_DM_SPI=y # CONFIG_SPI_MEM is not set # CONFIG_ALTERA_SPI is not set # CONFIG_APPLE_SPI is not set # CONFIG_ATCSPI200_SPI is not set # CONFIG_ATMEL_SPI is not set # CONFIG_BCMSTB_SPI is not set # CONFIG_CADENCE_QSPI is not set # CONFIG_CF_SPI is not set # CONFIG_DESIGNWARE_SPI is not set # CONFIG_EXYNOS_SPI is not set # CONFIG_FSL_DSPI is not set # CONFIG_FSL_QSPI is not set # CONFIG_GXP_SPI is not set # CONFIG_ICH_SPI is not set # CONFIG_IPROC_QSPI is not set # CONFIG_KIRKWOOD_SPI is not set # CONFIG_MICROCHIP_COREQSPI is not set # CONFIG_MPC8XXX_SPI is not set # CONFIG_MVEBU_A3700_SPI is not set # CONFIG_MXS_SPI is not set # CONFIG_SPI_MXIC is not set # CONFIG_NPCM_FIU_SPI is not set # CONFIG_NPCM_PSPI is not set CONFIG_OMAP3_SPI=y # CONFIG_PL022_SPI is not set # CONFIG_ROCKCHIP_SFC is not set # CONFIG_ROCKCHIP_SPI is not set # CONFIG_SPI_SIFIVE is not set # CONFIG_SOFT_SPI is not set # CONFIG_SPI_SUNXI is not set # CONFIG_TEGRA114_SPI is not set # CONFIG_TEGRA20_SFLASH is not set # CONFIG_TEGRA20_SLINK is not set # CONFIG_TEGRA210_QSPI is not set # CONFIG_TI_QSPI is not set # CONFIG_XILINX_SPI is not set # CONFIG_ZYNQ_SPI is not set # CONFIG_ZYNQ_QSPI is not set # CONFIG_ZYNQMP_GQSPI is not set # CONFIG_SH_QSPI is not set # CONFIG_MXC_SPI is not set # # SPMI support # # CONFIG_SPMI is not set # CONFIG_SYSINFO is not set # # System reset device drivers # # CONFIG_SYSRESET is not set # CONFIG_TEE is not set # CONFIG_DM_THERMAL is not set # # Timer Support # # CONFIG_TIMER is not set # # TPM support # # CONFIG_USB is not set # # UFS Host Controller Support # # CONFIG_TI_J721E_UFS is not set # # Graphics support # # CONFIG_VIDEO is not set # CONFIG_SPL_VIDEO is not set # # VirtIO Drivers # # CONFIG_VIRTIO_MMIO is not set # # 1-Wire support # # CONFIG_W1 is not set # # 1-wire EEPROM support # # CONFIG_W1_EEPROM is not set # # Watchdog Timer Support # # CONFIG_WATCHDOG is not set CONFIG_WATCHDOG_TIMEOUT_MSECS=60000 # CONFIG_IMX_WATCHDOG is not set # CONFIG_OMAP_WATCHDOG is not set # CONFIG_ULP_WATCHDOG is not set # CONFIG_WDT is not set CONFIG_SPL_WDT=y # CONFIG_PHYS_TO_BUS is not set # # File systems # # CONFIG_FS_BTRFS is not set # CONFIG_FS_CBFS is not set # CONFIG_SPL_FS_CBFS is not set CONFIG_FS_EXT4=y CONFIG_EXT4_WRITE=y CONFIG_FS_FAT=y CONFIG_FAT_WRITE=y CONFIG_FS_FAT_MAX_CLUSTSIZE=65536 # CONFIG_FS_JFFS2 is not set # CONFIG_UBIFS_SILENCE_MSG is not set # CONFIG_UBIFS_SILENCE_DEBUG_DUMP is not set # CONFIG_FS_CRAMFS is not set # CONFIG_YAFFS2 is not set # CONFIG_FS_SQUASHFS is not set # CONFIG_FS_EROFS is not set # # Library routines # # CONFIG_ADDR_MAP is not set # CONFIG_SYS_TIMER_COUNTS_DOWN is not set # CONFIG_PHYSMEM is not set # CONFIG_BCH is not set # CONFIG_CC_OPTIMIZE_LIBS_FOR_SPEED is not set CONFIG_CHARSET=y # CONFIG_DYNAMIC_CRC_TABLE is not set CONFIG_HAVE_PRIVATE_LIBGCC=y CONFIG_LIB_UUID=y CONFIG_RANDOM_UUID=y CONFIG_SPL_LIB_UUID=y # CONFIG_SEMIHOSTING is not set # CONFIG_SPL_SEMIHOSTING is not set CONFIG_PRINTF=y CONFIG_SPL_PRINTF=y CONFIG_SPRINTF=y CONFIG_SPL_SPRINTF=y CONFIG_STRTO=y CONFIG_SPL_STRTO=y CONFIG_USE_PRIVATE_LIBGCC=y CONFIG_SYS_HZ=1000 CONFIG_SPL_USE_TINY_PRINTF=y # CONFIG_PANIC_HANG is not set CONFIG_REGEX=y CONFIG_LIB_RAND=y # CONFIG_LIB_HW_RAND is not set CONFIG_SUPPORT_ACPI=y # CONFIG_ACPI is not set # CONFIG_SPL_ACPI is not set # CONFIG_SPL_TINY_MEMSET is not set # CONFIG_BITREVERSE is not set # CONFIG_TRACE is not set # CONFIG_CIRCBUF is not set # CONFIG_CMD_DHRYSTONE is not set # # Security support # # CONFIG_AES is not set # CONFIG_ECDSA is not set # CONFIG_RSA is not set # CONFIG_TPM is not set # CONFIG_SPL_TPM is not set # # Android Verified Boot # # # Hashing Support # # CONFIG_BLAKE2 is not set CONFIG_SHA1=y CONFIG_SHA256=y # CONFIG_SHA512 is not set # CONFIG_SHA384 is not set # CONFIG_SHA_HW_ACCEL is not set CONFIG_SPL_CRC32=y CONFIG_SPL_SHA1=y CONFIG_SPL_SHA256=y # CONFIG_SPL_SHA512 is not set # CONFIG_SPL_SHA384 is not set # CONFIG_SPL_SHA_HW_ACCEL is not set CONFIG_MD5=y # CONFIG_SPL_MD5 is not set CONFIG_CRC8=y # CONFIG_SPL_CRC8 is not set CONFIG_SPL_CRC16=y CONFIG_CRC32=y # # Compression Support # # CONFIG_LZ4 is not set # CONFIG_LZMA is not set CONFIG_LZO=y CONFIG_GZIP=y # CONFIG_ZLIB_UNCOMPRESS is not set # CONFIG_BZIP2 is not set CONFIG_ZLIB=y # CONFIG_ZSTD is not set # CONFIG_SPL_BZIP2 is not set # CONFIG_SPL_LZ4 is not set # CONFIG_SPL_LZMA is not set # CONFIG_VPL_LZMA is not set # CONFIG_SPL_LZO is not set # CONFIG_SPL_GZIP is not set # CONFIG_SPL_ZSTD is not set # CONFIG_ERRNO_STR is not set # CONFIG_HEXDUMP is not set # CONFIG_GETOPT is not set CONFIG_OF_LIBFDT=y CONFIG_OF_LIBFDT_ASSUME_MASK=0x0 CONFIG_SYS_FDT_PAD=0x3000 CONFIG_SPL_OF_LIBFDT=y CONFIG_SPL_OF_LIBFDT_ASSUME_MASK=0xff # # System tables # CONFIG_GENERATE_SMBIOS_TABLE=y # CONFIG_LIB_RATIONAL is not set # CONFIG_SPL_LIB_RATIONAL is not set CONFIG_SMBIOS=y # CONFIG_SMBIOS_PARSER is not set CONFIG_EFI_LOADER=y CONFIG_EFI_BINARY_EXEC=y CONFIG_EFI_BOOTMGR=y CONFIG_EFI_VARIABLE_FILE_STORE=y # CONFIG_EFI_VARIABLE_NO_STORE is not set # CONFIG_EFI_VARIABLES_PRESEED is not set CONFIG_EFI_VAR_BUF_SIZE=131072 # CONFIG_EFI_SCROLL_ON_CLEAR_SCREEN is not set # CONFIG_EFI_RUNTIME_UPDATE_CAPSULE is not set CONFIG_EFI_CAPSULE_MAX=15 CONFIG_EFI_DEVICE_PATH_TO_TEXT=y CONFIG_EFI_DEVICE_PATH_UTIL=y CONFIG_EFI_DT_FIXUP=y CONFIG_EFI_LOADER_HII=y CONFIG_EFI_UNICODE_COLLATION_PROTOCOL2=y CONFIG_EFI_UNICODE_CAPITALIZATION=y CONFIG_EFI_PLATFORM_LANG_CODES="en-US" CONFIG_EFI_GRUB_ARM32_WORKAROUND=y CONFIG_EFI_LOAD_FILE2_INITRD=y CONFIG_EFI_ECPT=y CONFIG_EFI_EBBR_2_1_CONFORMANCE=y # CONFIG_EFI_HTTP_BOOT is not set # CONFIG_OPTEE_LIB is not set # CONFIG_OPTEE_IMAGE is not set # CONFIG_BOOTM_OPTEE is not set # CONFIG_TEST_FDTDEC is not set CONFIG_LIB_ELF=y CONFIG_LMB=y CONFIG_LMB_USE_MAX_REGIONS=y CONFIG_LMB_MAX_REGIONS=16 # CONFIG_PHANDLE_CHECK_SEQ is not set # # Testing # # CONFIG_UNIT_TEST is not set # CONFIG_SPL_UNIT_TEST is not set # CONFIG_POST is not set # # Tools options # CONFIG_MKIMAGE_DTC_PATH="dtc" CONFIG_TOOLS_CRC32=y CONFIG_TOOLS_LIBCRYPTO=y CONFIG_TOOLS_KWBIMAGE=y CONFIG_TOOLS_FIT=y CONFIG_TOOLS_FIT_FULL_CHECK=y CONFIG_TOOLS_FIT_PRINT=y CONFIG_TOOLS_FIT_RSASSA_PSS=y CONFIG_TOOLS_FIT_SIGNATURE=y CONFIG_TOOLS_FIT_SIGNATURE_MAX_SIZE=0x10000000 CONFIG_TOOLS_FIT_VERBOSE=y CONFIG_TOOLS_MD5=y CONFIG_TOOLS_OF_LIBFDT=y CONFIG_TOOLS_SHA1=y CONFIG_TOOLS_SHA256=y CONFIG_TOOLS_SHA384=y CONFIG_TOOLS_SHA512=y # CONFIG_TOOLS_MKEFICAPSULE is not set # CONFIG_FSPI_CONF_HEADER is not set # CONFIG_TOOLS_MKFWUMDATA is not set