Other Parts Discussed in Thread: MSP430F5438, MSP430BT5190
Is the pan1323emk suitable for the bluetooth expansion for the usbstick ezdsp5535
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F5438, MSP430BT5190
Is the pan1323emk suitable for the bluetooth expansion for the usbstick ezdsp5535
Hi Seeni,
YES! The PAN1323ETU board is 100% compatible with the C5535 eZdsp.
The PAN1323EMK comes with...
Best Regards,
Mark
is it possible to transmit the Audio over the bluetoth using this two kits
ie ezDSP + PAN1323ETU --------------> any handsfree BT one way music.
pls suggest .
Hi Senthil,
Yes, it is very possible to transmit Audio over bluetooth using C5535 eZdsp + PAN1323ETU.
The Advanced Audio Distribution Profile (A2DP) well suited for this task.
Contact your local TI representative for details...
Best Regards,
Mark