This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J784S4: ENET RTOS debugging

Part Number: PROCESSOR-SDK-J784S4
Other Parts Discussed in Thread: TDA4VH

Tool/software:

Hello TI,

We are using custom board based on the TDA4VH (version 10.00 of PSDK RTOS).

We have integrated new Eth PHY (NXP PHY) in RTOS according to the integration guide. PHY is connected to the MAIN CPSW2G interface.

We are using enet_lwip_example in order to verify stack, but without success, so far.

Short status is that we have functional MDIO communication towards the PHY, but neither PING nor UDP echo functionality in the example does not work.  

Detailed changes on our side, apart from ETH PHY specific layer:

  1. Phy address in structure gEnetCpbBoard_j7xEthPort (new value 19U) and isStraped value from BFALSE to BTRUE inside enet_board_j784s4_evm.c
    1. Our PHY is HW strapped and in the rgmii-id mode, no config should be deployed in order to work. This has been tested on the Linux side, and is fully functional (both MDIO and RGMII side)
    2. Ethernet is 1Gbit FD.
  2.  Phy MDIO address in macro BOARD_MAIN_EMAC_PHY_ADDR   (19U) inside board_cfg.h file - not sure whether this is used at all.
  3. Static IP adress assignement for the given example:
    1. Uncommented USE_DHCP and USE_AUTOIP macros (default value is 0 and it is not changed) inside lwipcfg.h 
    2. Assigned values of ip address and gateway address in lines following lines inside lwipcfg.h
      1. #define LWIP_PORT_INIT_IPADDR(addr)   IP4_ADDR((addr), 192,168,0,1) (we used different values)
        define LWIP_PORT_INIT_GW(addr)       IP4_ADDR((addr), 169,254,1,1) 
      2. We are using direct connection with PC. Environment is tested with the Linux stack on board and is OK.
  4. Changed value of LWIP_PING_APP macro form 0 to 1 to enable ping application inside lwipcfg.h file

Below is output of enet_lwip_freertos application with some of our additional logs:

oard init finished
==========================
      Enet lwIP App
==========================
Select peripheral type
0: Main CPSW_2G

 

0
Select MAC port
0: ENET_MAC_PORT_1 - RGMII
0
EnetBoard_setupPorts: 1 of 1 ports configurations found
CPU Load: 100%
Starting lwIP, local interface IP is 169.254.27.170
Failed to read Main CPSW2G MAC IDs from EEPROM: -1
No valid MAC address found in EEPROM, falling back to static address
EnetMcm: CPSW_2G on MCU NAVSS
PHY 19 is alive
EnetPhy_bindDriver: PHY 19: OUI:0006ec Model:03 Ver:01 <-> 'TJA1120' : OK
Host MAC address: 70:ff:76:1d:92:c2
[LWIPIF_LWIP] Enet LLD netif initialized successfully
Status callbask sholud be registered here
Status callback function 1, this one is supposed to be calledstatus_callback==UP, local interface IP is 169.254.27.170
Enet lwIP App: Added Network IP address I/F ti0: 169.254.27.170
Initializing apps
UDP server listening on port 5001
Reg read value: 12
EnetPhy_tick: PHY 19: LINK_WAIT (rem ticks 50)
Cpsw_handleLinkUp: Port 1: Link up: 1-Gbps Full-Duplex
MAC Port 1: link up
Link callback 1
link_callback==UP

Log seems to match with similar example that you provided here in 4.7.6.1.3.1. Enet lwIP Example — Platform Development Kit (PDK) - JACINTO User Guide :

https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/09_01_00_06/exports/docs/pdk_jacinto_09_01_00_22/docs/userguide/jacinto/modules/enet/enet_lwip_example.html#running-lwip-example

 

We have read status register to make sure that TDA4 is in proper RGMII mode and we confirmed it (from app (using CPS_REG_READ) we read value 0x12 from the register 0x00104034).

We do have issue that application still does not work neither ping test or any ethtool test.

Do you have ideas how shall we proceed further with debugging, or what can be wrong?

Our expectation was that once the PHY is properly addresses rest of the SW stack should work fine. Is this assumption correct, or something else is needed to be performed?

Regards,

Milena

  • Hi,

    We do have issue that application still does not work neither ping test or any ethtool test.

    Do you have ideas how shall we proceed further with debugging, or what can be wrong?

    Can you check CPSW statistics, whether any Tx & Rx good packet counts are increasing or not?
    You can use GEL scripts to get the CPSW statistics, also check on link partner side whether you are receiving any packets or not?

    Our expectation was that once the PHY is properly addresses rest of the SW stack should work fine. Is this assumption correct, or something else is needed to be performed?

    Yes, if PHY is setup properly rest all taken care by SW stack other than any board specific dependents.

    Also, make sure you have removed extended configuration from "gEnetCpbBoard_j7xEthPort"

    Best Regards,
    Sudheer

  • Hello Sudheer,

    Can you check CPSW statistics, whether any Tx & Rx good packet counts are increasing or not?
    You can use GEL scripts to get the CPSW statistics, also check on link partner side whether you are receiving any packets or not?

    We will print the registers and send to you today. Have some issues with the CCS currently.

    We have monitored interface on PC with the Wireshark. But seems no messages arrived from ECU. Attached file (remove .txt extension) /cfs-file/__key/communityserver-discussions-components-files/791/ping_5F00_capture.pcapng.txt

    Also, make sure you have removed extended configuration from "gEnetCpbBoard_j7xEthPort"

    Extended configuration has been already removed.

    Best regards,

    Milena

  • Hi,

    We have monitored interface on PC with the Wireshark. But seems no messages arrived from ECU. Attached file (remove .txt extension) /cfs-file/__key/communityserver-discussions-components-files/791/ping_5F00_capture.pcapng.txt

    It seems like nothing is captured from remote side by referring to pcap log.

    Can you check CPSW statistics, whether any Tx & Rx good packet counts are increasing or not?
    You can use GEL scripts to get the CPSW statistics, also check on link partner side whether you are receiving any packets or not?

    We will print the registers and send to you today. Have some issues with the CCS currently.

    Sure, Please provide the CPSW statistics to check what went wrong.

    Best Regards,
    Sudheer

  • Hello Sudheer,

    We have captured wireshark log and logs from the registers for following scenario:

    PC connected directly to the ECU - static IP addresses:

    • PC: 169.254.27.163
    • ECU IP: 169.254.27.170

    Did following steps:

    • Wireshark capture started
    • ping command started from PC
    • ECU app started
    • after some time , ping command stopped, and udp echo command stared.

    CPSW statistics registers are printed periodically.

    Wireshark Capture (basically same as previous): /cfs-file/__key/communityserver-discussions-components-files/791/ping_5F00_udpecho_5F00_capture.pcapng.txt

    UART log from ECU:

    /cfs-file/__key/communityserver-discussions-components-files/791/cpsw_2D00_stats_2D00_log.txt

    Seems that RX and TX good frames counters are increasing properly.

    Best regards,

    Milena

  • Hi,

    From statistics it is observed that Host Port Rx and External Port Tx counters are increasing indicates Transmission from CPSW is success.
    But, not Rx counters on external port.

    Can you please check statistics at Peer side if any available and PHY side?

    Also, check RGMII status registers of CPSW.

    Best Regards,
    Sudheer

  • Will check additional info, and feedback.

    Which exact counters/registers are you looking at to check this one, which is not correct?

    But, not Rx counters on external port.

    Milena

  • Hello,

    Additional registers checked on TDA4 side - see at the end:

    Interesting is that the entire status register is 0x0, which indicates Link down.

    Register: 0xc23a000 -------- value: 0x22
    Register: 0xc23a004 -------- value: 0x22
    Register: 0xc23a008 -------- value: 0x0
    Register: 0xc23a00c -------- value: 0x0
    Register: 0xc23a010 -------- value: 0x0
    Register: 0xc23a018 -------- value: 0x0
    Register: 0xc23a020 -------- value: 0x0
    Register: 0xc23a024 -------- value: 0x0
    Register: 0xc23a028 -------- value: 0x0
    Register: 0xc23a02c -------- value: 0x0
    Register: 0xc23a030 -------- value: 0x880
    Register: 0xc23a034 -------- value: 0x0
    Register: 0xc23a038 -------- value: 0x0
    Register: 0xc23a03c -------- value: 0x0
    Register: 0xc23a064 -------- value: 0x0
    Register: 0xc23a068 -------- value: 0x22
    Register: 0xc23a06c -------- value: 0x0
    Register: 0xc23a070 -------- value: 0x0
    Register: 0xc23a074 -------- value: 0x0
    Register: 0xc23a078 -------- value: 0x0
    Register: 0xc23a07c -------- value: 0x0
    Register: 0xc23a080 -------- value: 0x880
    Register: 0xc23a084 -------- value: 0x0
    Register: 0xc23a088 -------- value: 0x0
    Register: 0xc23a08c -------- value: 0x0
    Register: 0xc23a090 -------- value: 0x0
    Register: 0xc23a094 -------- value: 0x0
    Register: 0xc23a098 -------- value: 0x0
    Register: 0xc23a09c -------- value: 0x0
    Register: 0xc23a0a0 -------- value: 0x0
    Register: 0xc23a0a4 -------- value: 0x0
    Register: 0xc23a0a8 -------- value: 0x0
    Register: 0xc23a0ac -------- value: 0x0
    Register: 0xc23a0b0 -------- value: 0x0
    Register: 0xc23a0b4 -------- value: 0x0
    Register: 0xc23a0b8 -------- value: 0x0
    Register: 0xc23a0bc -------- value: 0x0
    Register: 0xc23a0c0 -------- value: 0x0
    Register: 0xc23a0c4 -------- value: 0x0
    Register: 0xc23a0c8 -------- value: 0x0
    Register: 0xc23a0cc -------- value: 0x0
    Register: 0xc23a0d0 -------- value: 0x0
    Register: 0xc23a0d4 -------- value: 0x0
    Register: 0xc23a0d8 -------- value: 0x0
    Register: 0xc23a0dc -------- value: 0x0
    Register: 0xc23a140 -------- value: 0x0
    Register: 0xc23a144 -------- value: 0x0
    Register: 0xc23a148 -------- value: 0x0
    Register: 0xc23a14c -------- value: 0x0
    Register: 0xc23a150 -------- value: 0x0
    Register: 0xc23a154 -------- value: 0x0
    Register: 0xc23a200 -------- value: 0x0
    Register: 0xc23a204 -------- value: 0x0
    Register: 0xc23a208 -------- value: 0x0
    Register: 0xc23a20c -------- value: 0x0
    Register: 0xc23a210 -------- value: 0x0
    Register: 0xc23a214 -------- value: 0x0
    Register: 0xc23a218 -------- value: 0x0
    Register: 0xc23a21c -------- value: 0x0
    Register: 0xc23a220 -------- value: 0x0
    Register: 0xc23a224 -------- value: 0x0
    Register: 0xc23a228 -------- value: 0x0
    Register: 0xc23a22c -------- value: 0x0
    Register: 0xc23a230 -------- value: 0x0
    Register: 0xc23a234 -------- value: 0x23
    Register: 0xc23a238 -------- value: 0x23
    Register: 0xc23a23c -------- value: 0x0
    Register: 0xc23a240 -------- value: 0x0
    Register: 0xc23a244 -------- value: 0x0
    Register: 0xc23a248 -------- value: 0x0
    Register: 0xc23a24c -------- value: 0x0
    Register: 0xc23a250 -------- value: 0x0
    Register: 0xc23a254 -------- value: 0x0
    Register: 0xc23a258 -------- value: 0x0
    Register: 0xc23a25c -------- value: 0x0
    Register: 0xc23a260 -------- value: 0x0
    Register: 0xc23a264 -------- value: 0x8c0
    Register: 0xc23a268 -------- value: 0x23
    Register: 0xc23a26c -------- value: 0x0
    Register: 0xc23a270 -------- value: 0x0
    Register: 0xc23a274 -------- value: 0x0
    Register: 0xc23a278 -------- value: 0x0
    Register: 0xc23a27c -------- value: 0x0
    Register: 0xc23a280 -------- value: 0x8c0
    Register: 0xc23a284 -------- value: 0x0
    Register: 0xc23a288 -------- value: 0x0
    Register: 0xc23a28c -------- value: 0x0
    Register: 0xc23a290 -------- value: 0x0
    Register: 0xc23a294 -------- value: 0x0
    Register: 0xc23a298 -------- value: 0x0
    Register: 0xc23a29c -------- value: 0x0
    Register: 0xc23a2a0 -------- value: 0x0
    Register: 0xc23a2a4 -------- value: 0x0
    Register: 0xc23a2a8 -------- value: 0x0
    Register: 0xc23a2ac -------- value: 0x0
    Register: 0xc23a2b0 -------- value: 0x0
    Register: 0xc23a2b4 -------- value: 0x0
    Register: 0xc23a2b8 -------- value: 0x0
    Register: 0xc23a2bc -------- value: 0x0
    Register: 0xc23a2c0 -------- value: 0x0
    Register: 0xc23a2c4 -------- value: 0x0
    Register: 0xc23a2c8 -------- value: 0x0
    Register: 0xc23a2cc -------- value: 0x0
    Register: 0xc23a2d0 -------- value: 0x0
    Register: 0xc23a2d4 -------- value: 0x0
    Register: 0xc23a2d8 -------- value: 0x0
    Register: 0xc23a2dc -------- value: 0x0
    Register: 0xc23a340 -------- value: 0x0
    Register: 0xc23a344 -------- value: 0x0
    Register: 0xc23a348 -------- value: 0x0
    Register: 0xc23a34c -------- value: 0x0
    Register: 0xc23a350 -------- value: 0x0
    Register: 0xc23a354 -------- value: 0x0
    Register: 0xc23a37c -------- value: 0x0
    Register: 0xc23a380 -------- value: 0x0
    Register: 0xc23a3c0 -------- value: 0x0
    Register: 0xc23a3e0 -------- value: 0x0
    Register: 0xc200048 -------- value: 0x0
    Register: 0xc200f08 -------- value: 0x80000
    Register: 0xc200f0c -------- value: 0x0

  • Hi,

    Which exact counters/registers are you looking at to check this one, which is not correct?

    But, not Rx counters on external port.

    Yes, Please refer to Register Spec of CPSW.

    0x3A000 is Rx good frames of Host Port (Internal CPPI Port) ->  packets from Internal cores of SOC which is same as External Port Tx counts (0x3A234)
    0x3A204 is Rx goof frames of External Ports received from PHY, above these are 0s which means no Rx packets.

    Interesting is that the entire status register is 0x0, which indicates Link down.

    Are you talking about above CPSW statistics? if yes, no these are not indicators for Link status.

    0x0C200030 is RGMII status register.
    Can you also provide MAC Control register (0x0C222330)of CPSW.

    Best Regards,
    Sudheer

  • Hello,

    It turned out that the problem was actually our setup external to the board with TDA4 - cabling to be more precise. Once we sorted this out, ping started working.
    Thanks for your assistance. This thread can be marked as solved, or Milena will do that when she's back in office.

    Best Regards,
    Miloš

  • Hi,

    It turned out that the problem was actually our setup external to the board with TDA4 - cabling to be more precise. Once we sorted this out, ping started working.

    Thanks for the update.

    Best Regards,
    Sudheer