This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to run UDWORKS demo in EVM 8168?

Other Parts Discussed in Thread: PMP, TVP5158

Hi All,

         I want run UDWORKS demo in EVM8168, I use the hardware are  "816X/389X EVM ASSY 512870 REV F" and "DM816X VIDEO SECURITY BOARD ASSY 513500 REV B" ,  the software i used is  "DM8168DVR_RDK_00.07.00.01".

        when i run the demo, the message is this:

 

 

U-Boot 2010.06 (May 13 2011 - 01:05:43)

TI8168-GP rev 1.1

ARM clk: 987MHz
DDR clk: 796MHz

I2C:   ready
DRAM:  2 GiB
NAND:  256 MiB
Net:   Ethernet PHY: GENERIC @ 0x01
DaVinci EMAC
Hit any key to stop autoboot:  0
Connect speed 100M Full
Using DaVinci EMAC device
TFTP from server 192.168.47.134; our IP address is 192.168.47.162
Filename 'uImage_dvr'.
Load address: 0x81000000
Loading: *#################################################################
  #################################################################
  ############################
done
Bytes transferred = 2306532 (2331e4 hex)
## Booting kernel from Legacy Image at 81000000 ...
   Image Name:   Linux-2.6.37
   Created:      2011-05-27   2:20:45 UTC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2306468 Bytes = 2.2 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (root@idaroa-VirtualBox) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 Fri May 27 11:20:41 KST 2011
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168evm
vram size = 20971520 at 0
reserved size = 20971520 at 0
FB: Reserving 20971520 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8168 1.1
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 27392
Kernel command line: mem=128M console=ttyO2,115200n8 root=/dev/nfs rw rootfstype=jffs2 nfsroot=192.168.47.163:/work/00.07.00.01/target/rfs ip=192.168.47.162:192.168.47.163:192.168.47.1:255.255.255.0::eth0:off vram=20M
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 108MB = 108MB total
Memory: 104504k/104504k available, 26568k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xffc00000 - 0xffe00000   (   2 MB)
    vmalloc : 0xc8800000 - 0xf8000000   ( 760 MB)
    lowmem  : 0xc0000000 - 0xc8000000   ( 128 MB)
    modules : 0xbf000000 - 0xc0000000   (  16 MB)
      .init : 0xc0008000 - 0xc0034000   ( 176 kB)
      .text : 0xc0034000 - 0xc045c000   (4256 kB)
      .data : 0xc045c000 - 0xc0499060   ( 245 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:375
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ368
Trying to install interrupt handler for IRQ369
Trying to install interrupt handler for IRQ370
Trying to install interrupt handler for IRQ371
Trying to install interrupt handler for IRQ372
Trying to install interrupt handler for IRQ373
Trying to install interrupt handler for IRQ374
Trying to install type control for IRQ375
Trying to set irq flags for IRQ375
OMAP clockevent source: GPTIMER1 at 27000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 0
3-wired eeprom init done. (H/W ver:00)
registered ti816x_vpss device
pm_dbg_init: only OMAP3 supported
Registered ti81xx_fb device
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at c880c000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at c881e800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
sr1_fck HVT rate = 125000000
sr2_fck SVT rate = 125000000
SR NTarget value for HVT 0xa9ef8b
SR NTarget value for SVT 0xaaaeca
SmartReflex Driver initialized
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 204
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
console [ttyO2] enabled
brd: module loaded
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x3
ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
scsi1 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16
omap2-nand driver initializing
NAND device: Manufacturer ID: 0xec, Chip ID: 0xda (Samsung )
Creating 5 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000240000 : "U-Boot"
0x000000240000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x0000106c0000 : "File System"
mtd: partition "File System" extends beyond the end of device "omap2-nand.0" -- size truncated to 0xf940000
0x000010000000-0x000010000000 : "Reserved"
mtd: partition "Reserved" is out of reach -- disabled
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffff9
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver unknown
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
rtc-ds1307: probe of 1-0068 failed with error -5
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
PSTATE 1f20000
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
ALSA device list:
  #0: TI8168 DVR
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
davinci_emac_probe: using random MAC addr: 8a:4d:20:4b:6d:f7
davinci_emac_probe: using random MAC addr: e6:91:8e:02:02:f4
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
ata1: SATA link down (SStatus 0 SControl 300)
ata2: SATA link down (SStatus 0 SControl 300)
davinci_mdio davinci_mdio.0: resetting idled controller
net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=282f014)
IP-Config: Complete:
     device=eth0, addr=192.168.47.162, mask=255.255.255.0, gw=192.168.47.1,
     host=192.168.47.162, domain=, nis-domain=(none),
     bootserver=192.168.47.163, rootserver=192.168.47.163, rootpath=
PHY: 0:01 - Link is Up - 100/Full
VFS: Mounted root (nfs filesystem) on device 0:14.
devtmpfs: mounted
Freeing init memory: 176K

INIT: version 2.86 booting

Error opening /dev/fb0: No such file or directory
Please wait: booting...
Starting udev
udevd (70): /proc/70/oom_adj is deprecated, please use /proc/70/oom_score_adj instead.
Root filesystem already rw, not remounting
Caching udev devnodes
Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory
ALSA: Restoring mixer settings...
NOT configuring network interfaces: / is an NFS mount
No state is present for card DVR
Found hardware: "" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card DVR
hwclock: can't open '/dev/misc/rtc': No such file or directory
Mon Apr 11 10:13:00 UTC 2011
hwclock: can't open '/dev/misc/rtc': No such file or directory

INIT: Entering runlevel: 5

Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: NET: Registered protocol family 10
done
Starting thttpd.
SysLink version : 02.00.00.67_alpha2
SysLink module created on Date:May  9 2011 Time:07:39:43
Entered KnlUtilsDrv_initializeModule
traceMask value: 0x0
Leaving KnlUtilsDrv_initializeModule 0x0
[module] ti81xx_hdmi init done
load module completed
start application


 _   _ ___  _   _         _
| | | |    | ||| |___ ___| | _ ___
| |_| | |) |  ~  | . |  _| |/_|  -|
|_____|___ /____/ ___|_| |_| _|-__|

DVR_Netra Board (2011.04)

dvr login: input: dvr-keypad as /devices/virtual/input/input0
front_interface start
Wait for VM3 to to create the server first
app: dvr_init() ... done
enc: bitrate ... 1200000

app: dvr_startsystem ... start
Entering: OMX_TI_CMUX_ComponentInit
Entering: OMX_TI_DMUX_ComponentInit
 AVSERVER UI: Starting Streaming Server...
Entering: _OMX_TI_DMUX_DataProcPrdTaskFcn
Entering: _OMX_CMUXDataProcPrdTaskFcn
NetraDrvInit: 6
queue id:0
Initializing...
...done initializing
Play this stream using the URL:
 rtsp://192.168.47.162:8558/h264_ch8
NetraDrvInit: 2
queue id:0
Initializing...
...done initializing
Play this stream using the URL:
 rtsp://192.168.47.162:8557/h264_ch7
NetraDrvInit: 2
queue id:0
Initializing...
...done initializing
Play this stream using the URL:
 rtsp://192.168.47.162:8556/h264_ch6
NetraDrvInit: 10
NetraDrvInit: 9
queue id:0
Initializing...
...done initializing
Play this stream using the URL:
 rtsp://192.168.47.162:8554/h264_ch4
NetraDrvInit: 8
queue id:0
Initializing...
...done initializing
Play this stream using the URL:
 rtsp://192.168.47.162:8553/h264_ch3
NetraDrvInit: 6
queue id:0
Initializing...
...done initializing
Play this stream using the URL:
 rtsp://192.168.47.162:8552/h264_ch2
NetraDrvInit: 2
queue id:0
Initializing...
...done initializing
Play this stream using the URL:
 rtsp://192.168.47.162:8551/h264_ch1
queue id:0
Initializing...
...done initializing
Play this stream using the URL:
 rtsp://192.168.47.162:8555/h264_ch5
 AVSERVER UI: Starting Streaming Server...DONE
Entering: _OMX_CMUXEnablePeriodicDataProcess
[module] vpss probe done.
tinfo.pixelclock 74250, var->pixclock 13468
[module] ti81xxfb probe done.
app: lib816x_statsystem ... done
ReadProfileFile Fail
ReadProfileFile Fail

 

I change the TVP5158 address,but the frame on HDMI screen is only the first frame, what should i do now?

 

Regards,
Zhousheng

  • Zhousheng,

     

    Changing TVP5158 address is the only modification required to run UD Works DVR GUI on EVM+VS daughter card. Are you not able to see the GUI? Are you saying that the HDMI monitor just shows the first frame and then freezes?

    Also, we would recommend you to move to DVR RDK 01.06.00.11 version which is based on new frame work. Please contact your local FAE to get this release.

     

    Regards,

    Arun

  • Arun,

            Thank you for your reply! 

    "Changing TVP5158 address is the only modification required to run UD Works DVR GUI on EVM+VS daughter card. Are you not able to see the GUI? Are you saying that the HDMI monitor just shows the first frame and then freezes? "

    I can see the GUI, but the HDMI monitor just shows the first frame and then freezes.

    I now have the DVR RDK 01.06.00.11 version , but in these version not have the DVR Demo, i would to move to DVR RDK 01.06.00.11, but i want to show the dvr demo in our board, can you tell me how to change the code in DVR_RDK_00.07.00.01 Demo?

    Regards,

    ZhouSheng

  • Hi,

    Have you ordered DVRRDK on www.udworks.com ? If yes, you should have got an email notification of latest release being available on UDWorks website which has the GUI source code as well.

    Please let me know if you have not received any email from UDWorks and also tell me the registered emailId on the UDWorks website? I can follow up with them.

     

    Regards,

    Anshuman

    PS: Please mark this post as verified, if you think it has answered your question. Thanks.