Tool/software:
We are using TI's TMS320C6657 chip and recently encountered an abnormal phenomenon on one chip.
After bootloading and jumping to main, there's a probability of the system hanging, and there's also a probability that the software runs but with abnormal access to the chip peripherals. We've conducted power cycling tests, and the probabilities of the two abnormal phenomena are approximately 0.3% to 0.5%.
What could be the cause? In which areas can we analyze this issue?