This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM67A: TDA4VM, AM67A, or AM69A SoC for real-time control - Simulink

Part Number: AM67A
Other Parts Discussed in Thread: TDA4VM, AM69A

Tool/software:

Hello,

We are currently evaluating the possibility of using the C7x DSP cores in the TDA4VM, AM67A, or AM69A SoC for real-time control of a power converter (switching at 10 kHz, cycle period = 100 µs). The control will be based on a custom Model Predictive Control (MPC) algorithm written in C, as well as a Simulink model that will be compiled to C code for deployment.

Could someone please confirm with 100% certainty if the C7x DSPs are fully available for running custom user code (either written in C or compiled from Simulink) without any restrictions or special licensing requirements? Specifically:

  1. Are the C7x DSPs fully accessible for running custom code independently of the AI workloads and AI frameworks (such as the TI AI toolkit)?
  2. Are there any restrictions or limitations in terms of the DSP’s resources when used for non-AI tasks, such as real-time control or custom algorithm execution?
  3. Is it possible to configure the TDA4VM, AM67A, or AM69A SoC to run real-time control algorithms with full access to the C7x DSPs, while ensuring no interference from other processing workloads (e.g., AI, Linux tasks)?

Best regards,