Part Number: AM3352
Tool/software:
Hello,
I am designing a PCB using the AM3352BZCZ30 and a 4GBIT 16-bit DDR3 memory (D2516ECMDXGJD-U), which also benefits from ODT. I have three questions.
First, after reviewing TI’s open-source schematic files, I noticed that they used termination resistors for DDR2 memory, but not for DDR3. I’m wondering if I should use them for DDR3 as well?
Second, the datasheets suggest that DDR routing should be done on the same layer, or at most, two layers. However, in their files, I see that they routed the signals across different layers. Is this acceptable? For instance, can I route my data lines on both the top and bottom layers, and address lines on the top and inner layers, or is there a specific configuration I should follow?
Lastly, I see that DQS0, DQSN0, and DQS1,DQSN1 are differential pairs, but in their files, they were not defined as such and were routed separately and uncoupled. How should I handle this in my design?
Regards,