This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: Error: vdec 30210000.video-codec: OPP table not found in device tree

Part Number: AM62A7

Tool/software:

HI experts,

The version of the SDK used is:10.1.8--v10.01.08

Linux version 6.6.58-ti (aarch64-oe-linux-gcc (GCC) 13.3.0

When I use the above version, I get the following error:

vdec 30210000.video-codec: OPP table not found in device tree
vdec 30210000.video-codec: Added wave5 driver with caps: 'ENCODE' 'DECODE'
vdec 30210000.video-codec: Product Code: 0x521c
vdec 30210000.video-codec: Firmware Revision: 334314

What would be the cause of this error? Can you point us how to solve this error?
Why haven't I encountered this error with SDK09_02_00_05?

Best Regards

Shawn

  • Hi Shawn,

    Addition of the OPP table was adding latency as reported by few customers. so we removed it as a part of this commit below:

    https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/commit/arch/arm64/boot/dts/ti?h=ti-linux-6.6.y&id=7a0788f1d89af1e297b68ce9b085328546fdbfdc

    If you chose to have dynamic frequency, then feel free to add it back on the Device tree and this should suppress the warning.

    Thanks.

    Best Regards,

    Suren

  • Hi Suren,

    After adding it according to the attached patch, it doesn't prompt OPP related warnings anymore.

    Currently, there is still the following picture of the prompt error, wave5 driver this part should do what change, I compared SDK9.2 and SDK10.1, found that the wave5 driver change is bigger, currently in SDK10.1 does not generate v4l-subdev related sub-devices.

    Best Regards

    Shawn

  • Hi Shawn,

    The error is not an error but a warning that hr timer polling is being used as AM62A has no interrupt routed.

    You could ignore this in the log.

    Best Regards,

    Suren

  • Hi Suren,

    I know I should ignore the first two log prints, the exception is these logs:

    In SDK version 9.2, there is no wave5 driver error reported, and I get the following log, and the v4l-subdev device can also be registered.

    But now I am using SDK version 10.1.8, I don't see the v4l-subdev related subdev and there is an error reported by wave5 driver, which causes my camera driver to not get the video stream.Video related devices are also only these:

    Can you help me to solve this problem?

    Best Regards

    Shawn

  • To add, here is the complete log printout from my side:

    U-Boot SPL 2024.04-ti (Mar 03 2025 - 01:57:22 +0000)
    SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)')
    SPL initial stack usage: 13568 bytes
    Trying to boot from MMC2
    Authentication passed
    Authentication passed
    Authentication passed
    Authentication passed
    Authentication passed
    Starting ATF on ARM64 core...
    
    NOTICE:  BL31: v2.11.0(release):v2.11.0-906-g58b25570c9-dirty
    NOTICE:  BL31: Built : 04:20:32, Nov  1 2024
    
    U-Boot SPL 2024.04-ti (Mar 03 2025 - 01:57:10 +0000)
    SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)')
    Trying to boot from MMC2
    Authentication passed
    Authentication passed
    
    
    U-Boot 2024.04-ti (Mar 03 2025 - 01:57:10 +0000)
    
    SoC:   AM62AX SR1.0 HS-FS
    Model: Texas Instruments AM62A7 SK
    DRAM:  1 GiB
    Core:  81 devices, 29 uclasses, devicetree: separate
    MMC:   mmc@fa10000: 0, mmc@fa00000: 1
    Loading Environment from nowhere... OK
    In:    serial@2800000
    Out:   serial@2800000
    Err:   serial@2800000
    Net:   Could not get PHY for mdio@f00: addr 0
    am65_cpsw_nuss_port ethernet@8000000port@1: phy_connect() failed
    No ethernet found.
    
    Hit any key to stop autoboot:  0
    switch to partitions #0, OK
    mmc1 is current device
    SD/MMC found on device 1
    653 bytes read in 33 ms (18.6 KiB/s)
    Loaded env from uEnv.txt
    Importing environment from mmc1 ...
    53172 bytes read in 54 ms (960.9 KiB/s)
    Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
    Load Remote Processor 0 with data@addr=0x82000000 53172 bytes: Success!
    10719312 bytes read in 490 ms (20.9 MiB/s)
    Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
    Load Remote Processor 2 with data@addr=0x82000000 10719312 bytes: Success!
    21029376 bytes read in 903 ms (22.2 MiB/s)
    63218 bytes read in 38 ms (1.6 MiB/s)
    Working FDT set to 88000000
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
    Working FDT set to 88000000
       Loading Device Tree to 000000008feed000, end 000000008fffffff ... OK
    Working FDT set to 8feed000
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 6.6.58-ti (root@ba920d9ac912) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240723) #7 SMP PREEMPT Fri Feb 28 05:56:23 UTC 2025
    [    0.000000] KASLR disabled due to lack of seed
    [    0.000000] Machine model: Texas Instruments AM62A7 SK
    [    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
    [    0.000000] printk: bootconsole [ns16550a0] enabled
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000000bd000000, size 48 MiB
    [    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000bd000000..0x00000000bfffffff (49152 KiB) map reusable linux,cma
    [    0.000000] OF: reserved mem: 0x0000000080000000..0x000000008007ffff (512 KiB) nomap non-reusable tfa@80000000
    [    0.000000] Reserved memory: created DMA memory pool at 0x0000000099800000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node c7x-dma-memory@99800000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x0000000099800000..0x00000000998fffff (1024 KiB) nomap non-reusable c7x-dma-memory@99800000
    [    0.000000] Reserved memory: created DMA memory pool at 0x0000000099900000, size 30 MiB
    [    0.000000] OF: reserved mem: initialized node c7x-memory@99900000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x0000000099900000..0x000000009b7ffffe (31743 KiB) nomap non-reusable c7x-memory@99900000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009b800000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9b800000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009b800000..0x000000009b8fffff (1024 KiB) nomap non-reusable r5f-dma-memory@9b800000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009b900000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9b900000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009b900000..0x000000009c7fffff (15360 KiB) nomap non-reusable r5f-dma-memory@9b900000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9c800000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009c800000..0x000000009c8fffff (1024 KiB) nomap non-reusable r5f-dma-memory@9c800000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009c900000, size 30 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9c900000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009c900000..0x000000009e6fffff (30720 KiB) nomap non-reusable r5f-dma-memory@9c900000
    [    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
    [    0.000000] OF: reserved mem: 0x00000000a0000000..0x00000000a0ffffff (16384 KiB) nomap non-reusable edgeai-rtos-ipc-memory-region
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 32 MiB
    [    0.000000] OF: reserved mem: initialized node edgeai-dma-memory@a1000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000a1000000..0x00000000a2ffffff (32768 KiB) nomap non-reusable edgeai-dma-memory@a1000000
    [    0.000000] OF: reserved mem: initialized node edgeai_shared-memories, compatible id dma-heap-carveout
    [    0.000000] OF: reserved mem: 0x00000000a3000000..0x00000000a93fffff (102400 KiB) map non-reusable edgeai_shared-memories
    [    0.000000] OF: reserved mem: initialized node edgeai_license-memories@aa000000, compatible id dma-heap-carveout
    [    0.000000] OF: reserved mem: 0x00000000aa000000..0x00000000aa0fffff (1024 KiB) map non-reusable edgeai_license-memories@aa000000
    [    0.000000] OF: reserved mem: initialized node edgeai_update-memories@aa100000, compatible id dma-heap-carveout
    [    0.000000] OF: reserved mem: 0x00000000aa100000..0x00000000aa2fffff (2048 KiB) map non-reusable edgeai_update-memories@aa100000
    [    0.000000] OF: reserved mem: initialized node edgeai_canLog-memories@aa300000, compatible id dma-heap-carveout
    [    0.000000] OF: reserved mem: 0x00000000aa300000..0x00000000aa7fffff (5120 KiB) map non-reusable edgeai_canLog-memories@aa300000
    [    0.000000] OF: reserved mem: initialized node edgeai_buffuer1-memories@aa800000, compatible id dma-heap-carveout
    [    0.000000] OF: reserved mem: 0x00000000aa800000..0x00000000aa80ffff (64 KiB) map non-reusable edgeai_buffuer1-memories@aa800000
    [    0.000000] OF: reserved mem: initialized node edgeai_buffuer2-memories@aa900000, compatible id dma-heap-carveout
    [    0.000000] OF: reserved mem: 0x00000000aa900000..0x00000000aa90ffff (64 KiB) map non-reusable edgeai_buffuer2-memories@aa900000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000ae000000, size 32 MiB
    [    0.000000] OF: reserved mem: initialized node edgeai-core-heap-memory@ae000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000ae000000..0x00000000afffffff (32768 KiB) nomap non-reusable edgeai-core-heap-memory@ae000000
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x0000000080000000-0x00000000bfffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   empty
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x0000000080000000-0x000000008007ffff]
    [    0.000000]   node   0: [mem 0x0000000080080000-0x00000000997fffff]
    [    0.000000]   node   0: [mem 0x0000000099800000-0x000000009b7fefff]
    [    0.000000]   node   0: [mem 0x000000009b800000-0x000000009e6fffff]
    [    0.000000]   node   0: [mem 0x000000009e700000-0x000000009e7fffff]
    [    0.000000]   node   0: [mem 0x000000009e800000-0x00000000a2ffffff]
    [    0.000000]   node   0: [mem 0x00000000a3000000-0x00000000adffffff]
    [    0.000000]   node   0: [mem 0x00000000ae000000-0x00000000afffffff]
    [    0.000000]   node   0: [mem 0x00000000b0000000-0x00000000bfffffff]
    [    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff]
    [    0.000000] On node 0, zone DMA: 1 pages in unavailable ranges
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: Trusted OS migration not required
    [    0.000000] psci: SMC Calling Convention v1.5
    [    0.000000] percpu: Embedded 20 pages/cpu s43176 r8192 d30552 u81920
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: detected: GIC system register CPU interface
    [    0.000000] CPU features: detected: ARM erratum 845719
    [    0.000000] alternatives: applying boot alternatives
    [    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=02d35568-02 rw rootfstype=ext4 rootwait
    [    0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 258047
    [    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
    [    0.000000] software IO TLB: area num 4.
    [    0.000000] software IO TLB: mapped [mem 0x00000000b7c00000-0x00000000bbc00000] (64MB)
    [    0.000000] Memory: 593084K/1048572K available (12480K kernel code, 1272K rwdata, 4184K rodata, 2496K init, 528K bss, 406336K reserved, 49152K cma-reserved)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu:     RCU event tracing is enabled.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
    [    0.000000]  Trampoline variant of Tasks RCU enabled.
    [    0.000000]  Tracing variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
    [    0.000000] GICv3: 256 SPIs implemented
    [    0.000000] GICv3: 0 Extended SPIs implemented
    [    0.000000] Root IRQ handler: gic_handle_irq
    [    0.000000] GICv3: GICv3 features: 16 PPIs
    [    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
    [    0.000000] ITS [mem 0x01820000-0x0182ffff]
    [    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
    [    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
    [    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80c00000 (flat, esz 8, psz 64K, shr 0)
    [    0.000000] ITS: using cache flushing for cmd queue
    [    0.000000] GICv3: using LPI property table @0x0000000080440000
    [    0.000000] GIC: using cache flushing for LPI property table
    [    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080450000
    [    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
    [    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
    [    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
    [    0.008554] Console: colour dummy device 80x25
    [    0.013146] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
    [    0.023830] pid_max: default: 32768 minimum: 301
    [    0.028627] LSM: initializing lsm=capability,selinux,integrity
    [    0.034617] SELinux:  Initializing.
    [    0.038294] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
    [    0.045865] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
    [    0.055583] RCU Tasks: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
    [    0.062892] RCU Tasks Trace: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
    [    0.070810] rcu: Hierarchical SRCU implementation.
    [    0.075715] rcu:     Max phase no-delay instances is 1000.
    [    0.081302] Platform MSI: msi-controller@1820000 domain created
    [    0.087589] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
    [    0.097034] EFI services will not be available.
    [    0.101926] smp: Bringing up secondary CPUs ...
    [    0.107166] Detected VIPT I-cache on CPU1
    [    0.107238] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
    [    0.107255] GICv3: CPU1: using allocated LPI pending table @0x0000000080460000
    [    0.107300] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
    [    0.107964] Detected VIPT I-cache on CPU2
    [    0.108018] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
    [    0.108032] GICv3: CPU2: using allocated LPI pending table @0x0000000080470000
    [    0.108064] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
    [    0.108655] Detected VIPT I-cache on CPU3
    [    0.108703] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
    [    0.108715] GICv3: CPU3: using allocated LPI pending table @0x0000000080480000
    [    0.108743] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
    [    0.108812] smp: Brought up 1 node, 4 CPUs
    [    0.188536] SMP: Total of 4 processors activated.
    [    0.193348] CPU features: detected: 32-bit EL0 Support
    [    0.198618] CPU features: detected: CRC32 instructions
    [    0.203931] CPU: All CPU(s) started at EL2
    [    0.208129] alternatives: applying system-wide alternatives
    [    0.215179] devtmpfs: initialized
    [    0.227157] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.237157] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
    [    0.245620] pinctrl core: initialized pinctrl subsystem
    [    0.251482] DMI not present or invalid.
    [    0.256018] NET: Registered PF_NETLINK/PF_ROUTE protocol family
    [    0.262907] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
    [    0.270205] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.278194] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.286350] audit: initializing netlink subsys (disabled)
    [    0.292052] audit: type=2000 audit(0.180:1): state=initialized audit_enabled=0 res=1
    [    0.292501] thermal_sys: Registered thermal governor 'step_wise'
    [    0.299985] thermal_sys: Registered thermal governor 'power_allocator'
    [    0.306168] cpuidle: using governor menu
    [    0.317020] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.324041] ASID allocator initialised with 65536 entries
    [    0.334239] /bus@f0000/interrupt-controller@1800000: Fixed dependency cycle(s) with /bus@f0000/interrupt-controller@1800000
    [    0.345727] /bus@f0000/i2c@20000000/usb-power-controller@3f/connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
    [    0.358880] /bus@f0000/dwc3-usb@f900000/usb@31000000: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/usb-power-controller@3f/connector
    [    0.376929] /bus@f0000/i2c@20000000/usb-power-controller@3f/connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
    [    0.391115] /bus@f0000/dwc3-usb@f900000/usb@31000000: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/usb-power-controller@3f/connector
    [    0.407517] Modules: 27488 pages in range for non-PLT usage
    [    0.407530] Modules: 519008 pages in range for PLT usage
    [    0.413953] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.426358] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
    [    0.432770] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.439710] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
    [    0.446118] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.453057] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
    [    0.459465] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.466404] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
    [    0.474167] k3-chipinfo 43000014.chipid: Family:AM62AX rev:SR1.0 JTAGID[0x0bb8d02f] Detected
    [    0.483738] iommu: Default domain type: Translated
    [    0.488666] iommu: DMA domain TLB invalidation policy: strict mode
    [    0.495279] SCSI subsystem initialized
    [    0.499421] usbcore: registered new interface driver usbfs
    [    0.505065] usbcore: registered new interface driver hub
    [    0.510525] usbcore: registered new device driver usb
    [    0.516137] pps_core: LinuxPPS API ver. 1 registered
    [    0.521218] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.530568] PTP clock support registered
    [    0.534768] EDAC MC: Ver: 3.0.0
    [    0.538454] scmi_core: SCMI protocol bus registered
    [    0.543728] FPGA manager framework
    [    0.547287] Advanced Linux Sound Architecture Driver Initialized.
    [    0.554471] vgaarb: loaded
    [    0.557589] clocksource: Switched to clocksource arch_sys_counter
    [    0.564108] VFS: Disk quotas dquot_6.6.0
    [    0.568165] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.582080] Carveout Heap: Exported 100 MiB at 0x00000000a3000000
    [    0.588469] Carveout Heap: Exported 1 MiB at 0x00000000aa000000
    [    0.594634] Carveout Heap: Exported 2 MiB at 0x00000000aa100000
    [    0.600795] Carveout Heap: Exported 5 MiB at 0x00000000aa300000
    [    0.606952] Carveout Heap: Exported 0 MiB at 0x00000000aa800000
    [    0.613107] Carveout Heap: Exported 0 MiB at 0x00000000aa900000
    [    0.619258] NET: Registered PF_INET protocol family
    [    0.624372] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear)
    [    0.632942] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)
    [    0.641559] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
    [    0.649493] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)
    [    0.657469] TCP bind hash table entries: 8192 (order: 6, 262144 bytes, linear)
    [    0.665061] TCP: Hash tables configured (established 8192 bind 8192)
    [    0.671673] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
    [    0.678475] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
    [    0.685846] NET: Registered PF_UNIX/PF_LOCAL protocol family
    [    0.692050] RPC: Registered named UNIX socket transport module.
    [    0.698123] RPC: Registered udp transport module.
    [    0.702933] RPC: Registered tcp transport module.
    [    0.707742] RPC: Registered tcp-with-tls transport module.
    [    0.713350] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.719941] NET: Registered PF_XDP protocol family
    [    0.724855] PCI: CLS 0 bytes, default 64
    [    0.730237] Initialise system trusted keyrings
    [    0.734995] workingset: timestamp_bits=46 max_order=18 bucket_order=0
    [    0.741906] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.748132] NFS: Registering the id_resolver key type
    [    0.753335] Key type id_resolver registered
    [    0.757614] Key type id_legacy registered
    [    0.761728] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.768584] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.810168] Key type asymmetric registered
    [    0.814369] Asymmetric key parser 'x509' registered
    [    0.819408] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
    [    0.827126] io scheduler mq-deadline registered
    [    0.831767] io scheduler kyber registered
    [    0.835897] io scheduler bfq registered
    [    0.842712] pinctrl-single 4084000.pinctrl: 34 pins, size 136
    [    0.849308] pinctrl-single f4000.pinctrl: 151 pins, size 604
    [    0.861960] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
    [    0.879592] loop: module loaded
    [    0.883832] megasas: 07.725.01.00-rc1
    [    0.891221] tun: Universal TUN/TAP device driver, 1.6
    [    0.897356] VFIO - User Level meta-driver version: 0.3
    [    0.903703] usbcore: registered new interface driver usb-storage
    [    0.910426] i2c_dev: i2c /dev entries driver
    [    0.916277] sdhci: Secure Digital Host Controller Interface driver
    [    0.922620] sdhci: Copyright(c) Pierre Ossman
    [    0.927284] sdhci-pltfm: SDHCI platform and OF driver helper
    [    0.933689] ledtrig-cpu: registered to indicate activity on CPUs
    [    0.940114] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
    [    0.947380] usbcore: registered new interface driver usbhid
    [    0.953082] usbhid: USB HID core driver
    [    0.958275] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
    [    0.967241] optee: probing for conduit method.
    [    0.971814] optee: revision 4.4 (8f645256efc0dc66)
    [    0.972124] optee: dynamic shared memory is enabled
    [    0.982702] random: crng init done
    [    0.986291] optee: initialized driver
    [    0.991514] Initializing XFRM netlink socket
    [    0.995933] NET: Registered PF_PACKET protocol family
    [    1.001180] Key type dns_resolver registered
    [    1.013992] registered taskstats version 1
    [    1.018332] Loading compiled-in X.509 certificates
    [    1.036187] ti-sci 44043000.system-controller: ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)')
    [    1.080689] /bus@f0000/i2c@20000000/usb-power-controller@3f/connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
    [    1.094051] /bus@f0000/i2c@20000000/pmic@48: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/pmic@48/regulators/buck5
    [    1.106002] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
    [    1.113424] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz
    [    1.119982] omap_i2c 20020000.i2c: bus 2 rev0.12 at 400 kHz
    [    1.125919] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
    [    1.134235] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
    [    1.143486] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
    [    1.152467] ti-sci-inta 4e0a0000.interrupt-controller: Interrupt Aggregator domain 200 created
    [    1.162024] ti-udma 485c0100.dma-controller: Number of rings: 82
    [    1.170778] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
    [    1.181949] ti-udma 485c0000.dma-controller: Number of rings: 150
    [    1.193064] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
    [    1.202716] ti-udma 4e230000.dma-controller: Number of rings: 6
    [    1.209387] ti-udma 4e230000.dma-controller: Channels: 6 (bchan: 0, tchan: 0, rchan: 6)
    [    1.218841] printk: console [ttyS2] disabled
    [    1.223620] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 249, base_baud = 3000000) is a 8250
    [    1.232502] printk: console [ttyS2] enabled
    [    1.232502] printk: console [ttyS2] enabled
    [    1.240970] printk: bootconsole [ns16550a0] disabled
    [    1.240970] printk: bootconsole [ns16550a0] disabled
    [    1.655870] spi-nand: probe of spi0.0 failed with error -110
    [    1.662354] /bus@f0000/i2c@20000000/usb-power-controller@3f/connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
    [    1.675305] /bus@f0000/dwc3-usb@f900000/usb@31000000: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/usb-power-controller@3f/connector
    [    1.688805] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [    1.694315] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
    [    1.702083] xhci-hcd xhci-hcd.0.auto: USB3 root hub has no ports
    [    1.708095] xhci-hcd xhci-hcd.0.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000008020000010
    [    1.717523] xhci-hcd xhci-hcd.0.auto: irq 253, io mem 0x31000000
    [    1.724363] hub 1-0:1.0: USB hub found
    [    1.728156] hub 1-0:1.0: 1 port detected
    [    1.734303] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
    [    1.739847] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
    [    1.747611] xhci-hcd xhci-hcd.1.auto: USB3 root hub has no ports
    [    1.753630] xhci-hcd xhci-hcd.1.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000008020000010
    [    1.763062] xhci-hcd xhci-hcd.1.auto: irq 254, io mem 0x31100000
    [    1.769898] hub 2-0:1.0: USB hub found
    [    1.773711] hub 2-0:1.0: 1 port detected
    [    1.779277] cpufreq: cpufreq_online: CPU0: Running at unlisted initial frequency: 1200000 KHz, changing to: 1250000 KHz
    [    1.791728] mmc0: CQHCI version 5.10
    [    1.791879] mmc1: CQHCI version 5.10
    [    1.834138] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
    [    1.839638] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
    [    1.884629] mmc1: new high speed SDHC card at address aaaa
    [    1.890704] mmcblk1: mmc1:aaaa SK32G 29.7 GiB
    [    1.897012]  mmcblk1: p1 p2
    [    2.013794] mmc0: Command Queue Engine enabled
    [    2.018262] mmc0: new HS200 MMC card at address 0001
    [    2.023755] mmcblk0: mmc0:0001 8GUF4R 7.28 GiB
    [    2.030740]  mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15 p16 p17 p18
    [    2.040369] mmcblk0boot0: mmc0:0001 8GUF4R 31.9 MiB
    [    2.046113] mmcblk0boot1: mmc0:0001 8GUF4R 31.9 MiB
    [    2.051750] mmcblk0rpmb: mmc0:0001 8GUF4R 4.00 MiB, chardev (239:0)
    [    2.082095] vddshv_sdio: Bringing 1800000uV into 3300000-3300000uV
    [    2.085214] clk: Disabling unused clocks
    [    2.095863] ALSA device list:
    [    2.098905]   No soundcards found.
    [    2.718759] EXT4-fs (mmcblk1p2): recovery complete
    [    2.725035] EXT4-fs (mmcblk1p2): mounted filesystem 788cb707-2ee3-4ee4-9e42-d22c8d8dcdfc r/w with ordered data mode. Quota mode: none.
    [    2.737185] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    2.745130] devtmpfs: mounted
    [    2.748777] Freeing unused kernel memory: 2496K
    [    2.753383] Run /sbin/init as init process
    [    3.257369] systemd[1]: System time before build time, advancing clock.
    [    3.343245] NET: Registered PF_INET6 protocol family
    [    3.349028] Segment Routing with IPv6
    [    3.352758] In-situ OAM (IOAM) with IPv6
    [    3.414445] systemd[1]: systemd 255.13^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMMON +UTMP +SYSVINIT default-hierarchy=unified)
    [    3.446385] systemd[1]: Detected architecture arm64.
    
    Welcome to Arago 2023.10!
    
    [    3.466701] systemd[1]: Hostname set to <am62axx-evm>.
    [    3.593378] systemd-sysv-generator[101]: SysV service '/etc/init.d/edgeai-launcher.sh' lacks a native systemd unit file. ~ Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it safe, robust and future-proof. ! This compatibility logic is deprecated, expect removal soon. !
    [    3.820452] systemd[1]: /usr/lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    3.936061] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    4.024608] systemd[1]: Queued start job for default target Graphical Interface.
    [    4.075645] systemd[1]: Created slice Slice /system/getty.
    [  OK  ] Created slice Slice /system/getty.
    [    4.099955] systemd[1]: Created slice Slice /system/modprobe.
    [  OK  ] Created slice Slice /system/modprobe.
    [    4.123933] systemd[1]: Created slice Slice /system/serial-getty.
    [  OK  ] Created slice Slice /system/serial-getty.
    [    4.147343] systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    [    4.170020] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Started Dispatch Password Requests to Console Directory Watch.
    [    4.193920] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Started Forward Password Requests to Wall Directory Watch.
    [    4.217777] systemd[1]: Expecting device /dev/ttyS2...
             Expecting device /dev/ttyS2...
    [    4.233824] systemd[1]: Reached target Path Units.
    [  OK  ] Reached target Path Units.
    [    4.249719] systemd[1]: Reached target Remote File Systems.
    [  OK  ] Reached target Remote File Systems.
    [    4.269703] systemd[1]: Reached target Slice Units.
    [  OK  ] Reached target Slice Units.
    [    4.285721] systemd[1]: Reached target Swaps.
    [  OK  ] Reached target Swaps.
    [    4.338078] systemd[1]: Listening on RPCbind Server Activation Socket.
    [  OK  ] Listening on RPCbind Server Activation Socket.
    [    4.361887] systemd[1]: Reached target RPC Port Mapper.
    [  OK  ] Reached target RPC Port Mapper.
    [    4.388518] systemd[1]: Listening on Process Core Dump Socket.
    [  OK  ] Listening on Process Core Dump Socket.
    [    4.410143] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [    4.434861] systemd[1]: Listening on Journal Audit Socket.
    [  OK  ] Listening on Journal Audit Socket.
    [    4.458384] systemd[1]: Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on Journal Socket (/dev/log).
    [    4.482412] systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
    [    4.498563] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [    4.523361] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    4.546324] systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    [    4.566352] systemd[1]: Listening on User Database Manager Socket.
    [  OK  ] Listening on User Database Manager Socket.
    [    4.617968] systemd[1]: Mounting Huge Pages File System...
             Mounting Huge Pages File System...
    [    4.637838] systemd[1]: Mounting POSIX Message Queue File System...
             Mounting POSIX Message Queue File System...
    [    4.666121] systemd[1]: Mounting Kernel Debug File System...
             Mounting Kernel Debug File System...
    [    4.682247] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing).
    [    4.700082] systemd[1]: Mounting Temporary Directory /tmp...
             Mounting Temporary Directory /tmp...
    [    4.723341] systemd[1]: Starting Create List of Static Device Nodes...
             Starting Create List of Static Device Nodes...
    [    4.750275] systemd[1]: Starting Load Kernel Module configfs...
             Starting Load Kernel Module configfs...
    [    4.770542] systemd[1]: Starting Load Kernel Module drm...
             Starting Load Kernel Module drm...
    [    4.790372] systemd[1]: Starting Load Kernel Module fuse...
             Starting Load Kernel Module fuse...
    [    4.818900] systemd[1]: Starting Start psplash boot splash screen...
             Starting Start psplash boot splash screen...
    [    4.839873] fuse: init (API version 7.39)
    [    4.864055] systemd[1]: Starting RPC Bind...
             Starting RPC Bind...
    [    4.878149] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/).
    [    4.898866] systemd[1]: Starting Journal Service...
             Starting Journal Service...
    [    4.923507] systemd[1]: Starting Load Kernel Modules...
             Starting Load Kernel Modules...
    [    4.943129] systemd[1]: Starting Generate network units from Kernel command line...
             Starting Generate network units from Kernel command line...
    [    4.971649] systemd[1]: Starting Remount Root and Kernel File Systems...
             Starting Remount Root and Kernel File Systems...
    [    4.999119] systemd[1]: Starting Coldplug All udev Devices...
    [    5.008903] systemd-journald[122]: Collecting audit messages is enabled.
    
    [    5.036343] systemd[1]: Started RPC Bind.
    [  OK  ] Started RPC Bind.
    [    5.046015] EXT4-fs (mmcblk1p2): re-mounted 788cb707-2ee3-4ee4-9e42-d22c8d8dcdfc r/w. Quota mode: none.
    [    5.060388] systemd[1]: Mounted Huge Pages File System.
    [  OK  ] Mounted Huge Pages File System.
    [    5.082342] systemd[1]: Started Journal Service.
    [  OK  ] Started Journal Service.
    [  OK  ] Mounted POSIX Message Queue File System.
    [  OK  ] Mounted Kernel Debug File System.
    [  OK  ] Mounted Temporary Directory /tmp.
    [  OK  ] Finished Create List of Static Device Nodes.
    [  OK  ] Finished Load Kernel Module configfs.
    [  OK  ] Finished Load Kernel Module drm.
    [  OK  ] Finished Load Kernel Module fuse.
    [FAILED] Failed to start Start psplash boot splash screen.
    See 'systemctl status psplash-start.service' for details.
    [DEPEND] Dependency failed for Start psplas…temd progress communication helper.
    [  OK  ] Finished Load Kernel Modules.
    [  OK  ] Finished Generate network units from Kernel command line.
    [  OK  ] Finished Remount Root and Kernel File Systems.
             Mounting FUSE Control File System...
             Mounting Kernel Configuration File System...
             Starting Flush Journal to Persistent Storage...
             Starting Apply Kernel Variables...
    [    5.561867] systemd-journald[122]: Received client request to flush runtime journal.
             Starting Create Static Device Nodes in /dev gracefully...
    [  OK  ] Mounted FUSE Control File System.
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Finished Flush Journal to Persistent Storage.
    [  OK  ] Finished Apply Kernel Variables.
    [  OK  ] Finished Coldplug All udev Devices.
    [  OK  ] Finished Create Static Device Nodes in /dev gracefully.
             Starting Create Static Device Nodes in /dev...
    [  OK  ] Finished Create Static Device Nodes in /dev.
    [  OK  ] Reached target Preparation for Local File Systems.
             Mounting /var/volatile...
    [    5.828261] audit: type=1334 audit(1728487094.568:2): prog-id=6 op=LOAD
    [    5.835067] audit: type=1334 audit(1728487094.576:3): prog-id=7 op=LOAD
             Starting Rule-based Manager for Device Events and Files...
    [  OK  ] Mounted /var/volatile.
             Starting Load/Save OS Random Seed...
    [  OK  ] Reached target Local File Systems.
             Starting Create System Files and Directories...
    [  OK  ] Finished Load/Save OS Random Seed.
    [  OK  ] Finished Create System Files and Directories.
    [    6.051841] audit: type=1334 audit(1728487094.792:4): prog-id=8 op=LOAD
             Starting Network Name Resolution...
    [    6.093503] audit: type=1334 audit(1728487094.832:5): prog-id=9 op=LOAD
             Starting Network Time Synchronization...
             Starting Record System Boot/Shutdown in UTMP...
    [    6.148053] audit: type=1334 audit(1728487094.888:6): prog-id=10 op=LOAD
    [    6.154894] audit: type=1334 audit(1728487094.896:7): prog-id=11 op=LOAD
    [    6.161711] audit: type=1334 audit(1728487094.904:8): prog-id=12 op=LOAD
             Starting User Database Manager...
    [  OK  ] Finished Record System Boot/Shutdown in UTMP.
    [  OK  ] Started User Database Manager.
    [  OK  ] Started Rule-based Manager for Device Events and Files.
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Reached target System Time Set.
    [  OK  ] Started Network Name Resolution.
    [  OK  ] Reached target Host and Network Name Lookups.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Started Daily rotation of log files.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Reached target Timer Units.
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
             Starting Docker Socket for the API...
    [  OK  ] Listening on dropbear.socket.
    [  OK  ] Listening on PC/SC Smart Card Daemon Activation Socket.
             Starting Weston socket...
    [    6.851591] audit: type=1334 audit(1728530165.191:9): prog-id=13 op=LOAD
             Starting D-Bus System Message Bus...
             Starting Reboot and dump vmcore via kexec...
    [  OK  ] Listening on Docker Socket for the API.
    [  OK  ] Listening on Weston socket.
    [  OK  ] Found device /dev/ttyS2.
    [  OK  ] Finished Reboot and dump vmcore via kexec.
    [  OK  ] Started D-Bus System Message Bus.
    [    7.143533] dbus-broker-lau[292]: memfd_create() called without MFD_EXEC or MFD_NOEXEC_SEAL set
    [  OK  ] Reached target Socket Units.
    [  OK  ] Reached target Basic System.
    [  OK  ] Started Job spooling tools.
             Starting Avahi mDNS/DNS-SD Stack...
    [  OK  ] Started Periodic Command Scheduler.
             Starting Print notice about GPLv3 packages...
             Starting IPv6 Packet Filtering Framework...
             Starting IPv4 Packet Filtering Framework...
    [  OK  ] Started irqbalance daemon.
             Starting Telephony service...
             Starting Expand the rootfs partiti…to full size of the boot device....
    [  OK  ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf.
    [    7.445430] audit: type=1334 audit(1728530165.787:10): prog-id=14 op=LOAD
    [    7.457497] audit: type=1334 audit(1728530165.799:11): prog-id=15 op=LOAD
             Starting User Login Management...
             Starting Telnet Server...
    [  OK  ] Finished IPv6 Packet Filtering Framework.
    [  OK  ] Finished IPv4 Packet Filtering Framework.
    [  OK  ] Finished Telnet Server.
    [  OK  ] Reached target Preparation for Network.
             Starting Network Configuration...
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [  OK  ] Started Telephony service.
    [  OK  ] Started User Login Management.
    [    8.160075] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [    8.184989] Bluetooth: Core ver 2.22
    [    8.188783] NET: Registered PF_BLUETOOTH protocol family
    [    8.194965] Bluetooth: HCI device and connection manager initialized
    [    8.201717] Bluetooth: HCI socket layer initialized
    [    8.206950] Bluetooth: L2CAP socket layer initialized
    [    8.212166] Bluetooth: SCO socket layer initialized
    [    8.225414] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [    8.231895] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
    [  OK  ] Finished Expand the rootfs partition to full size of the boot device..
    [  OK  ] Started Network Configuration.
    [  OK  ] Reached target Network.
             Starting Enable and configure wl18xx bluetooth stack...
             Starting containerd container runtime...
             Starting LLDP daemon...
    [  OK  ] Started Netperf Benchmark Server.
             Starting Simple Network Management Protocol (SNMP) Daemon....
             Starting Permit User Sessions...
    [  OK  ] Finished Enable and configure wl18xx bluetooth stack.
    [  OK  ] Finished Permit User Sessions.
    [  OK  ] Started Getty on tty1.
    [  OK  ] Started Serial Getty on ttyS2.
    [  OK  ] Reached target Login Prompts.
             Starting Synchronize System and HW clocks...
             Starting Weston, a Wayland compositor, as a system service...
    [  OK  ] Started LLDP daemon.
    [FAILED] Failed to start Synchronize System and HW clocks.
    See 'systemctl status sync-clocks.service' for details.
    [  OK  ] Created slice Slice /system/systemd-fsck.
    [  OK  ] Created slice User Slice of UID 1000.
             Starting File System Check on /dev/mmcblk0p10...
             Starting File System Check on /dev/mmcblk0p11...
             Starting File System Check on /dev/mmcblk0p12...
             Starting File System Check on /dev/mmcblk0p13...
             Starting File System Check on /dev/mmcblk0p14...
             Starting File System Check on /dev/mmcblk0p15...
             Starting File System Check on /dev/mmcblk0p16...
             Starting File System Check on /dev/mmcblk0p17...
             Starting File System Check on /dev/mmcblk0p18...
             Starting User Runtime Directory /run/user/1000...
    [  OK  ] Finished User Runtime Directory /run/user/1000.
             Starting User Manager for UID 1000...
    [   10.839699] kauditd_printk_skb: 2 callbacks suppressed
    [   10.839717] audit: type=1006 audit(1728530169.183:14): pid=1029 uid=0 subj=kernel old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1
    [   10.859511] audit: type=1300 audit(1728530169.183:14): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffd713d518 a2=4 a3=1 items=0 ppid=1 pid=1029 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/usr/lib/systemd/systemd-executor" subj=kernel key=(null)
    [   10.888159] audit: type=1327 audit(1728530169.183:14): proctitle="(systemd)"
             Expecting device /dev/mmcblk1p1...
    [  OK  ] Finished File System Check on /dev/mmcblk0p14.
    [  OK  ] Finished File System Check on /dev/mmcblk0p11.
    [  OK  ] Finished File System Check on /dev/mmcblk0p15.
    [  OK  ] Finished File System Check on /dev/mmcblk0p16.
    [  OK  ] Finished File System Check on /dev/mmcblk0p17.
    [  OK  ] Finished File System Check on /dev/mmcblk0p12.
    [  OK  ] [   11.050566] mc: Linux media interface: v0.10
    Finished File System Check on /dev/mmcblk0p13.
    [  OK  ] Finished File System Check on /dev/mmcblk0p10.
    [  OK  ] Finished File System Check on /dev/mmcblk0p18.
             Mounting /run/media/algorithm_a-mmcblk0p12...
    [   11.155224] videodev: Linux video capture interface: v2.00
             Mounting /run/media/algorithm_b-mmcblk0p13[   11.161853] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fca100
    ...
    [   11.173807] omap-mailbox 29010000.mailbox: omap mailbox rev 0x66fca100
    [   11.180852] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fca100
    [   11.187783] omap-mailbox 29030000.mailbox: no available mbox devices found
             Mounting /run/media/data-mmcblk0p18...
    [   11.215049] EXT4-fs (mmcblk0p12): mounted filesystem 57f8f4bc-abf4-655f-bf67-946fc0f9f25b r/w with ordered data mode. Quota mode: none.
             Mounting /run/media/log-mmcblk0p16...
             Mounting /run/media/persist-mmcblk0p14...
             Mounting /run/media/sign-mmcblk0p17...
    [   11.280478] EXT4-fs (mmcblk0p13): mounted filesystem 57f8f4bc-abf4-655f-bf67-946fc0f9f25b r/w with ordered data mode. Quota mode: none.
    [   11.281818] EXT4-fs (mmcblk0p18): mounted filesystem 57f8f4bc-abf4-655f-bf67-946fc0f9f25b r/w with ordered data mode. Quota mode: none.
             Mounting /run/media/sva_a-mmcblk0p10...
             Mounting /run/media/sva_b-mmcblk0p11...
    [   11.327718] === ox02c10_power_on
             Mounting /run/media/update_data-mmcblk0p15...
    [   11.401913] EXT4-fs (mmcblk0p16): mounted filesystem 57f8f4bc-abf4-655f-bf67-946fc0f9f25b r/w with ordered data mode. Quota mode: none.
    [   11.421415] EXT4-fs (mmcblk0p14): mounted filesystem 57f8f4bc-abf4-655f-bf67-946fc0f9f25b r/w with ordered data mode. Quota mode: none.
    [   11.447516] EXT4-fs (mmcblk0p11): mounted filesystem 57f8f4bc-abf4-655f-bf67-946fc0f9f25b r/w with ordered data mode. Quota mode: none.
    [  OK  ] Mounted /run/media/algorithm_a-mmcblk0p12.
    [   11.467309] === ox02c10_power_on max96714 is locked, loops:1
    [   11.480108] === ox02c10_power_off
    [   11.487262] EXT4-fs (mmcblk0p17): mounted filesystem 57f8f4bc-abf4-655f-bf67-946fc0f9f25b r/w with ordered data mode. Quota mode: none.
    [   11.487540] k3-dsp-rproc 7e000000.dsp: assigned reserved memory node c7x-dma-memory@99800000
    [   11.508669] k3-dsp-rproc 7e000000.dsp: configured DSP for IPC-only mode
    [   11.520345] EXT4-fs (mmcblk0p10): mounted filesystem 57f8f4bc-abf4-655f-bf67-946fc0f9f25b r/w with ordered data mode. Quota mode: none.
    [   11.521030] remoteproc remoteproc0: 7e000000.dsp is available
    [  OK  ] Mounted /run/media/algorithm_b-mmcb[   11.557356] remoteproc remoteproc0: attaching to 7e000000.dsp
    lk0p13.
    [  OK  ] Mounted /run/media/data-mmcblk0p18.
    [  OK  ] Mounted /run/media/log-mmcbl[   11.574428] rproc-virtio rproc-virtio.7.auto: assigned reserved memory node c7x-dma-memory@99800000
    k0p16.
    [   11.577729] EXT4-fs (mmcblk0p15): mounted filesystem 57f8f4bc-abf4-655f-bf67-946fc0f9f25b r/w with ordered data mode. Quota mode: none.
    [   11.596427] virtio_rpmsg_bus virtio0: rpmsg host is online
    [   11.601821] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xd
    [  OK  ] Mounted /run/media/persist-mmcblk0p[   11.616512] rproc-virtio rproc-virtio.7.auto: registered virtio0 (type 7)
    14.
    [  OK  ] Mounted /run/media/sign-mmcblk0p17.
    [   11.638061] remoteproc remoteproc0: remote processor 7e000000.dsp is now attached
    [   11.667124] vdec 30210000.video-codec: error -ENXIO: IRQ index 0 not found
    [   11.668662] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
    [   11.674127] vdec 30210000.video-codec: failed to get irq resource, falling back to polling
    [  OK  ] Mounted /run/media/sva_a-mmcblk0p10[   11.690639] tidss 30200000.dss: [drm] No compatible format found
    .
    [   11.702350] tidss 30200000.dss: [drm] Cannot find any crtc or sizes
    [  OK  ] Mounted /run/media/sva_b-mmcblk0p11[   11.708935] platform 79000000.r5f: configured R5F for IPC-only mode
    .
    [   11.709083] platform 79000000.r5f: assigned reserved memory node r5f-dma-memory@9b800000
    [  OK  ] Mounted /run/media/update_data-mmcblk0p15.
    [   11.753791] remoteproc remoteproc1: 79000000.r5f is available
    [   11.766837] remoteproc remoteproc1: attaching to 79000000.r5f
    [   11.773226] rproc-virtio rproc-virtio.8.auto: assigned reserved memory node r5f-dma-memory@9b800000
    [  OK  ] Found device /dev/mmcblk1p1.
    [   11.805279] vdec 30210000.video-codec: Added wave5 driver with caps: 'ENCODE' 'DECODE'
    [   11.814036] vdec 30210000.video-codec: Product Code:      0x521c
    [   11.820321] vdec 30210000.video-codec: Firmware Revision: 334314
    [   11.840747] virtio_rpmsg_bus virtio1: rpmsg host is online
    [   11.841293] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd
    [   11.854361] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe
    [   11.873909] rproc-virtio rproc-virtio.8.auto: registered virtio1 (type 7)
    [   11.880863] remoteproc remoteproc1: remote processor 79000000.r5f is now attached
             Starting File System Check on /dev/mmcblk1p1...
    [   11.922832] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
    [  OK  ] Started Simple Network Management Protocol (SNMP) Daemon..
    [   11.945804] platform 78000000.r5f: configured R5F for IPC-only mode
    [   11.958879] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9c800000
    [   11.963617] rtc-ti-k3 2b1f0000.rtc: registered as rtc0
    [   11.969944] remoteproc remoteproc2: 78000000.r5f is available
    [   11.987527] remoteproc remoteproc2: attaching to 78000000.r5f
    [   11.993236] rtc-ti-k3 2b1f0000.rtc: setting system clock to 1970-01-01T00:00:10 UTC (10)
    [   12.004251] rproc-virtio rproc-virtio.10.auto: assigned reserved memory node r5f-dma-memory@9c800000
             Expecting device /dev/mmcblk0p8...
    [   12.025385] virtio_rpmsg_bus virtio2: rpmsg host is online
    [   12.031277] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xd
    [   12.038626] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0x15
    [   12.043342] rproc-virtio rproc-virtio.10.auto: registered virtio2 (type 7)
    [   12.046185] virtio_rpmsg_bus virtio2: creating channel ti.ipc4.ping-pong addr 0xe
    [   12.053349] remoteproc remoteproc2: remote processor 78000000.r5f is now attached
    [   12.060491] virtio_rpmsg_bus virtio2: msg received with no recipient
    [   12.074322] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0x15
    [   12.081814] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xe
    [   12.089762] virtio_rpmsg_bus virtio0: msg received with no recipient
             Expecting device /dev/mmcblk0p9...
             Expecting device /dev/mmcblk0p7...
    [  OK  ] Found device /dev/mmcblk0p8.
    [   12.273765] e5010 fd20000.jpeg-encoder: Device registered as /dev/video2
             Starting File System Check on /dev/mmcblk0p8...
    [  OK  ] Finished File System Check on /dev/mmcblk0p8.
    [  OK  ] Found device /dev/mmcblk0p9.
    [  OK  ] Found device /dev/mmcblk0p7.
             Expecting device /dev/mmcblk0p6...
    [   12.489691] === ox02c10_stop_streaming
    [   12.494949] ox02c 0-0010: ox02c10_stop_streaming failed to set stream
             Mounting /run/media/svp_a-mmcblk0p8...
    [   12.510778] ox02c 0-0010: Runtime PM usage count underflow!
             Starting File System Check on /dev/mmcblk0p7   12.524747] handle_lock_status, Image no signal! Reinitialize...
    0m...
             Starting File System Check on /dev/mmcblk0p9...
    [   12.554248] EXT4-fs (mmcblk0p8): mounted filesystem 57f8f4bc-abf4-655f-bf67-946fc0f9f25b r/w with ordered data mode. Quota mode: none.
    [  OK  ] Mounted /run/media/svp_a-mmcblk0p8.
    [  OK  ] Found device /dev/mmcblk0p6.
             Starting File System Check on /dev/mmcblk0p6...
    [  OK  ] Finished File System Check on /dev/mmcblk0p7.
    [  OK  ] Finished File System Check on /dev/mmcblk0p9.
    [FAILED] Failed to start File System Check on /dev/mmcblk0p6.
    See 'systemctl status systemd-fsck@dev-mmcblk0p6.service' for details.
    [DEPEND] Dependency failed for /run/media/rootfs_a-mmcblk0p6.
    [  OK  ] Created slice Slice /system/tee-supplicant.
    [  OK  ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
             Mounting /run/media/rootfs_b-mmcblk0p7...
             Mounting /run/media/svp_b-mmcblk0p9...
             Starting Virtual Console Setup...
    [  OK  ] Started TEE Supplicant on teepriv0.
    [   13.424494] EXT4-fs (mmcblk0p7): mounted filesystem 57f8f4bc-abf4-655f-bf67-946fc0f9f25b r/w with ordered data mode. Quota mode: none.
    [   13.440361] EXT4-fs (mmcblk0p9): mounted filesystem 57f8f4bc-abf4-655f-bf67-946fc0f9f25b r/w with ordered data mode. Quota mode: none.
    [  OK  ] Mounted /run/media/rootfs_b-mmcblk0p7.
    [  OK  ] Mounted /run/media/svp_b-mmcblk0p9.
    [   13.545645] === ox02c10_power_on
    [  OK  ] Started User Manager for UID 1000.
    [  OK  ] Started Session c1 of User weston.
    [   13.583978] audit: type=1006 audit(1728530171.929:15): pid=705 uid=0 subj=kernel old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=2 res=1
    [   13.597666] audit: type=1300 audit(1728530171.929:15): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffc723c8b8 a2=4 a3=1 items=0 ppid=1 pid=705 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/usr/lib/systemd/systemd-executor" subj=kernel key=(null)
    [   13.609670] === ox02c10_power_on max96714 is locked, loops:0
    [   13.625269] audit: type=1327 audit(1728530171.929:15): proctitle="(weston)"
    [  OK  ] Finished File System Check on /dev/mmcblk1p1.
             Mounting /run/media/boot-mmcblk1p1...
    [  OK  ] Finished Virtual Console Setup.
    [   13.895207] ====== ox02c10_set_ctrl V4L2_CID_EXPOSURE
    [   13.900422] ====== ox02c10_set_ctrl V4L2_CID_ANALOGUE_GAIN
    [   13.906016] ====== ox02c10_set_ctrl V4L2_CID_DIGITAL_GAIN
    [   13.911518] ====== ox02c10_set_ctrl V4L2_CID_VFLIP
    [   13.916429] ====== ox02c10_set_ctrl V4L2_CID_VFLIP
    [   13.921322] ====== ox02c10_set_ctrl V4L2_CID_TEST_PATTERN
    [   14.035806] === ox02c10_start_streaming max96714 0x11A = 0x62
    [   14.041915] === ox02c10_start_streaming max96717 0x112 = 0x8a
    [   14.048025] === ox02c10_start_streaming OX02C10 0x4613 = 0x5
    [   14.056522] === ox02c10_start_streaming OX02C10 0x3508 = 0x3
    [   14.064089] === ox02c10_start_streaming OX02C10 0x3509 = 0x0
    [   14.072756] === ox02c10_start_streaming OX02C10 0x4613 = 0x6
    [   14.666176] vdec 30210000.video-codec: Runtime PM usage count underflow!
    [   14.741641] vdec 30210000.video-codec: error -ENXIO: IRQ index 0 not found
    [   14.748568] vdec 30210000.video-codec: failed to get irq resource, falling back to polling
    [   14.760942] vdec 30210000.video-codec: Added wave5 driver with caps: 'ENCODE' 'DECODE'
    [   14.769198] vdec 30210000.video-codec: Product Code:      0x521c
    [   14.775278] vdec 30210000.video-codec: Firmware Revision: 334314
    
     _____                    _____           _         _
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
                  |___|                    |___|
    
    Arago Project am62axx-evm ttyS2
    
    Arago 2023.10 am62axx-evm ttyS2
    
    am62axx-evm login: [   15.044880] audit: type=1701 audit(1728530173.389:16): auid=4294967295 uid=0 gid=0 ses=4294967295 subj=kernel pid=1444 comm="kmsprint" exe="/usr/bin/kmsprint" sig=6 res=1
    [   15.094103] audit: type=1334 audit(1728530173.441:17): prog-id=18 op=LOAD
    [   15.100988] audit: type=1334 audit(1728530173.445:18): prog-id=19 op=LOAD
    [   15.107845] audit: type=1334 audit(1728530173.453:19): prog-id=20 op=LOAD
    [   17.824148] kauditd_printk_skb: 3 callbacks suppressed
    [   17.824163] audit: type=1701 audit(1728530176.169:23): auid=4294967295 uid=0 gid=0 ses=4294967295 subj=kernel pid=1461 comm="edgeai-gui-app" exe="/usr/bin/edgeai-gui-app" sig=6 res=1
    [   17.852897] audit: type=1334 audit(1728530176.197:24): prog-id=21 op=LOAD
    [   17.859847] audit: type=1334 audit(1728530176.205:25): prog-id=22 op=LOAD
    [   17.866717] audit: type=1334 audit(1728530176.213:26): prog-id=23 op=LOAD
    [   18.729910] audit: type=1334 audit(1728530177.077:27): prog-id=23 op=UNLOAD
    [   18.737106] audit: type=1334 audit(1728530177.077:28): prog-id=22 op=UNLOAD
    [   18.744165] audit: type=1334 audit(1728530177.077:29): prog-id=21 op=UNLOAD
    [   18.903052] vdec 30210000.video-codec: Runtime PM usage count underflow!
    [   19.002183] vdec 30210000.video-codec: error -ENXIO: IRQ index 0 not found
    [   19.009109] vdec 30210000.video-codec: failed to get irq resource, falling back to polling
    [   19.021254] vdec 30210000.video-codec: Added wave5 driver with caps: 'ENCODE' 'DECODE'
    [   19.029334] vdec 30210000.video-codec: Product Code:      0x521c
    [   19.035474] vdec 30210000.video-codec: Firmware Revision: 334314
    [   19.056294] audit: type=1701 audit(1728530177.401:30): auid=4294967295 uid=0 gid=0 ses=4294967295 subj=kernel pid=1660 comm="kmsprint" exe="/usr/bin/kmsprint" sig=6 res=1
    [   19.085029] audit: type=1334 audit(1728530177.429:31): prog-id=24 op=LOAD
    [   19.092052] audit: type=1334 audit(1728530177.437:32): prog-id=25 op=LOAD
    ***************************************************************
    ***************************************************************
    NOTICE: This file system contains the following GPL-3.0 packages:
            adwaita-icon-theme-symbolic
            autoconf
            bash-dev
            bash
            bc
            binutils
            cifs-utils
            coreutils-stdbuf
            coreutils
            cpio
            cpp-symlinks
            cpp
            dosfstools
            elfutils-dev
            elfutils
            findutils
            g++-symlinks
            g++
            gawk
            gcc-symlinks
            gcc
            gdb
            gdbserver
            gettext
            glmark2
            gnu-config
            grub-common
            grub-editenv
            grub-efi
            gzip
            hidapi
            kbd-dev
            kbd-keymaps-pine
            less
            libasm1
            libatomic-dev
            libatomic1
            libbfd
            libdebuginfod1
            libdw1
            libelf1
            libgcc-s-dev
            libgcc1
            libgdbm-compat4
            libgdbm-dev
            libgdbm6
            libgettextlib
            libgettextsrc
            libgmp-dev
            libgmp10
            libgmpxx4
            libgnutls-dev
            libgnutls-openssl27
            libidn2-0
            libidn2-dev
            libmpc3
            libmpfr6
            libopcodes
            libqt5charts-examples
            libqt5charts-plugins
            libqt5charts-qmlplugins
            libqt5charts5
            libqt5serialport-examples
            libqt5serialport-plugins
            libqt5serialport-qmlplugins
            libqt5serialport5
            libqt5svg-examples
            libqt5svg-plugins
            libqt5svg-qmlplugins
            libqt5svg5
            libqt5virtualkeyboard-plugins
            libqt5virtualkeyboard-qmlplugins
            libqt5virtualkeyboard5
            libreadline-dev
            libreadline8
            libstdc++-dev
            libstdc++6
            libtasn1-dev
            libunistring-dev
            libunistring5
            m4
            make
            nettle-dev
            nettle
            parted
            piglit
            qt3d-plugins
            qt3d-qmlplugins
            qt3d
            qtbase-examples
            qtbase-plugins
            qtbase-qmlplugins
            qtbase
            qtconnectivity-plugins
            qtconnectivity-qmlplugins
            qtconnectivity
            qtdeclarative-plugins
            qtdeclarative-qmlplugins
            qtdeclarative-tools
            qtdeclarative
            qtgraphicaleffects-qmlplugins
            qtlocation-examples
            qtlocation-plugins
            qtlocation-qmlplugins
            qtlocation
            qtmultimedia-examples
            qtmultimedia-plugins
            qtmultimedia-qmlplugins
            qtmultimedia
            qtquick3d-plugins
            qtquick3d-qmlplugins
            qtquick3d
            qtquics-qmlplugins.control
            qtquics2-plugins.control
            qtquics2-qmlplugins.control
            qtquics2.control
            qtscript-examples
            qtscript-plugins
            qtscript-qmlplugins
            qtscript
            qtwayland-examples
            qtwayland-plugins
            qtwayland-qmlplugins
            qtwayland
            tar
            which
    
    If you do not wish to distribute GPL-3.0 components please remove
    the above packages prior to distribution.  This can be done using
    the opkg remove command.  i.e.:
        opkg remove <package>
    Where <package> is the name printed in the list above
    
    NOTE: If the package is a dependency of another package you
          will be notified of the dependent packages.  You should
          use the --force-removal-of-dependent-packages option to
          also remove the dependent packages as well
    ***************************************************************
    ***************************************************************
    
    am62axx-evm login: root
    [   26.433998] kauditd_printk_skb: 4 callbacks suppressed
    [   26.434012] audit: type=1006 audit(1728530184.781:37): pid=2085 uid=0 subj=kernel old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=3 res=1
    [   26.452778] audit: type=1300 audit(1728530184.781:37): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=fffff221f488 a2=1 a3=1 items=0 ppid=1 pid=2085 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="(systemd)" exe="/usr/lib/systemd/systemd-executor" subj=kernel key=(null)
    [   26.480426] audit: type=1327 audit(1728530184.781:37): proctitle="(systemd)"
    [   26.487517] audit: type=1334 audit(1728530184.797:38): prog-id=27 op=LOAD
    [   26.494364] audit: type=1300 audit(1728530184.797:38): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffd16f8698 a2=90 a3=0 items=0 ppid=1 pid=2085 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/usr/lib/systemd/systemd" subj=kernel key=(null)
    [   26.521231] audit: type=1327 audit(1728530184.797:38): proctitle="(systemd)"
    [   26.528323] audit: type=1334 audit(1728530184.825:39): prog-id=27 op=UNLOAD
    [   26.535336] audit: type=1300 audit(1728530184.825:39): arch=c00000b7 syscall=57 success=yes exit=0 a0=8 a1=1 a2=0 a3=ffff8b95cc60 items=0 ppid=1 pid=2085 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/usr/lib/systemd/systemd" subj=kernel key=(null)
    [   26.562044] audit: type=1327 audit(1728530184.825:39): proctitle="(systemd)"
    [   26.569174] audit: type=1334 audit(1728530184.825:40): prog-id=28 op=LOAD
    [   27.861258] vdec 30210000.video-codec: Runtime PM usage count underflow!
    [   27.922340] vdec 30210000.video-codec: error -ENXIO: IRQ index 0 not found
    [   27.929350] vdec 30210000.video-codec: failed to get irq resource, falling back to polling
    [   27.941393] vdec 30210000.video-codec: Added wave5 driver with caps: 'ENCODE' 'DECODE'
    [   27.949508] vdec 30210000.video-codec: Product Code:      0x521c
    [   27.955717] vdec 30210000.video-codec: Firmware Revision: 334314
    terminate called after throwing an instance of 'std::runtime_error'
      what():  No modesetting DRM card found
    root@am62axx-evm:/opt/edgeai-gst-apps#
    root@am62axx-evm:/opt/edgeai-gst-apps#
    root@am62axx-evm:/opt/edgeai-gst-apps# ls -l /sys/class/video4linux/
    total 0
    lrwxrwxrwx 1 root root 0 Oct 10 03:16 video0 -> ../../devices/platform/bus@f0000/30210000.video-codec/video4linux/video0
    lrwxrwxrwx 1 root root 0 Oct 10 03:16 video1 -> ../../devices/platform/bus@f0000/30210000.video-codec/video4linux/video1
    lrwxrwxrwx 1 root root 0 Oct 10 03:16 video2 -> ../../devices/platform/bus@f0000/fd20000.jpeg-encoder/video4linux/video2
    root@am62axx-evm:/opt/edgeai-gst-apps#
    root@am62axx-evm:/opt/edgeai-gst-apps#
    root@am62axx-evm:/opt/edgeai-gst-apps# dmesg | grep -i video
    [   11.155224] videodev: Linux video capture interface: v2.00
    [   11.667124] vdec 30210000.video-codec: error -ENXIO: IRQ index 0 not found
    [   11.674127] vdec 30210000.video-codec: failed to get irq resource, falling back to polling
    [   11.805279] vdec 30210000.video-codec: Added wave5 driver with caps: 'ENCODE' 'DECODE'
    [   11.814036] vdec 30210000.video-codec: Product Code:      0x521c
    [   11.820321] vdec 30210000.video-codec: Firmware Revision: 334314
    [   12.273765] e5010 fd20000.jpeg-encoder: Device registered as /dev/video2
    [   14.666176] vdec 30210000.video-codec: Runtime PM usage count underflow!
    [   14.741641] vdec 30210000.video-codec: error -ENXIO: IRQ index 0 not found
    [   14.748568] vdec 30210000.video-codec: failed to get irq resource, falling back to polling
    [   14.760942] vdec 30210000.video-codec: Added wave5 driver with caps: 'ENCODE' 'DECODE'
    [   14.769198] vdec 30210000.video-codec: Product Code:      0x521c
    [   14.775278] vdec 30210000.video-codec: Firmware Revision: 334314
    [   18.903052] vdec 30210000.video-codec: Runtime PM usage count underflow!
    [   19.002183] vdec 30210000.video-codec: error -ENXIO: IRQ index 0 not found
    [   19.009109] vdec 30210000.video-codec: failed to get irq resource, falling back to polling
    [   19.021254] vdec 30210000.video-codec: Added wave5 driver with caps: 'ENCODE' 'DECODE'
    [   19.029334] vdec 30210000.video-codec: Product Code:      0x521c
    [   19.035474] vdec 30210000.video-codec: Firmware Revision: 334314
    [   27.861258] vdec 30210000.video-codec: Runtime PM usage count underflow!
    [   27.922340] vdec 30210000.video-codec: error -ENXIO: IRQ index 0 not found
    [   27.929350] vdec 30210000.video-codec: failed to get irq resource, falling back to polling
    [   27.941393] vdec 30210000.video-codec: Added wave5 driver with caps: 'ENCODE' 'DECODE'
    [   27.949508] vdec 30210000.video-codec: Product Code:      0x521c
    [   27.955717] vdec 30210000.video-codec: Firmware Revision: 334314
    root@am62axx-evm:/opt/edgeai-gst-apps#
    root@am62axx-evm:/opt/edgeai-gst-apps#
    root@am62axx-evm:/opt/edgeai-gst-apps#
    

    Best Regards

  • Hi Shawn,

    Have you connected any camera's on your AM62A board?

    You would see ticsi2rx  related devices only when camera is connected. 

    I have successfully used 10.1 SDK image on my AM62A board with no errors and camera's functioning properly.

    Best Regards,

    Suren

  • Hi Suren,

    Yes, the camera on the AM62A board is connected properly, it is the process of initializing the camera driver during power up.

    Normally, the next step would be to get the video stream, but now the wave5 driver is reporting an error, v4l-subdev is not created.

    Best Regards

    Shawn

  • Please share the output of media-ctl -p /dev/media0 on your setup with camera connected.

    The issue seems to be camera related and not wave5.

    Best Regards,

    Suren

  • Please share the output of media-ctl -p /dev/media0 on your setup with camera connected.

    The issue seems to be camera related and not wave5.

    Best Regards,

    Suren

  • The result is as follows:
    Failed to enumerate /dev/media0 (-2)

    However, unrelated to wave5, which module is related to the creation and generation of v4l-subdev?

  • This camera driver file is working fine for me on SDK9.2, the only modification is the probe registration, can you help determine if this is related?

  • Hi Shawn,

    Its related to camera. I will have my colleague respond and help resolve the issue. Expect a response soon!

    Best Regards,

    Suren

  • Thanks, looking forward to having the next update to assist with this issue.

  • Hi Shawn,

    You code snippet looks good - ".probe" is what's needed in Linux 6.6 (SDK 10.1).

    Yes, the camera on the AM62A board is connected properly, it is the process of initializing the camera driver during power up.

    Where is exactly the failure? I can't tell from your screen capture.

    Regards,

    Jianzhong

  • Hi Jianzhong,

    The initialization camera program reported no errors, the log screenshot is the normal initialization process, just to prove that the camera on the AM62A board is connected properly.

    Now the question is, why is there no v4l-subdev node generated?

    Best Regards

    Shawn

  • Hi Shawn,

    To add, here is the complete log printout from my side

    From this log, I can't find anything about csi. Your device tree overlay may have some problem. 

    Can you compare with the boot log of SDK 9.2 and see the difference? The boot log should have the following even if the sensor doesn't probe:

    cdns-csi2rx 30101000.csi-bridge: Probed CSI2RX with 2/4 lanes, 4 streams, external D-PHY

    Regards,

    Jianzhong

  • Hi Jianzhong,

    Okay, yesterday I have analyzed the cause of the problem and solved the issue.

    Best Regards

    Shawn