Tool/software:
Hi
Customer are now researching RTC module of AM62 and need some user guide or example showing how to use this part.
Can you help to provide it?
Thanks
Zekun
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zekun,
Can you let us know what OS are you intending to use, this will help route your query to the rightful expert. (Linux or RTOS).
Best Regards,
Suren
Hi Suren
I find in the academy of RTC usage, which need rtcwake source to move the device from deep sleep mode to normal operation.
https://dev.ti.com/tirex/explore/node?node=A__AYK37rZ2.ceC01eCpxC6jg__AM62-ACADEMY__uiYMDcq__LATEST
But here is customer usage and want to check with you.
The control board based on AM62 will face the power off for more than 1 month. For this scenario, customer want to know if they can provide a battery and a crystal vibration to RTC module, RTC module can be running during the power off state and record the timestamp when power on.
If this solution can not be feasible, they will need an external RTC silicon + battery + crystal vibration to implement this function.
Regards
Zekun
Hi Zekun,
I have routed your query to our expert. Please expect a response soon.
Best Regards,
Suren
Hello Zuken.
Thank you.
But here is customer usage and want to check with you.
The control board based on AM62 will face the power off for more than 1 month. For this scenario, customer want to know if they can provide a battery and a crystal vibration to RTC module, RTC module can be running during the power off state and record the timestamp when power on.
If this solution can not be feasible, they will need an external RTC silicon + battery + crystal vibration to implement this function.
Providing backup power to retain the RTC on the Am62x is not a tested or support option.
After Power-up the RTC module can be configure and using the 32K clock can increment the time.
Regards,
Sreenivasa