Other Parts Discussed in Thread: CC3351,
Tool/software:
Hi team,
We are currently designing a module based on the TI AM623 in combination with the CC3351, and we have a specific requirement regarding the CPSW3G0 RGMII1 interface. Before proceeding further, we would like to confirm the feasibility of the following implementation:
- We need to connect the AM623 CPSW3G0 RGMII1 signals to an external device.
- If the external device operates in MAC mode, we need to configure the AM623 via software to MAC mode.
- If the external device operates in PHY mode, we need to configure the AM623 via software to PHY mode.
In summary, does the AM623 have registers that allow configuring the functionality of GMII pins, such as setting them to PHY mode or MAC mode?
Could you please confirm whether this configuration is achievable using the AM623? If so, are there any specific software or hardware considerations we should be aware of?
If this setup is not feasible, do you have any alternative solutions that can fulfill this requirement? We would appreciate your technical insights and recommendations.
Looking forward to your response.
Best regards,
Sheng