Other Parts Discussed in Thread: OMAP-L137, OMAP-L138
Please find the board details and issue in USB(device mode) below. EVM Board: OMAP-L137 EVIM from spectrum digital. REV-E
Requirement: EVM Board needs to be configured as a bulk device (device mode only, no otg support needed).
Steps taken in the firmware:
- Configured the USB0 and powered up the PHY.
- Able to read the PHY and ctrl registers successfully
- Set the SOFTCON bit. - Enabled all DEVICE and EP# related interrupts.
- Observed(using Osc Scope) the DP(D+) and DM(D-) line in idle state i.e DP-HIGH and DM-LOW And then when connect the EVM board to the host
- DP is pulling down to LOW for some and remained in the same state (DP-Low and DM-Low) around ~18 secs moving back to idle state.
- Results in failing enumeration and windows HOST come up with “USB Device not Recognized” notification.
Please help me to move further