Other Parts Discussed in Thread: LM3S6965, LM35
Hello Sir/Mam,
I want to sense the temperature with Lm35.I have purchased the kit EKS LM3S6965.
For this i take guideline from the folder enet_io which is provided as sample program with this kit. it control the LED & PWM through web page(CGI Script).
Now i connect the LM35 TO THE BOARD such that vcc=+5v, o/p to AIDCO pin of board.
For that i make some changed in file io.c& io_cgi file as
io.c file
//*****************************************************************************
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_pwm.h"
#include "inc/hw_types.h"
#include "driverlib/gpio.h"
#include "driverlib/pwm.h"
#include "driverlib/sysctl.h"
#include "utils/ustdlib.h"
#include "io.h"
#include "driverlib/adc.h"
#define SIZE_VALUEC_BUFFER 32
//*****************************************************************************
//
//*****************************************************************************
unsigned long g_ulFrequency;
unsigned long g_ulDutyCycle;
//*****************************************************************************
//
// Initialize the IO used in this demo
// 1. STATUS LED on Port F pin 0
// 2. PWM on Port D Pin 1 (PWM1)
//
//*****************************************************************************
void
io_init(void)
{
unsigned long ulPWMClock;
//
// Enable GPIO bank F to allow control of the LED.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, 3, 0, ADC_CTL_TS | ADC_CTL_IE |
ADC_CTL_END);
//
// Since sample sequence 3 is now configured, it must be enabled.
//
ADCSequenceEnable(ADC0_BASE, 3);
//
// Clear the interrupt status flag. This is done to make sure the
// interrupt flag is cleared before we sample.
//
ADCIntClear(ADC0_BASE, 3);
//
// Configure Port F0 for as an output for the status LED.
//
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE,GPIO_PIN_0);
//
// Initialize LED to OFF (0)
//
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, 0);
//
// Enable Port D1 for PWM output.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
GPIOPinTypePWM(GPIO_PORTD_BASE,GPIO_PIN_1);
//
// Enable the PWM generator.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM);
//
// Configure the PWM generator for count down mode with immediate updates
// to the parameters.
//
PWMGenConfigure(PWM_BASE, PWM_GEN_0,
PWM_GEN_MODE_DOWN | PWM_GEN_MODE_NO_SYNC);
//
// Divide the PWM clock by 4.
//
SysCtlPWMClockSet(SYSCTL_PWMDIV_4);
//
// Get the PWM clock.
//
ulPWMClock = SysCtlClockGet()/4;
//
// Intialize the PWM frequency and duty cycle.
//
g_ulFrequency = 440;
g_ulDutyCycle = 50;
//
// Set the period of PWM1.
//
//PWMGenPeriodSet(PWM_BASE, PWM_GEN_0, ulPWMClock / g_ulFrequency);
//
// Set the pulse width of PWM1.
//
PWMPulseWidthSet(PWM_BASE, PWM_OUT_1,
((ulPWMClock * g_ulDutyCycle)/100) / g_ulFrequency);
//
// Start the timers in generator 0.
//
PWMGenEnable(PWM_BASE, PWM_GEN_0);
}
//*****************************************************************************
//
// Set the status LED on or off.
//
//*****************************************************************************
void
io_set_led(tBoolean bOn)
{
//
// Turn the LED on or off as requested.
//
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, bOn ? GPIO_PIN_0 : 0);
}
//*****************************************************************************
//
// Turn PWM on/off
//
//*****************************************************************************
void
io_set_pwm(tBoolean bOn)
{
//
// Enable or disable the PWM1 output.
//
PWMOutputState(PWM_BASE, PWM_OUT_1_BIT, bOn);
}
//*****************************************************************************
//
// Set PWM Frequency
//
//*****************************************************************************
/*void
io_pwm_freq(unsigned long ulFreq)
{
unsigned long ulPWMClock;
//
// Get the PWM clock
//
ulPWMClock = SysCtlClockGet()/4;
//
// Set the global frequency
//
g_ulFrequency = ulFreq;
//
// Set the period.
//
PWMGenPeriodSet(PWM_BASE, PWM_GEN_0, ulPWMClock / g_ulFrequency);
//
// Set the pulse width of PWM1
//
PWMPulseWidthSet(PWM_BASE, PWM_OUT_1,
((ulPWMClock * g_ulDutyCycle)/100) / g_ulFrequency);
}
*/
//*****************************************************************************
//
// Set PWM Duty Cycle
//
//*****************************************************************************
void
io_pwm_dutycycle(unsigned long ulDutyCycle)
{
unsigned long ulPWMClock;
//
// Get the PWM clock
//
ulPWMClock = SysCtlClockGet()/4;
//
// Set the global duty cycle
//
g_ulDutyCycle = ulDutyCycle;
//
// Set the period.
//
PWMGenPeriodSet(PWM_BASE, PWM_GEN_0, ulPWMClock / g_ulFrequency);
//
// Set the pulse width of PWM1
//
PWMPulseWidthSet(PWM_BASE, PWM_OUT_1,
((ulPWMClock * g_ulDutyCycle)/100) / g_ulFrequency);
}
//*****************************************************************************
//
// Return LED state
//
//*****************************************************************************
void
io_get_ledstate(char * pcBuf, int iBufLen)
{
//
// Get the state of the LED
//
if(GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_0))
{
usnprintf(pcBuf, iBufLen, "ON");
}
else
{
usnprintf(pcBuf, iBufLen, "OFF");
}
}
//*****************************************************************************
//
// Return LED state as an integer, 1 on, 0 off.
//
//*****************************************************************************
int
io_is_led_on(void)
{
//
// Get the state of the LED
//
if(GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_0))
{
return(1);
}
else
{
return(0);
}
}
void io_get_temp()
{
char pcValueC[SIZE_VALUEC_BUFFER];
// RIT128x96x4Init(1000000);
unsigned long ulADC0_Value[1];
//
// These variables are used to store the temperature conversions for
// Celsius and Fahrenheit.
//
unsigned long ulTemp_ValueC;
// unsigned long ulTemp_ValueF;
//
// Set the clocking to run at 20 MHz (200 MHz / 10) using the PLL. When
// using the ADC, you must either use the PLL or supply a 16 MHz clock
// source.
// TODO: The SYSCTL_XTAL_ value must be changed to match the value of the
// crystal on your board.
//
// SysCtlClockSet(SYSCTL_SYSDIV_10 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
// SYSCTL_XTAL_8MHZ);
//
// The ADC0 peripheral must be enabled for use.
//
// SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
//
// Enable sample sequence 3 with a processor signal trigger. Sequence 3
// will do a single sample when the processor sends a singal to start the
// conversion. Each ADC module has 4 programmable sequences, sequence 0
// to sequence 3. This example is arbitrarily using sequence 3.
//
// ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0);
//
// Configure step 0 on sequence 3. Sample the temperature sensor
// (ADC_CTL_TS) and configure the interrupt flag (ADC_CTL_IE) to be set
// when the sample is done. Tell the ADC logic that this is the last
// conversion on sequence 3 (ADC_CTL_END). Sequence 3 has only one
// programmable step. Sequence 1 and 2 have 4 steps, and sequence 0 has
// 8 programmable steps. Since we are only doing a single conversion using
// sequence 3 we will only configure step 0. For more information on the
// ADC sequences and steps, reference the datasheet.
//
/* ADCSequenceStepConfigure(ADC0_BASE, 3, 0, ADC_CTL_TS | ADC_CTL_IE |
ADC_CTL_END);
//
// Since sample sequence 3 is now configured, it must be enabled.
//
ADCSequenceEnable(ADC0_BASE, 3);
//
// Clear the interrupt status flag. This is done to make sure the
// interrupt flag is cleared before we sample.
//
ADCIntClear(ADC0_BASE, 3);*/
//
// Sample the temperature sensor forever. Display the value on the
// console.
//
// while(1)
// {
//
// Trigger the ADC conversion.
//
ADCProcessorTrigger(ADC0_BASE, 3);
//
// Wait for conversion to be completed.
//
while(!ADCIntStatus(ADC0_BASE, 3, false))
{
}
//
// Read ADC Value.
//
ADCSequenceDataGet(ADC0_BASE, 3, ulADC0_Value);
//
// Use non-calibrated conversion provided in the data sheet. Make
// sure you divide last to avoid dropout.
//
ulTemp_ValueC = ((1475 * 1023) - (2250 * ulADC0_Value[0])) / 10230;
//usnprintf(pcValueC,SIZE_VALUEC_BUFFER,"%d",ulTemp_ValueC);
usnprintf(pcValueC,SIZE_VALUEC_BUFFER,ulTemp_ValueC);
//RIT128x96x4StringDraw(pcValueC,10, 24, 15);
//if(pcValueC<=24)
// RIT128x96x4StringDraw("TURN OFF THE FAN!", 10, 44, 15);
//else if((pcValueC>=25) &&(pcValueC<=35))
//RIT128x96x4StringDraw("MEDIUM SPEED FOR FAN!", 10, 44, 15);
//else
//RIT128x96x4StringDraw("HIGH SPEED FOR FAN!", 10, 44, 15);
//
// This function provides a means of generating a constant length
// delay. The function delay (in cycles) = 3 * parameter. Delay
// 250ms arbitrarily.
//
SysCtlDelay(SysCtlClockGet() / 12);
}
//*****************************************************************************
//
// Return PWM state
//
//*****************************************************************************
void
io_get_pwmstate(char * pcBuf, int iBufLen)
{
//
// Get the state of the PWM1
//
if(HWREG(PWM_BASE + PWM_O_ENABLE) & PWM_OUT_1_BIT)
{
usnprintf(pcBuf, iBufLen, "ON");
}
else
{
usnprintf(pcBuf, iBufLen, "OFF");
}
}
//*****************************************************************************
//
// Return PWM state as an integer, 1 on, 0 off.
//
//*****************************************************************************
int
io_is_pwm_on(void)
{
//
// Get the state of the PWM1
//
if(HWREG(PWM_BASE + PWM_O_ENABLE) & PWM_OUT_1_BIT)
{
return(1);
}
else
{
return(0);
}
}
//*****************************************************************************
//
// Return PWM frequency
//
//*****************************************************************************
/*unsigned long
io_get_pwmfreq(void)
{
//
// Return PWM frequency
//
return g_ulFrequency;
}
*/
//*****************************************************************************
//
// Return PWM duty cycle
//
//*****************************************************************************
unsigned long
io_get_pwmdutycycle(void)
{
//
// Return PWM duty cycle
//
return g_ulDutyCycle;
}
Io_cgi.shtml
<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.01 Transitional//EN">
<html><head>
<meta content="text/html;charset=ISO-8869-1" http-equiv="content-type"><title>I/O Control Demo 2</title>
<script type="text/javascript">
<!--
function SetFormDefaults()
{
document.iocontrol.LEDOn.checked = ls;
document.iocontrol.TEMPSense.value=ts;
document.iocontrol.PWMOn.checked = ps;
document.iocontrol.PWMFrequency.value = pf;
document.iocontrol.PWMDutyCycle.value = pd;
}
//-->
</script>
<style type="text/css">
body
{
font-family: Arial;
background-color: white;
margin: 10px;
padding: 0px
}
h1
{
color: #7C7369;
font-family: Arial;
font-size: 24pt;
font-style: italic;
}
h2
{
color: #000000;
font-family: Arial;
font-size: 18pt;
font-style: bold;
}
h3
{
color: #7C7369;
font-family: Arial;
font-size: 12pt;
font-style: bold;
}
.style1
{
width: 4%;
}
.style2
{
width: 359px;
}
.style3
{
width: 241px;
}
.style4
{
width: 339px;
}
.style5
{
width: 875px;
height: 171px;
}
</style>
</head>
<body onload="SetFormDefaults()">
<!-- Copyright (c) 2009-2010 Texas Instruments Incorporated. All rights reserved. --><!--#FormVars-->
<table width="100%" border="0" cellspacing="0" cellpadding="0">
<tr>
<td align="left" valign="center">
</td>
<td align="center" valign="center">
<h1>CGI Demo</h1>
</td>
</tr>
</table>
<table width="100%">
<tbody>
<tr>
<td align="left" valign="top" class="style1">
<br>
</td>
<td align="left" valign="top" width="75%">
<center>
<h2 align="center"></h2>
</center>
<hr size="2" width="100%">
<ul>
</ul>
<table align="center" border="1" width="80%">
<tbody>
<tr>
<td class="style5">
<form method="get" action="iocontrol.cgi" name="iocontrol">
<table align="center" border="0" cellpadding="2" cellspacing="2"
style="width: 105%">
<tbody>
<tr>
<td align="left" valign="top" class="style2"><b>Control</b></td>
<td align="center" valign="top" class="style3"><b>Current</b></td>
<td align="center" valign="top" class="style4"><b>New</b></td>
</tr>
<tr>
<td align="left" valign="top" class="style2">LED
State</td>
<td align="center" valign="top" class="style3"><!--#LEDtxt--></td>
<td align="center" valign="top" class="style4"><input name="LEDOn" value="1" type="checkbox"></td>
</tr>
<tr>
<td align="left" valign="top" class="style2">Temperature(Degree Celcius)
</td>
<td align="center" valign="top" class="style3"><!--#TEMPSen--></td>
<td align="center" valign="top" class="style4"><input maxlength="4" size="4" name="TEMPSense" value=" "></td>
</tr>
<tr>
<td align="left" valign="top" class="style2">PWM
State</td>
<td align="center" valign="top" class="style3"><!--#PWMtxt--></td>
<td align="center" valign="top" class="style4"><input name="PWMOn" value="1" type="checkbox"></td>
</tr>
<tr>
<td align="left" valign="top" class="style2">PWM
Duty Cycle (%)</td>
<td align="center" valign="top" class="style3"><!--#PWMduty--></td>
<td align="center" valign="top" class="style4"><input maxlength="3" size="3" name="PWMDutyCycle" value=""></td>
</tr>
<tr>
<td colspan="3" rowspan="1" align="center" valign="middle">
<input name="Update" value="Update Settings" type="submit"></td>
</tr>
</tbody>
</table>
</form>
</td>
</tr>
</tbody>
</table>
<ul>
</ul>
<br>
<br>
</td>
</tr>
</tbody>
</table>
<table border="0" cellpadding="0" cellspacing="0" width="100%">
<tbody>
<tr>
<td align="right" valign="center">
<h1><br>
</h1>
</td>
<td align="right" valign="center">
<h3></h3>
</td>
</tr>
</tbody>
</table>
</body></html>
After building, debug it give following page in which temp value is not display.it give the o/p as
Temperature (degree celcius) ***Unknown tag TEMPSen***
with the correct o/p for LED & PWM .
What is solution for that ? I think i have done any mistake while sending temp. to web page.
Thank You in advance
Waiting for replay.