Tool/software:
Hello,
If I am using both the ports of CPSW as an external ethernet ports, then using the third internal port of the CPSW, what application in embedded Linux can be used on AM6442 to be able to monitor the traffic in the CPSW in the real time. Is something like this possible?
Further as an alternate route can we use the PRU2 ethernet port to monitor the internal CPSW traffic? Is something like that already is available in the SDK or not?
Thanks,
Dhruvil