This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM62L ( AM62L32 , AM62L31 ) Custom board hardware design – OSPI (OSPI0) interface implementation (on TMDS62LEVM) guidelines

Part Number: AM62L
Other Parts Discussed in Thread: TMDS62LEVM, , AM62D-Q1, AM62P

Tool/software:

Hi TI Experts,

I have the below queries regarding the OSPI0 peripheral and interface

1. I see x1 OSPI device and x1 QSPI device interfaced on the TMDS62LEVM. Does the AM62L OSPI0 interface support connecting more than x1 devices 

2. Are there some recommendation when interfaced to x1 device and more than x1 devices on the OSPI0 interface 

Let me know your thoughts.

Note:

Collaterals and FAQ that can be referenced during flash selection

e2e.ti.com/.../faq-ospi-faq-for-sitara-jacinto-devices
Section 3 from the following link is helpful:
www.ti.com/.../sprads5.pdf
e2e.ti.com/.../faq-mcu-plus-sdk-am62x-how-to-interface-qspi-flash-part
e2e.ti.com/.../faq-tda4vm-is-there-a-guide-to-choosing-the-right-ospi-flash-parts-that-are-supported-on-jacinto-7
e2e.ti.com/.../am62-am64-am243-tda4vl-tda4al-j721s2-ospi-boot-ospi-flash-vendor-selection
e2e.ti.com/.../am2434-qe-1-quad-fixed-flash-device-for-qspi-boot
www.ti.com/.../sprad50
www.ti.com/.../sprt764
www.ti.com/.../sprad95
www.ti.com/.../SPRUJF5

  • Hi Board designers, 

    Guidance and inputs provided by our device expert: Paul Eaves

    I have listed (highlighted) some of the recommendations (expectations and limitations) board designers are required to be familiar and follow, when connecting two memory devices to the AM62Lx OSPI0 peripheral.   

     

    OSPI0 interface

    The AM62lX supports interfacing to

    • X1 memory device
    • X2 memory devices

     

    Interfacing to x1 memory device

    When interfacing to x1 memory device, recommend following the OSPI0 interface approach that is implemented in AM64x, AM62x, AM62Ax, AM62D-Q1 or AM62Px processor families SKs.

     

    Interfacing to x2 memory devices

    When interfacing to x2 memory devices, the recommendation is to follow the OSPI0 interface approach that is implemented in the AM62L processor family EVM.

     One of the two OSPI/QSPI memory device must provide a DQS output that is connected to the AM62Lx OSPI0_DQS input.  This memory device will use the AM62Lx OSPI0_CLK output as the clock source, and will not use the AM62Lx OSPI0_LBCLKO clock output.  The memory device will be located on the far-end of the OSPI0 data bus.  The memory device will be able to operate at high data transfer rates because it is located at the far-end of the signal traces and will not encounter signal distortion caused by reflections from stubs.

     The second OSPI/QSPI memory device will only operate in non-PHY mode (Tap SDR or Tap DDR), so the memory device does not need a DQS output.  The memory device will use the AM62Lx OSPI0_LBCLKO as its clock source.  The memory device will be located as close to the far-end of the data bus as possible, and connected such that it doesn’t introduce any stubs on the signals.  The memory device is expected (will need) to operate at reduced data transfer rates because it is located in the middle of the signal traces and will encounter signal distortion caused by reflections from stubs.  The maximum data transfer rate must be determined based on the how long it takes for the data signals to settle for a specific board layout implementation.

     

    Configuring x2 memory devices

    The OSPI0 peripheral needs to be configured to communicate with one memory device at a time.  When changing memory devices, the communications channel needs to be gracefully torn-down, the OSPI0 peripheral subsystem is reset, any AM62Lx IOs configuration changes are applied, and the OSPI0 peripheral is reinitialized to operate with the other memory device.  The memory device change is only expected during the AM62Lx boot sequence, where the initial boot image resides in a QSPI or OSPI memory device operating in Tap mode.  After the system boots, the operating system will change to an OSPI memory device operating in one of the faster data transfer modes for run-time storage.

     

    Series resistor on the clock output

    There is no specific requirement for series resistors unless the board designer performs a signal quality simulation and finds a series resistor is need to resolve signal distortion.  There is a possibility that series resistors are need on the far-end of the signals if the memory device attached the far-end has a source impedance that is significantly lower than the signal trace impedance.

    As a good design practice, it is recommended to provision for a series resistor for the clock output near to the processor clock output pin

     

    Terminating the OSPI0 interface Chip select, Clock, INT# and data signals

    Each of the two devices will have their own chip select and clock signals. 

    The recommendation is to pull memory device chip select high since the input has an active low function. The recommended location for the pull-up is near the input that would be floating when the signal is not driven (near the memory device).   

    The recommendation is to pull memory device clock input low. The recommended location for the pulldown is near the input that would be floating when the signal is not driven (near the memory device).   

    The recommendation is to pull memory device data signals D0..D7 (depends on the interface used). There is no preference of location for pull-up placement on the data signals since the signals are bidirectional, and there are times when the signals are not driven by any device.  In this case, all device inputs would be floating without the pull-up resistors.  The biggest difference between the data signals and the chip select and clock signals is the logic state of the data signals are only relevant when they are being driven by one of the devices.  Therefore, we are not worried about noise changing the logic state while no device is actively driving the data signals.  The biggest concern is making sure customers do not create stubs when connecting any of the pull resistors.  One end of each pull resistor should be attached directly to its signal and the other end of the resistor should be routed to the nearest appropriate power rail.  I’m basically saying any signal trace required to connect the pull resistor should be added to the power side rather than the signal side of the resistor.

    The recommendation is to place the pullup for the INT# (open drain output) near to the processor input the interrupt input connects.   The resistor needs to be near the floating input to prevent noise changing its logic state.  The INT# pins on the memory device are outputs, not inputs. 

     

     Connecting x2 OSPI or QSPI memory devices

    There is no hardware reason that prevents using two OSPI devices.  The one connected to the far-end of the bus should be the one configured to operates at a faster data transfer rate and needs its DQS output connected to the AM62Lx OSPI0_DQS input.  The other OSPI device will operate in Tap mode at a slower data transfer rate, so its DQS can be left unconnected since Tap mode doesn’t use this signal and the AM62Lx device only have one DQS input.  There may be some software limitations that need to be considered.  We may need to discuss this topic with the software team.

     Two QSPI devices can be connected, but there may be further limitations with data transfer rates since most QSPI devices do not have a DQS output.  Therefore, it may not be possible for the QSPI device connected to the far-end of the bus to operate at the same speed of a OSPI device that has a DQS output which can be connected the AM62Lx DQS input and used to capture receive data.  Again, there may be some software limitations that need to be considered.

     

    Recommended pullup or pulldown values

    The recommendation is to follow the pull value in the EVM as a starting point. The board designer is responsible for selecting pull resistor values to meets the requirements of their specific system implementation.

     

     Need for placing the pull resistor near the pin that is floating

    Let me explain why it is better to place the pull resistor near the pin that is floating.  We need an external resistor on the chip select and clock signals to prevent the memory inputs from floating since the IOs associated with the OPSI host are turned off (not driven) by default.  These pulls will hold a valid logic state on the chip select and clock signals until software initializes the OSPI host and associated IOs.  It is very difficult to induce a potential that causes problems when a signal is actively driven because it will have a very low impedance to VDD or VSS.  That may not be the case if noise were to couple to a signal trace while not actively driven.  When not actively driven, noise may induce a voltage potential on the signal and the highest impedance end of the signal trace will see the largest potential.  Placing the pull near the memory device minimizes the voltage potential that can be induced at the memory device end of the signal trace.  This makes it harder for noise to cause a logic state change at the memory device input.  We do not want noise to induce an active low state on the chip select input of the memory device since this could cause it to do something unpredictable.  With this connectivity topology, noise would induce the larger potential on the OSPI host IO.  This can be problematic for the OSPI host IOs if the induced potential exceeds the Absolute Maximum Ratings limits of the IO cell.  If this happens the system designer will need to find a way to eliminate or reduce noise coupling

     

    What is the reason we selected pulldown instead of pullup for OSPI0 or other peripherals?

    Because there are cases where the clock is stopped or paused in a low logic state and the pull-down option is consistent with this logic state.

     

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Inputs related to OSPI0-Nor read or write performnce.

     https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1585031/am62l-am62l-ospi-write-performance 

    We have connected MRAM to the OSPI(as Quad-SPI) of the AM62L and are measuring the read and write performance.
    The PSDK is using version 11.00.15.05.
    I am checking how much the performance improves when changing the OSPI clock frequency(OSPI_CLK) to 25MHz, 50MHz, and 100MHz.
     
    When performing a 512KB full area read using the dd command, the read time decreases proportionally with the frequency.(25MHz: 43ms, 50MHz: 20ms, 100MHz: 8ms)
     
    However, in the case of writing, the writing time becomes slightly shorter according to the frequency, but it is not as short as the read time. (25MHz: 127ms, 50MHz: 104ms, 100MHz: 98ms)

    For ospi-nor, read performance is generally scalable proportionally with the interface clock, but on write, while you can speed up the command and data transfer phases by increasing the clock frequency, the actual programming time remains constant. This is why NOR flash write performance doesn't scale linearly with clock frequency beyond a certain point.

    Are you using the Linux kernel driver on the specific MRAM device? or you're using the generic Linux kernel cadence qspi-nor driver?

    If the generic qspi-nor driver is used, kernel drive might poll the busy signal or bit, but MRAM doesn't have busy signal or bit on write. That may explain the MRAM write performance vs the clock frequency you observed on your testing.

    Regards,

    Sreenivasa

  • Hi Board Designers, 

    Inputs related to recommended pulldown value for the attached memory device pulldown:

    Memory interface peripherals pulldown value AM62x or Am64x 

    I have a few customer using 1K pulldown for some of the signals from the SOC mostly for memory interfaces.

    Wanted to get your thoughts on the use case.

    The current draw from the IO seems more and could affect the VOH. Any thoughts on the use case please.

    I agree the 1k resistor could impact the VOH level to the attached device, and it could also impact our VIHSS level if our receiver is turned on. 

     

    The customer should run a simulation of their system using the IBIS models of each device connected to the signal to determine if the output can achieve an appropriate levels after accounting for the output buffer drive capability, worst case pull resistance, and worst case leakage of all attached components.  I would suggest they consider a 4.7k if there is a concern with 10k.

    information on sizing of external pulls.

    A resistor must be selected that is able to hold the signal above the steady-state high (VIHSS) or below the steady-state low (VILSS) based on the signals worst-case combination of leakage, which will be the sum of the max leakage of all attached devices. 

    For example, if it is assumed AM62P is connected to a single UART device that has a max leakage of 5uA when operating at 1.8V.  The worst-case leakage would be 10uA + 5uA = 15uA.  VIHSS for the LVCMOS IO cell operating at 1.8V is 0.85 x VDD = 1.53V.  A pull-up resistor value would need to be at less than 18k ohms to hold the voltage above 1.53V for a worst-case leakage of 15uA.  It is suggested to use a value that is less than 18K ohm for this example.

    Hi Board Designers, 

    Inputs related to external pullup resistor 

    (+) AM625: Enable pulls on OSPI/QSPI signals in ROM bootloader - Processors forum - Processors - TI E2E support forums

    As mentioned above, we do not turn on internal pulls of pins that support multiplexed signal functions because we do not know what is going to be connected to these pins. Turning on internal pulls by default could introduce a mid-supply condition on signals if the attached device has an internal pull turned on by default that is in contention with the AM62x internal pull.

    You may ask, why not have the ROM code turn on the internal pulls once it detects OSPI boot mode. The answer to this question is, because the inputs of the attached device would be left floating until the ROM code detects OSPI boot mode and configures the internal pulls. 

    Creating a condition where signals are held in a mid-supply state or allowing signals to float is a bad design practice, so we recommend external pulls on the signals to ensure the attached device inputs are held in a valid logic state as soon as power is applied.

    You should never allow a digital signal to float.
    Some device input buffers may tolerate floating or mid-supply voltage for long periods of time, but in general it is not a good design practice to allow this to happen because the input buffer will have its p-channel and n-channel transistors partially turned on when its input is at mid-supply. This causes shoot-through current to flow from VDD to VSS through the input buffer. Too much time spent in this condition can stress the circuits in the input buffer, which can result in electromigration issues or premature aging of the transistors.

    You should never allow a mid-supply voltage on any AM62x input buffer when its RXACTIVE bit in the respective PADCONFIG register is enabled. It is okay to apply a mid-supply voltage to a AM62x input when the RXACTIVE bit is disabled. The second paragraph of the note following the Connectivity Requirements table addresses this concern by saying "Any IO with its input buffer (RX) turned off is allowed to float without damaging the device. However, any IO with its input buffer (RX) turned on shall never be allowed to float to any potential between VILSS and VIHSS. The input buffer can enter a high-current state which could damage the IO cell if allowed to float between these levels."
    This concern is also addressed by the minimum input slew rate parameter in each of the Electrical Characteristics tables. The signal should never spend more than 1000ns in the voltage transition region between VILSS and VIHSS. The 1000ns limit applies for signal toggle frequency up to 100kHz. The min slew rate decreases as a function of toggle frequency once the signal toggle rate increases above 100kHz.
    In the case where no OSPI device is connected, you can leave the pins unconnected as long as you ensure software never enables the RXACTIVE bit and you do not connect any PCB signal trace to the pins.

    Regards,

    Sreenivasa