Part Number: PROCESSOR-SDK-AM64X
Other Parts Discussed in Thread: TMDS64EVM, SYSCONFIG, DP83869
Tool/software:
I am running Linux on the A53 cores, and I want to control a networking interface with an R5F core. How do I get the Linux cores and the R5F core to run alongside each other?
This FAQ will show an example of getting a specific networking example running alongside Linux. The same concepts will apply to other networking examples.
This FAQ builds on concepts that are covered in the AM64x academy's Multicore module:
https://dev.ti.com/tirex/explore/node?node=A__AJa64F6ctzZNbb.TYx4mCA__AM64-ACADEMY__WI1KRXP__LATEST
This FAQ uses the following configuration:
* AM64x MCU+ SDK 10.1, AM64x Linux SDK 10.1 (files for SDK 9.2 are in appendix)
* AM64x EVM (TMDS64EVM)
A53: Linux
R5F0-0: RTOS
Boot media: Linus SDK SD Card image
Boot flow: SPL (the default in Linux SDK)
R5F example: ENET Lwip ICSSG