Part Number: AM5729
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
If im not able to flash is the processor working
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Assigned expert is currently out of office, please expect delay in response.
Regards,
Manojna
Hello Nishalini,
Can you share more details?
What is the SW being used?
Is this a custom or TI board?
Any details/logs of the failure?
-Josue
Hi Josue,
SW- Code composer Studio
This is custom board
We dont have logs as we need to flash first to get logs
Nishalini,
What is the procedure that you are following in order to flash QSPI? are you trying to use UNIFLASH?
-Josue
after i load program out file in tx i can see its being high and low for working processor, but in not working processor its always high in 3 v
Nishalini,
Can you please delineate your exact procedure with logs/pictures you are following and UNIFLASH version?
What Host are you Using? (Windows/Linux)
There should be logs from the UNIFLASH tool.
You could also use other methods to load QSPI as explained in the following FAQ: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/959283/faq-ccs-am5728-am57xx-boot-modes-supported
I do not understand what you are communicating with the following:
tx i can see its being high and low for working processor, but in not working processor its always high in 3 v
Can you please explain?