This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA829V: Main2_1 is receiving additional data bytes in Eth payload from CPSW-9G

Part Number: DRA829V

Tool/software:

Port 1 and 2 of 88q5050 we are doing Ingress Monitoring and Port 7 is Destination port.

we are observing additional bytes in payload and Type also got changed as highlited, With different scenario lenth and bytes are different.

Input:

Detail View
[-] Ethernet
| Destination: 02:C4:46:18:1E:02
| Source: 02:C4:46:18:1E:01
| Type: IPv4 0800
[-] Payload
| Length 46 bytes
| 45 00 00 2E 00 00 40 00 40 11 3A C0 00 00 00 00 00 00 00 00 00 00 00 00 00 1A FF BA 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

Output:

Destination Address: 0x02c446181e02
Source Address: 0x02c446181e01
Type/Length: 0x8100
Payload: 0x018f91000000840c000108004500002e0000400040113ac0000000000000000000000000001affba000000000000000000000000000000000000