This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AL-Q1: IMX728 image problem

Part Number: TDA4AL-Q1

Tool/software:

Hi, TI expert,

I have a project that needs to bring up the imx728 sensor driver.

And, I find the TI support the D3 IMX728 sensor driver with IQ tuning on the SDK of ti-processor-sdk-rtos-j721s2-evm-10_01_00_04.tar.gz.

So, I try to run the run_app_single_cam.sh in vision app with this SDK.

But when I run this app, the image is shown a hidden pattern in left side on image, please check the below.

Do you have same issue on your side?

Note: I use the evm board for test, but it not use FPD link, use FPC connect to camera module directly.

I remove some related function about the Serializer and Deserializer. 

raw:

yuv:

Thanks.

YL