This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A consequence due to overexposure

hi everyone,

I've encountered a problem while using DM365.

the problem is that when camera captures a frame with overexposure and non-overexposure parts at the same time,

some unexpected lines appear in the non-overexposure part.

it is normal if the image without overexposure, so I think these lines should result from the overexposure.

following is the image with unexpected lines:

and the most strange thing is,

the original resolution is 1080p but if I change the resolution to 720p

I get a nomal image:

I've searched for this kind of problem in this forum but find nothing.

does anybody encounter the same problem?

or does anybody have any sense of solving this problem?

thanks