This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TDA4AEN-Q1: How to measure power consumption on Linux using the on board INA226

Part Number: TDA4AEN-Q1
Other Parts Discussed in Thread: INA226

Tool/software:

Can we use Linux to enable the on-board INA226 instances to measure power?

  • Hello,

    Using the below patch we can enable the INA226 to measure power on TDA4AEN/AM67-EVM.

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/0001_2D00_arm64_2D00_dts_2D00_ti_2D00_k3_2D00_j722s_2D00_evm_2D00_Add_2D00_INA226_2D00_nodes_2D00_for_2D00_power.patch

    Download the above patch to:

    $SDK_Path/board-support/ti-linux-kernel-6.6.44+git-ti
    cd $SDK_Path/board-support/ti-linux-kernel-6.6.44+git-ti
    git am 0001-arm64-dts-ti-k3-j722s-evm-Add-INA226-nodes-for-power.patch
    cd ../..
    make linux


    Steps to install the new dtb to SD card:

    Edit $SDK_Path/Rules.make file sudh that ROOTFS_PART=/media/$USER/root
    Insert the SD card of 10.1 SDK.

    sudo make linux-install

    Once you boot with SD after the above steps you can see the hwmon interfaces in Linux giving Live power numbers:

    root@j722s-evm:~# cat /sys/class/hwmon/hwmon*/power1_input
    1962500
    81250
    12500
    81250
    0
    18750
    18750
    5281250
    181250
    68750
    81250
    
    Above are the power numbers in micro Watts
    
    root@j722s-evm:~# cat /sys/class/hwmon/hwmon*/in1_input                                                                                                          
    863
    850
    3300
    1798
    749
    1800
    1798
    3300
    1099
    3295
    1801
    
    Above are the voltage rails in milli Volts

    Note: I have used the latest 10.1 Linux SDK to enable the feature.

    Best Regards,
    Keerthy