This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: [SDK 9.0] How to remove default TI boot logo and process psplash ok

Part Number: AM625


Tool/software:

Hello TI

We are using SDK 9.0 Yocto linux.

We failed to remove the default TI boot logo and progress bar on our system image.

We don't know the detail of psplash operation/setting, please guide.

We try to remove the psplash in the image we build by adding below bbappend in our meta-custom :

ti_am62x/sources/meta-custom/recipes-core/images$ cat tisdk-default-image.bbappend
# Remove splash screen package
IMAGE_INSTALL:remove = "psplash"
IMAGE_FEATURES:remove = "splash"

Then, after power on, the psplash is removed our system (no psplash binary or its run file).

But we found that our LCD and backlight is off and when we try to display a picture ,  sudo fbi -d /dev/fb0 -a  /tmp/img.png, then it shows nothing.

Based on our observation (not remove psplash) case:

1. When power on, we see the default TI boot logo and progress bar is shown "once" on our lcd, but in the following next power on, it does not show any thing on our lcd.

2. When we run " #/usr/bin/psplash" on shell,  we found this binary  in /etc/init.d/psplash.sh ,  the TI boot logo is shown and run  sudo fbi -d /dev/fb0 -a  /tmp/img.png, we could see the img.png on the LCD. 

It seems that to make custom image display, psplash is needed (?). 

How to remove the psplash and make our display works (lcd/backlight-able to display img.png)? 

Below is log:

U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
SPL initial stack usage: 13376 bytes
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE:  BL31: Built : 00:42:57, Jan 13 2023

U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
SPL initial stack usage: 1856 bytes
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted


U-Boot 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)

SoC:   AM62X SR1.0 GP
Model: Texas Instruments AM625 SK
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed -1
DRAM:  2 GiB
Core:  67 devices, 29 uclasses, devicetree: separate
MMC:   mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed -1
Net:   eth0: ethernet@8000000port@1
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
574 bytes read in 14 ms (40 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
## Error: "main_cpsw0_qsgmii_phyinit" not defined
21768704 bytes read in 881 ms (23.6 MiB/s)
58901 bytes read in 20 ms (2.8 MiB/s)
Working FDT set to 88000000
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
ERROR: reserving fdt memory region failed (addr=ff700000 size=8ca000 flags=4)
   Loading Device Tree to 000000008feee000, end 000000008fffffff ... OK
Working FDT set to 8feee000

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.1.33-g40c32565ca (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.3.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Thu Jul  6 14:17:24 UTC 2023
[    0.000000] Machine model: Texas Instruments AM625 SK
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] printk: bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB
[    0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB
[    0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009c7fffff]
[    0.000000]   node   0: [mem 0x000000009c800000-0x000000009e6fffff]
[    0.000000]   node   0: [mem 0x000000009e700000-0x000000009e77ffff]
[    0.000000]   node   0: [mem 0x000000009e780000-0x000000009fffffff]
[    0.000000]   node   0: [mem 0x00000000a0000000-0x00000000ff6fffff]
[    0.000000]   node   0: [mem 0x00000000ff700000-0x00000000fffc9fff]
[    0.000000]   node   0: [mem 0x00000000fffca000-0x00000000ffffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.2
[    0.000000] percpu: Embedded 19 pages/cpu s38376 r8192 d31256 u77824
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 516096
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),98048k@32m(ospi.rootfs),256k@130816k(ospi.phypattern);omap2-nand.0:2m(NAND.tiboot3),2m(NAND.tispl),2m(NAND.tiboot3.backup),4m(NAND.u-boot),256k(NAND.u-boot-env),256k(NAND.u-boot-env.backup),-(NAND.file-system) root=PARTUUID=a84e93f1-02 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] Memory: 1836936K/2097152K available (13120K kernel code, 1418K rwdata, 4324K rodata, 2240K init, 503K bss, 129144K reserved, 131072K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000]  Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 256 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000080040000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080050000
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.008538] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.019225] pid_max: default: 32768 minimum: 301
[    0.024000] LSM: Security Framework initializing
[    0.028866] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.036451] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.046283] cblist_init_generic: Setting adjustable number of callback queues.
[    0.053743] cblist_init_generic: Setting shift to 2 and lim to 1.
[    0.060049] cblist_init_generic: Setting shift to 2 and lim to 1.
[    0.066444] rcu: Hierarchical SRCU implementation.
[    0.071350] rcu:     Max phase no-delay instances is 1000.
[    0.076960] Platform MSI: msi-controller@1820000 domain created
[    0.083279] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
[    0.093134] EFI services will not be available.
[    0.098068] smp: Bringing up secondary CPUs ...
[    0.103368] Detected VIPT I-cache on CPU1
[    0.103480] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[    0.103499] GICv3: CPU1: using allocated LPI pending table @0x0000000080060000
[    0.103556] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.104289] Detected VIPT I-cache on CPU2
[    0.104363] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[    0.104378] GICv3: CPU2: using allocated LPI pending table @0x0000000080070000
[    0.104412] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.105030] Detected VIPT I-cache on CPU3
[    0.105112] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[    0.105127] GICv3: CPU3: using allocated LPI pending table @0x0000000080080000
[    0.105160] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.105225] smp: Brought up 1 node, 4 CPUs
[    0.184961] SMP: Total of 4 processors activated.
[    0.189774] CPU features: detected: 32-bit EL0 Support
[    0.195046] CPU features: detected: CRC32 instructions
[    0.200367] CPU: All CPU(s) started at EL2
[    0.204564] alternatives: applying system-wide alternatives
[    0.212171] devtmpfs: initialized
[    0.223917] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.233919] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.245509] pinctrl core: initialized pinctrl subsystem
[    0.251503] DMI not present or invalid.
[    0.256072] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.263334] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[    0.270903] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.279013] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.287203] audit: initializing netlink subsys (disabled)
[    0.292899] audit: type=2000 audit(0.188:1): state=initialized audit_enabled=0 res=1
[    0.293325] thermal_sys: Registered thermal governor 'step_wise'
[    0.300830] thermal_sys: Registered thermal governor 'power_allocator'
[    0.307014] cpuidle: using governor menu
[    0.317884] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.324919] ASID allocator initialised with 65536 entries
[    0.343978] platform 30200000.dss: Fixed dependency cycle(s) with /display
[    0.352876] KASLR disabled due to lack of seed
[    0.364770] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.371744] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.378154] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.385093] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.391501] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.398441] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.404849] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.411788] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.419976] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected
[    0.431022] iommu: Default domain type: Translated
[    0.436039] iommu: DMA domain TLB invalidation policy: strict mode
[    0.442765] SCSI subsystem initialized
[    0.446992] usbcore: registered new interface driver usbfs
[    0.452641] usbcore: registered new interface driver hub
[    0.458095] usbcore: registered new device driver usb
[    0.463855] mc: Linux media interface: v0.10
[    0.468268] videodev: Linux video capture interface: v2.00
[    0.473911] pps_core: LinuxPPS API ver. 1 registered
[    0.478987] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.488335] PTP clock support registered
[    0.492475] EDAC MC: Ver: 3.0.0
[    0.496659] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100
[    0.503806] FPGA manager framework
[    0.507383] Advanced Linux Sound Architecture Driver Initialized.
[    0.514627] clocksource: Switched to clocksource arch_sys_counter
[    0.521140] VFS: Disk quotas dquot_6.6.0
[    0.525193] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.533351] NET: Registered PF_INET protocol family
[    0.538636] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.547889] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[    0.556699] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.564636] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.572842] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[    0.580830] TCP: Hash tables configured (established 16384 bind 16384)
[    0.587746] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.594672] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.602224] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.608495] RPC: Registered named UNIX socket transport module.
[    0.614576] RPC: Registered udp transport module.
[    0.619386] RPC: Registered tcp transport module.
[    0.624195] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.630786] NET: Registered PF_XDP protocol family
[    0.635700] PCI: CLS 0 bytes, default 64
[    0.640512] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[    0.650673] Initialise system trusted keyrings
[    0.655491] workingset: timestamp_bits=46 max_order=19 bucket_order=0
[    0.667820] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.674492] NFS: Registering the id_resolver key type
[    0.679736] Key type id_resolver registered
[    0.684014] Key type id_legacy registered
[    0.688179] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.695034] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.702624] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[    0.709243] 9p: Installing v9fs 9p2000 file system support
[    0.749490] Key type asymmetric registered
[    0.753682] Asymmetric key parser 'x509' registered
[    0.758729] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[    0.766464] io scheduler mq-deadline registered
[    0.771105] io scheduler kyber registered
[    0.778768] pinctrl-single 4084000.pinctrl: 34 pins, size 136
[    0.785327] pinctrl-single f4000.pinctrl: 171 pins, size 684
[    0.792135] pinctrl-single a40000.pinctrl: 512 pins, size 2048
[    0.800402] clk_mcasp1: gpio_clk_driver_probe: Can't get 'enable' named GPIO property
[    0.808433] gpio-clk: probe of clk_mcasp1 failed with error -2
[    0.820121] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
[    0.836631] loop: module loaded
[    0.841292] megasas: 07.719.03.00-rc1
[    0.849393] tun: Universal TUN/TAP device driver, 1.6
[    0.855397] thunder_xcv, ver 1.0
[    0.858745] thunder_bgx, ver 1.0
[    0.862069] nicpf, ver 1.0
[    0.865248] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[    0.872636] hns3: Copyright (c) 2017 Huawei Corporation.
[    0.878130] hclge is initializing
[    0.881544] e1000: Intel(R) PRO/1000 Network Driver
[    0.886530] e1000: Copyright (c) 1999-2006 Intel Corporation.
[    0.892438] e1000e: Intel(R) PRO/1000 Network Driver
[    0.897512] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    0.903593] igb: Intel(R) Gigabit Ethernet Network Driver
[    0.909112] igb: Copyright (c) 2007-2014 Intel Corporation.
[    0.914838] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[    0.921246] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    0.927438] sky2: driver version 1.30
[    0.931940] VFIO - User Level meta-driver version: 0.3
[    0.938051] usbcore: registered new interface driver usb-storage
[    0.944553] Gt9xx driver installing..
[    0.948348] >> i2c_add_driver - ret : 0x0
[    0.952939] i2c_dev: i2c /dev entries driver
[    0.958152] usbcore: registered new interface driver uvcvideo
[    0.965942] sdhci: Secure Digital Host Controller Interface driver
[    0.972310] sdhci: Copyright(c) Pierre Ossman
[    0.977299] Synopsys Designware Multimedia Card Interface Driver
[    0.983933] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.990654] ledtrig-cpu: registered to indicate activity on CPUs
[    0.997015] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    1.003990] usbcore: registered new interface driver usbhid
[    1.009694] usbhid: USB HID core driver
[    1.015050] optee: probing for conduit method.
[    1.019644] optee: revision 3.20 (8e74d476)
[    1.019966] optee: dynamic shared memory is enabled
[    1.029499] optee: initialized driver
[    1.035914] Initializing XFRM netlink socket
[    1.040342] NET: Registered PF_PACKET protocol family
[    1.045652] 9pnet: Installing 9P2000 support
[    1.050092] Key type dns_resolver registered
[    1.054924] registered taskstats version 1
[    1.059148] Loading compiled-in X.509 certificates
[    1.073226] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
[    1.142339] at24 0-0051: supply vcc not found, using dummy regulator
[    1.170806] at24 0-0051: 65536 byte 24c512 EEPROM, writable, 64 bytes/write
[    1.178255] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
[    1.185321] i2c 1-0044: Fixed dependency cycle(s) with /bus@f0000/ticsi2rx@30102000/csi-bridge@30101000
[    1.195582] tas2505-codec 1-0018: tas2505_i2c_probe: clock-source = MCLK
[    1.202522] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz
[    1.208675] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
[    1.217018] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
[    1.226280] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[    1.236528] ti-udma 485c0100.dma-controller: Number of rings: 82
[    1.244708] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
[    1.255860] ti-udma 485c0000.dma-controller: Number of rings: 150
[    1.265907] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
[    1.276181] printk: console [ttyS2] disabled
[    1.280691] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 240, base_baud = 3000000) is a 8250
[    1.289590] printk: console [ttyS2] enabled
[    1.289590] printk: console [ttyS2] enabled
[    1.298053] printk: bootconsole [ns16550a0] disabled
[    1.298053] printk: bootconsole [ns16550a0] disabled
[    1.309329] 2840000.serial: ttyS4 at MMIO 0x2840000 (irq = 242, base_baud = 3000000) is a 8250
[    1.319062] 2860000.serial: ttyS6 at MMIO 0x2860000 (irq = 243, base_baud = 3000000) is a 8250
[    1.330563] spi-nor spi0.0: s28hs512t (65536 Kbytes)
[    1.335667] 7 fixed-partitions partitions found on MTD device fc40000.spi.0
[    1.342630] Creating 7 MTD partitions on "fc40000.spi.0":
[    1.348024] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[    1.354856] 0x000000080000-0x000000280000 : "ospi.tispl"
[    1.361272] 0x000000280000-0x000000680000 : "ospi.u-boot"
[    1.367727] 0x000000680000-0x0000006c0000 : "ospi.env"
[    1.373974] 0x0000006c0000-0x000000700000 : "ospi.env.backup"
[    1.380792] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[    1.387378] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[    1.395837] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[    1.442647] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    1.451902] mdio_bus 8000f00.mdio: MDIO device at address 1 is missing.
[    1.458524] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867
[    1.466663] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
[    1.479620] am65-cpsw-nuss 8000000.ethernet: Use random MAC address
[    1.485889] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
[    1.493017] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[    1.499525] pps pps0: new PPS source ptp0
[    1.503846] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[    1.514324] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[    1.523467] (NULL device *): taeha0203x, Searching for format with pixel format: 0x59565955
[    1.531843] (NULL device *): taeha0203x Format found: 0x59565955
[    1.537842] (NULL device *): Filling V4L2 format for CSI format: 0x59565955
[    1.544794] (NULL device *): Initial width: 640, height: 480, bpp: 16
[    1.551224] (NULL device *): Pixels in word: 8
[    1.555660] (NULL device *): Clamped and rounded width: 640
[    1.561223] (NULL device *): Clamped height: 480
[    1.566670] (NULL device *): taeha0203x, Searching for format with pixel format: 0x59565955
[    1.575056] (NULL device *): taeha0203x Format found: 0x59565955
[    1.581056] (NULL device *): Filling V4L2 format for CSI format: 0x59565955
[    1.588007] (NULL device *): Initial width: 640, height: 480, bpp: 16
[    1.594437] (NULL device *): Pixels in word: 8
[    1.598874] (NULL device *): Clamped and rounded width: 640
[    1.604437] (NULL device *): Clamped height: 480
[    1.609745] (NULL device *): taeha0203x, Searching for format with pixel format: 0x59565955
[    1.618091] (NULL device *): taeha0203x Format found: 0x59565955
[    1.624088] (NULL device *): Filling V4L2 format for CSI format: 0x59565955
[    1.631039] (NULL device *): Initial width: 640, height: 480, bpp: 16
[    1.637470] (NULL device *): Pixels in word: 8
[    1.641907] (NULL device *): Clamped and rounded width: 640
[    1.647470] (NULL device *): Clamped height: 480
[    1.652760] (NULL device *): taeha0203x, Searching for format with pixel format: 0x59565955
[    1.661103] (NULL device *): taeha0203x Format found: 0x59565955
[    1.667101] (NULL device *): Filling V4L2 format for CSI format: 0x59565955
[    1.674050] (NULL device *): Initial width: 640, height: 480, bpp: 16
[    1.680481] (NULL device *): Pixels in word: 8
[    1.684917] (NULL device *): Clamped and rounded width: 640
[    1.690481] (NULL device *): Clamped height: 480
[    1.696972] cdns-csi2rx 30101000.csi-bridge: Probed CSI2RX with 4/4 lanes, 4 streams, external D-PHY
[    1.709873] mmc0: CQHCI version 5.10
[    1.710359] mmc1: CQHCI version 5.10
[    1.718295] mmc2: CQHCI version 5.10
[    1.728480] [gtp_probe:1962]
[    1.732377] goodix-ts 0-005d: GTP Driver Version: V2.8.0.2<2017/12/14>
[    1.738899] goodix-ts 0-005d: GTP I2C Address: 0x5d
[    1.743779] goodix-ts 0-005d: Unset touchscreen-max-id, use default
[    1.747236] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[    1.750040] goodix-ts 0-005d: touch input parameters is [id x y w p]<16 800 480 1024 1024>
[    1.758300] mmc2: SDHCI controller on fa20000.mmc [fa20000.mmc] using ADMA 64-bit
[    1.758308] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[    1.765753] goodix-ts 0-005d: int-sync enabled
[    1.765759] goodix-ts 0-005d: driver-send-cfg enabled
[    1.765769] goodix-ts 0-005d: auto-update-cfg enabled
[    1.791382] mmc1: new high speed SDHC card at address 59b4
[    1.795212] goodix-ts 0-005d: esd-protect enabled
[    1.795217] goodix-ts 0-005d: type-a-report enabled
[    1.801583] mmcblk1: mmc1:59b4 SN32G 29.7 GiB
[    1.813446]  mmcblk1: p1 p2
[    1.817542] goodix-ts 0-005d: get RST [0x1f2] INT [0x1f1] from DTS
[    1.823764] goodix-ts 0-005d: supply vdd_ana not found, using dummy regulator
[    1.823896] mmc0: Command Queue Engine enabled
[    1.831100] goodix-ts 0-005d: supply vcc_i2c not found, using dummy regulator
[    1.835376] mmc0: new HS200 MMC card at address 0001
[    1.836111] mmcblk0: mmc0:0001 0IM20E 29.6 GiB
[    1.842675] goodix-ts 0-005d: Failed get pinctrl state:output_high
[    1.849958] mmcblk0boot0: mmc0:0001 0IM20E 31.5 MiB
[    1.852032] goodix-ts 0-005d: Success request irq-gpio
[    1.859409] mmcblk0boot1: mmc0:0001 0IM20E 31.5 MiB
[    1.863160] goodix-ts 0-005d: Success request rst-gpio
[    1.869277] mmcblk0rpmb: mmc0:0001 0IM20E 4.00 MiB, chardev (239:0)
[    1.873251] goodix-ts 0-005d: Guitar reset
[    1.966772] goodix-ts 0-005d: GTP reset Guitar
[    1.973739] goodix-ts 0-005d: I2C Addr is 5d
[    1.981300] goodix-ts 0-005d: IC Version: 911_1060
[    1.986822] goodix-ts 0-005d: Config group5 used,length: 186
[    1.996463] goodix-ts 0-005d: Driver send config
[    2.021347] goodix-ts 0-005d: Use type A report protocol
[    2.027167] input: goodix-ts as /devices/virtual/input/input0
[    2.033163] goodix-ts 0-005d: INT num 275, trigger type:2
[    2.038996] goodix-ts 0-005d: create proc entry gt9xx_config success
[    2.045417] goodix-ts 0-005d: Alloc memory size:1534.
[    2.050476] goodix-ts 0-005d: I2C function: without pre and end cmd!
[    2.056836] goodix-ts 0-005d: Create proc entry success!
[    2.062160] goodix-ts 0-005d: ESD on
[    2.066166] tp2855 1-0044: tp2855 probe starts
[    2.070790] tp2855 1-0044: tp2855 probe reset gpio = 0
[    2.075972] tp2855 1-0044: tp2855 probe tp2855->clk = 29794688
[    2.081810] tp2855 1-0044: xvclk rate: 27000000 Hz
[    2.086596] tp2855 1-0044: tp2855 Probe hardware reset
[    2.102630] tp2855 1-0044: tp2855 probe init decoder registers IN/OUT
[    2.164120] tp2855 1-0044: tp2855, tp2855_start_stream and init ALL registors
[    2.214632] tp2855 1-0044: tp2855,  init ALL registors end
[    2.225145] tp2855 1-0044: tp2855  chip id found id_high = 0x28, id_low = 0x55
[    2.232803] tp2855 1-0044: Initialize the subdev and its controls finish.
[    2.239631] tp2855 1-0044: Consider updating driver tp2855 to match on endpoints
[    2.248410] tp2855 1-0044: tp2855 probed  successfully
[    2.256523] tas2505-codec 1-0018: tas2505_codec_probe: Probe finished
[    2.263081] tas2505-codec 1-0018: tas2505_set_dai_sysclk: clk_id: 0, freq: 12288000
[    2.273401] tas2505-codec 1-0018: tas2505_set_dai_sysclk: id [0] tas2505->sysclk: 12288000, freq: 12288000
[    2.286868] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[    2.308538] ALSA device list:
[    2.312152]   #0: TAS2505
[    2.616991] EXT4-fs (mmcblk1p2): recovery complete
[    2.626583] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none.
[    2.635226] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    2.643262] devtmpfs: mounted
[    2.647728] Freeing unused kernel memory: 2240K
[    2.652399] Run /sbin/init as init process
[    4.043774] systemd[1]: System time before build time, advancing clock.
[    4.327779] NET: Registered PF_INET6 protocol family
[    4.335550] Segment Routing with IPv6
[    4.339375] In-situ OAM (IOAM) with IPv6
[    4.490129] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[    4.523282] systemd[1]: Detected architecture arm64.

Welcome to Arago 2023.04!

[    4.641958] systemd[1]: Hostname set to <am62xx-evm>.
[    4.959424] systemd-sysv-generator[161]: SysV service '/etc/init.d/resize_rootfs.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    4.984730] systemd-sysv-generator[161]: SysV service '/etc/init.d/dropbear' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    5.011314] systemd-sysv-generator[161]: SysV service '/etc/init.d/netperf' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    5.035562] systemd-sysv-generator[161]: SysV service '/etc/init.d/sysrepo' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    5.062737] systemd-sysv-generator[161]: SysV service '/etc/init.d/inetd.busybox' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    5.087576] systemd-sysv-generator[161]: SysV service '/etc/init.d/psplash.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    5.117223] systemd-sysv-generator[161]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    5.142818] systemd-sysv-generator[161]: SysV service '/etc/init.d/telnetd' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    5.166937] systemd-sysv-generator[161]: SysV service '/etc/init.d/docker.init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    5.210805] systemd-sysv-generator[161]: SysV service '/etc/init.d/netopeer2-server' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    5.732381] systemd[1]: Configuration file /etc/systemd/system/ti-apps-launcher.service is marked executable. Please remove executable permission bits. Proceeding anyway.
[    5.841364] systemd[1]: /lib/systemd/system/startwlansta.service:7: Unknown key name 'After' in section 'Service', ignoring.
[    5.854803] systemd[1]: /lib/systemd/system/startwlanap.service:7: Unknown key name 'After' in section 'Service', ignoring.
[    5.919055] systemd[1]: /lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[    6.014894] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[    6.132269] systemd[1]: Queued start job for default target Graphical Interface.
[    6.225704] systemd[1]: Created slice Slice /system/getty.
[  OK  ] Created slice Slice /system/getty.
[    6.250082] systemd[1]: Created slice Slice /system/modprobe.
[  OK  ] Created slice Slice /system/modprobe.
[    6.274514] systemd[1]: Created slice Slice /system/serial-getty.
[  OK  ] Created slice Slice /system/serial-getty.
[    6.297807] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[    6.319347] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Started Dispatch Password …ts to Console Directory Watch.
[    6.343342] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Started Forward Password R…uests to Wall Directory Watch.
[    6.367493] systemd[1]: Reached target Path Units.
[  OK  ] Reached target Path Units.
[    6.383079] systemd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[    6.402892] systemd[1]: Reached target Slice Units.
[  OK  ] Reached target Slice Units.
[    6.419063] systemd[1]: Reached target Swaps.
[  OK  ] Reached target Swaps.
[    6.513425] systemd[1]: Listening on RPCbind Server Activation Socket.
[  OK  ] Listening on RPCbind Server Activation Socket.
[    6.535202] systemd[1]: Reached target RPC Port Mapper.
[  OK  ] Reached target RPC Port Mapper.
[    6.572986] systemd[1]: Listening on Process Core Dump Socket.
[  OK  ] Listening on Process Core Dump Socket.
[    6.595797] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[    6.620743] systemd[1]: Listening on Journal Audit Socket.
[  OK  ] Listening on Journal Audit Socket.
[    6.644218] systemd[1]: Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket (/dev/log).
[    6.669738] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Journal Socket.
[    6.688902] systemd[1]: Listening on Network Service Netlink Socket.
[  OK  ] Listening on Network Service Netlink Socket.
[    6.712709] systemd[1]: Listening on udev Control Socket.
[  OK  ] Listening on udev Control Socket.
[    6.737126] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[    6.761226] systemd[1]: Listening on User Database Manager Socket.
[  OK  ] Listening on User Database Manager Socket.
[    6.819360] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
[    6.842493] systemd[1]: Mounting POSIX Message Queue File System...
         Mounting POSIX Message Queue File System...
[    6.899446] systemd[1]: Mounting Kernel Debug File System...
         Mounting Kernel Debug File System...
[    6.915566] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
[    6.942476] systemd[1]: Mounting Temporary Directory /tmp...
         Mounting Temporary Directory /tmp...
[    6.971275] systemd[1]: Starting Create List of Static Device Nodes...
         Starting Create List of Static Device Nodes...
[    7.019825] systemd[1]: Starting Load Kernel Module configfs...
         Starting Load Kernel Module configfs...
[    7.041966] systemd[1]: Starting Load Kernel Module drm...
         Starting Load Kernel Module drm...
[    7.065863] systemd[1]: Starting Load Kernel Module fuse...
         Starting Load Kernel Module fuse...
[    7.259585] fuse: init (API version 7.37)
[    7.279996] systemd[1]: Starting Start psplash boot splash screen...
         Starting Start psplash boot splash screen...
[    7.314018] systemd[1]: Starting RPC Bind...
         Starting RPC Bind...
[    7.331509] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
[    7.388067] systemd[1]: Starting Journal Service...
         Starting Journal Service...
[    7.468854] systemd[1]: Starting Load Kernel Modules...
         Starting Load Kernel Modules...
[    7.543868] systemd[1]: Starting Generate network units from Kernel command line...
         Starting Generate network …ts from Kernel command line...
[    7.598340] cryptodev: loading out-of-tree module taints kernel.
[    7.603754] systemd[1]: Starting Remount Root and Kernel File Systems...
         Starting Remount Root and Kernel File Systems cryptodev: driver 1.12 loaded.
[0m...
[    7.643551] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none.
[    7.655886] systemd[1]: Starting Coldplug All udev Devices...
         Starting Coldplug All udev Devices...
[    7.691447] systemd[1]: Started RPC Bind.
[  OK  ] Started RPC Bind.
[    7.711752] systemd[1]: Mounted Huge Pages File System.
[  OK  ] Mounted Huge Pages File System.
[    7.735607] systemd[1]: Mounted POSIX Message Queue File System.
[  OK  ] Mounted POSIX Message Queue File System.
[    7.759723] systemd[1]: Mounted Kernel Debug File System.
[  OK  ] Mounted Kernel Debug File System.
[    7.783680] systemd[1]: Mounted Temporary Directory /tmp.
[  OK  ] Mounted Temporary Directory /tmp.
[    7.807713] systemd[1]: Started Journal Service.
[  OK  ] Started Journal Service.
[  OK  ] Finished Create List of Static Device Nodes.
[  OK  ] Finished Load Kernel Module configfs.
[  OK  ] Finished Load Kernel Module drm.
[  OK  ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star…progress communication helper.
[  OK  ] Finished Load Kernel Modules.
[  OK  ] Finished Generate network units from Kernel command line.
[  OK  ] Finished Remount Root and Kernel File Systems.
         Mounting FUSE Control File System...
         Mounting Kernel Configuration File System...
         Starting Flush Journal to Persistent Storage...
         Starting Apply Kernel Variables...
[    8.168222] systemd-journald[176]: Received client request to flush runtime journal.
         Starting Create Static Device Nodes in /dev...
[  OK  ] Mounted FUSE Control File System.
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Finished Flush Journal to Persistent Storage.
[  OK  ] Finished Apply Kernel Variables.
[  OK  ] Finished Create Static Device Nodes in /dev.
[  OK  ] Reached target Preparation for Local File Systems.
         Mounting /media/ram...
         Mounting /var/volatile...
[    8.408886] audit: type=1334 audit(1651167749.376:2): prog-id=5 op=LOAD
[    8.415714] audit: type=1334 audit(1651167749.384:3): prog-id=6 op=LOAD
         Starting Rule-based Manage…for Device Events and Files...
[  OK  ] Finished Coldplug All udev Devices.
[  OK  ] Mounted /media/ram.
[  OK  ] Mounted /var/volatile.
         Starting Load/Save Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Finished Create Volatile Files and Directories.
         Starting Network Time Synchronization...
         Starting Record System Boot/Shutdown in UTMP...
[  OK  ] Started Rule-based Manager for Device Events and Files.
[  OK  ] Finished Record System Boot/Shutdown in UTMP.
[    9.039962] systemd-journald[176]: Oldest entry in /run/log/journal/fee9e02077a946f4a1ec2f0a2c1dd2b7/system.journal is older than the configured file retention duration (1month), suggesting rotation.
[    9.058749] systemd-journald[176]: /run/log/journal/fee9e02077a946f4a1ec2f0a2c1dd2b7/system.journal: Journal header limits reached or header out-of-date, rotating.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target System Time Set.
[  OK  ] Started Daily rotation of log files.
[  OK  ] Reached target Timer Units.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[    9.198148] pwm-backlight backlight: supply power not found, using dummy regulator
[  OK  ] Listening on D-Bus System Message Bus Socket.
[    9.277785] rtc rtc0: Unknown quartz-load-femtofarads value: 1250. Assuming 12500
         Starting Docker Socket for the API...
[    9.313429] rtc-pcf8523 1-0068: registered as rtc0
[    9.320843] rtc-pcf8523 1-0068: setting system clock to 2025-03-13T04:50:12 UTC (1741841412)
[  OK  ] Listening on dropbear.socket.
         Starting Weston socket...
         Starting D-Bus System Message Bus...
         Starting Reboot and dump vmcore via kexec.[    9.501497] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@9cb00000
..
[    9.506829] rtc-ti-k3 2b1f0000.rtc: registered as rtc1
[    9.522243] k3-m4-rproc 5000000.m4fss: configured M4 for remoteproc mode
[    9.530017] k3-m4-rproc 5000000.m4fss: local reset is deasserted for device
[  OK  ] Listening on Docker Socket for the API.
[    9.554323] remoteproc remoteproc0: 5000000.m4fss is available
[  OK  ] Listening on Weston socket.
[  OK  ] Found device /dev/ttyS2.
[  OK  ] Reached target Socket Units.
[    9.612663] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[    9.625321] CAN device driver interface
[    9.629349] platform 78000000.r5f: configured R5F for IPC-only mode
[    9.635899] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9da00000
[    9.644425] remoteproc remoteproc1: 78000000.r5f is available
[    9.650432] remoteproc remoteproc1: attaching to 78000000.r5f
[    9.657162] platform 78000000.r5f: R5F core initialized in IPC-only mode
[    9.658667] random: crng init done
[    9.663958] rproc-virtio rproc-virtio.1.auto: assigned reserved memory node r5f-dma-memory@9da00000
[    9.677153] virtio_rpmsg_bus virtio0: rpmsg host is online
[    9.677595] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[    9.682769] rproc-virtio rproc-virtio.1.auto: registered virtio0 (type 7)
[    9.690455] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[    9.697033] remoteproc remoteproc1: remote processor 78000000.r5f is now attached
[   10.024102] m_can_platform 4e00000.can: m_can device registered (irq=0, version=32)
[   10.034206] m_can_platform 4e10000.can: m_can device registered (irq=0, version=32)
[   10.036196] PVR_K:  206: Device: fd00000.gpu
[   10.046587] PVR_K:  206: Read BVNC 33.15.11.3 from HW device registers
[   10.054860] PVR_K:  206: RGX Device registered with BVNC 33.15.11.3
[   10.062753] [drm] Initialized pvr 23.1.6404501 20170530 for fd00000.gpu on minor 0
[   10.090654] remoteproc remoteproc0: powering up 5000000.m4fss
[   10.096580] remoteproc remoteproc0: Booting fw image am62-mcu-m4f0_0-fw, size 54860
[   10.109971] rproc-virtio rproc-virtio.2.auto: assigned reserved memory node m4f-dma-memory@9cb00000
[   10.128361] virtio_rpmsg_bus virtio1: rpmsg host is online
[   10.129786] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd
[   10.134089] rproc-virtio rproc-virtio.2.auto: registered virtio1 (type 7)
[   10.144674] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe
[   10.148481] remoteproc remoteproc0: remote processor 5000000.m4fss is now up
[  OK  ] Finished Load/Save Random Seed.
[   10.207257] panel-simple display: supply power not found, using dummy regulator
[   10.215317] panel-simple display: Specify missing bus_flags
[   10.226834] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 1
[   10.237316] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device
[  OK  ] Finished Reboot and dump vmcore via kexec.
[  OK  ] Started D-Bus System Message Bus.
[  OK  ] Reached target Basic System.
         Starting Save/Restore Sound Card State...
[  OK  ] Started Job spooling tools.
[  OK  ] Started Periodic Command Scheduler.
         Starting Print notice about GPLv3 packages...
         Starting IPv6 Packet Filtering Framework...
         Starting IPv4 Packet Filtering Framework...
[  OK  ] Started irqbalance daemon.
         Starting startwlanap...
         Starting startwlansta...
[   11.063173] audit: type=1334 audit(1741841414.240:4): prog-id=7 op=LOAD
[   11.075110] audit: type=1334 audit(1741841414.252:5): prog-id=8 op=LOAD
         Starting User Login Management...
[  OK  ] Started TEE Supplicant.
         Starting telnetd.service...
[  OK  ] Started ti-apps-launcher service.
[  OK  ] Finished Save/Restore Sound Card State.
[  OK  ] Finished IPv6 Packet Filtering Framework.
[  OK  ] Finished IPv4 Packet Filtering Framework.
[  OK  ] Started startwlanap.
[  OK  ] Started startwlansta.
[  OK  ] Started telnetd.service.
[   11.386906] remoteproc remoteproc2: 30074000.pru is available
[   11.394500] remoteproc remoteproc3: 30078000.pru is available
[   11.453646] dwc3 31000000.usb: Configuration mismatch. dr_mode forced to gadget
[  OK  ] Created slice Slice /system/systemd-backlight.
[  OK  ] Reached target Preparation for Network.
[  OK  ] Reached target Sound Card.
         Starting LSB: Expand Rootfs of boot device...
         Starting Load/Save Screen …ness of backlight:backlight...
         Starting Network Configuration...
[   11.718737] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[   11.736331] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[  OK  ] Reached target Hardware activated USB gadget.
[  OK  ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
[   11.910597] xhci-hcd xhci-hcd.3.auto: xHCI Host Controller
[   11.916341] xhci-hcd xhci-hcd.3.auto: new USB bus registered, assigned bus number 1
[   11.924368] xhci-hcd xhci-hcd.3.auto: USB3 root hub has no ports
[   11.930471] xhci-hcd xhci-hcd.3.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000000000010010
[   11.940106] xhci-hcd xhci-hcd.3.auto: irq 459, io mem 0x31100000
[  OK  ] Finished Load/Save Screen …htness[   11.992232] hub 1-0:1.0: USB hub found
 of backlight:backlight.
[   12.001948] hub 1-0:1.0: 1 port detected
[  OK  ] Started User Login Management.
[   12.262741] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[   12.416832] usb-storage 1-1:1.0: USB Mass Storage device detected
[   12.423960] scsi host0: usb-storage 1-1:1.0
[  OK  ] Started Network Configuration.
[   13.012785] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
         Starting Wait for Network to be Configured...
         Starting Network Name Resolution...
[   13.093974] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[   13.103481] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[  OK  ] Started LSB: Expand Rootfs of boot device.
[   13.459909] scsi 0:0:0:0: Direct-Access     SanDisk  Cruzer Blade     1.00 PQ: 0 ANSI: 6
[   13.471777] sd 0:0:0:0: [sda] 30031872 512-byte logical blocks: (15.4 GB/14.3 GiB)
[   13.480880] sd 0:0:0:0: [sda] Write Protect is off
[   13.486521] sd 0:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA
[   13.508721]  sda: sda1
[   13.512126] sd 0:0:0:0: [sda] Attached SCSI removable disk
[  OK  ] Started Network Name Resolution.
[  OK  ] Reached target Network.
[  OK  ] Reached target Host and Network Name Lookups.
         Starting Avahi mDNS/DNS-SD Stack...
         Starting Enable and configure wl18xx bluetooth stack...
         Starting containerd container runtime...
[  OK  ] Started Netperf Benchmark Server.
[  OK  ] Started NFS status monitor for NFSv2/3 locking..
         Starting Simple Network Ma…ent Protocol (SNMP) Daemon....
         Starting Permit User Sessions...
[  OK  ] Finished Enable and configure wl18xx bluetooth stack.
[  OK  ] Finished Permit User Sessions.
[  OK  ] Started Serial Getty on ttyS2.
[  OK  ] Reached target Login Prompts.
         Starting Synchronize System and HW clocks...
[   14.341423] startwlanap.sh[633]: sed: unmatched '/'
[   14.466283] startwlanap.sh[634]: adding wlan1 interface
[   14.892944] startwlanap.sh[656]: command failed: No such file or directory (-2)
[  OK  ] Finished Synchronize System and HW clocks.
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[  OK  ] Created slice Slice /system/systemd-fsck.
[  OK  ] Found device Cruzer_Blade MYUSB1.
         Starting File System Check on /dev/sda1...
         Starting File System Check on /dev/mmcblk1p1...
[  OK  ] Finished File System Check on /dev/mmcblk1p1.
         Mounting /run/media/boot-mmcblk1p1...
[  OK  ] Mounted /run/media/boot-mmcblk1p1.
[   16.394062] startwlanap.sh[687]: SIOCSIFADDR: No such device
[   16.408112] startwlanap.sh[687]: wlan1: ERROR while getting interface flags: No such device
[   16.418914] startwlanap.sh[687]: SIOCSIFNETMASK: No such device
[   16.434802] startwlanap.sh[687]: wlan1: ERROR while getting interface flags: No such device
[   16.669782] startwlanap.sh[657]: Line 499: unknown configuration item 'wep_rekey_period'
[   16.670989] startwlanap.sh[657]: 1 errors found in configuration file '/usr/share/wl18xx/hostapd.conf'
[   16.671664] startwlanap.sh[657]: Failed to set up interface with /usr/share/wl18xx/hostapd.conf
[   16.672637] startwlanap.sh[657]: Failed to initialize interface
[  OK  ] Finished File System Check on /dev/sda1.
         Mounting /run/media/MYUSB1-sda1...
[  OK  ] Mounted /run/media/MYUSB1-sda1.
[   19.608851] audit: type=1325 audit(1741841422.696:6): table=nat family=2 entries=0 op=xt_register pid=701 comm="iptables"
[   19.620000] audit: type=1300 audit(1741841422.696:6): arch=c00000b7 syscall=209 success=yes exit=0 a0=4 a1=0 a2=40 a3=fffff0b8c9c8 items=0 ppid=634 pid=701 auid=4294967295 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=4294967295 comm="iptables" exe="/usr/sbin/xtables-legacy-multi" key=(null)
[   19.648060] audit: type=1327 audit(1741841422.696:6): proctitle=69707461626C6573002D74006E6174002D4100504F5354524F5554494E47002D6F0065746830002D6A004D415351554552414445
[   19.663181] audit: type=1325 audit(1741841422.784:7): table=nat family=2 entries=5 op=xt_replace pid=701 comm="iptables"
[   19.674130] audit: type=1300 audit(1741841422.784:7): arch=c00000b7 syscall=208 success=yes exit=0 a0=4 a1=0 a2=40 a3=2937210 items=0 ppid=634 pid=701 auid=4294967295 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=4294967295 comm="iptables" exe="/usr/sbin/xtables-legacy-multi" key=(null)
[   19.701738] audit: type=1327 audit(1741841422.784:7): proctitle=69707461626C6573002D74006E6174002D4100504F5354524F5554494E47002D6F0065746830002D6A004D415351554552414445

 _____                    _____           _         _
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
              |___|                    |___|

Arago Project am62xx-evm -

Arago 2023.04 am62xx-evm -

am62xx-evm login: [   20.565505] startwlanap.sh[712]: iperf3: error - unable to start listener for connections: Cannot assign requested address
[   20.566307] startwlanap.sh[712]: iperf3: exiting

am62xx-evm login: root
[   28.783784] audit: type=1334 audit(1741841431.960:8): prog-id=9 op=LOAD
[   28.792497] audit: type=1334 audit(1741841431.968:9): prog-id=10 op=LOAD
[   29.287670] audit: type=1006 audit(1741841432.464:10): pid=732 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[   29.300343] audit: type=1300 audit(1741841432.464:10): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffe0fee7b8 a2=1 a3=ffff88277020 items=0 ppid=1 pid=732 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
[   29.326843] audit: type=1327 audit(1741841432.464:10): proctitle="(systemd)"
[   29.360835] audit: type=1334 audit(1741841432.536:11): prog-id=11 op=LOAD
[   29.367869] audit: type=1300 audit(1741841432.536:11): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffea1d9790 a2=78 a3=0 items=0 ppid=1 pid=732 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="systemd" exe="/lib/systemd/systemd" key=(null)
[   29.393411] audit: type=1327 audit(1741841432.536:11): proctitle="(systemd)"
[   29.400683] audit: type=1334 audit(1741841432.536:12): prog-id=11 op=UNLOAD
[   29.407951] audit: type=1334 audit(1741841432.536:13): prog-id=12 op=LOAD
root@am62xx-evm:~#
root@am62xx-evm:~# weston &
[1] 749
root@am62xx-evm:~# Date: 2025-03-13 UTC
[04:50:36.822] weston 10.0.2
               https://wayland.freedesktop.org
               Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
               Build: 10.0.2
[04:50:36.822] Command line: weston
[04:50:36.822] OS: Linux, 6.1.33-g40c32565ca, #1 SMP PREEMPT Thu Jul  6 14:17:24 UTC 2023, aarch64
[04:50:36.823] Flight recorder: enabled
[04:50:36.826] Using config file '/etc/xdg/weston/weston.ini'
[04:50:36.852] Output repaint window is 7 ms maximum.
[04:50:36.857] Loading module '/usr/lib/libweston-10/wayland-backend.so'
[04:50:37.906] Error: Failed to retrieve wl_shm from parent Wayland compositor
[04:50:37.906] BUG: layer_list is not empty after shutdown. Calls to weston_layer_fini() are missing somwhere.
[04:50:37.906] fatal: failed to create compositor backend

[1]+  Done(1)                 weston
root@am62xx-evm:~#
root@am62xx-evm:~# mkdir /tmp/myusb
root@am62xx-evm:~# mount /dev/sda1 /tmp/myusb
root@am62xx-evm:~# cd /tmp/myusb/
root@am62xx-evm:/tmp/myusb# ls
'System Volume Information'   img.png   img2.jpeg   img3.png   tp630_os
root@am62xx-evm:/tmp/myusb# sudo fbi -d /dev/fb0 -a img.png
using "DejaVu Sans Mono-16", pixelsize=16.67 file=/usr/share/fonts/truetype/DejaVuSansMono.ttf
trying fbdev: /dev/fb0 ...
ioctl VT_GETSTATE: Inappropriate ioctl for device
ioctl VT_GETMODE: Inappropriate ioctl for device
NOTICE: No vt switching available on terminal.
NOTICE: Not started from linux console?  CONFIG_VT=n?
WARNING: Running on framebuffer and can't manage access.
WARNING: Other processes (fbcon too) can write to display.
WARNING: Also can't properly cleanup on exit.
img.png
root@am62xx-evm:/tmp/myusb#
root@am62xx-evm:/tmp/myusb# echo "nothing display on screen. It is black, backlight is also not on"
nothing display on screen. It is black, backlight is also not on
root@am62xx-evm:/tmp/myusb# /usr/bin/psplash
Error Cannot open /dev/tty0: No such file or directory
warning: FBIOPUT_VSCREENINFO failed, double buffering disabled


root@am62xx-evm:/tmp/myusb# sudo fbi -d /dev/fb0 -a img.png n"
using "DejaVu Sans Mono-16", pixelsize=16.67 file=/usr/share/fonts/truetype/DejaVuSansMono.ttf
trying fbdev: /dev/fb0 ...
ioctl VT_GETSTATE: Inappropriate ioctl for device
ioctl VT_GETMODE: Inappropriate ioctl for device
NOTICE: No vt switching available on terminal.
NOTICE: Not started from linux console?  CONFIG_VT=n?
WARNING: Running on framebuffer and can't manage access.
WARNING: Other processes (fbcon too) can write to display.
WARNING: Also can't properly cleanup on exit.
img.png
root@am62xx-evm:/tmp/myusb# echo "image img.png is shown well".
image img.png is shown well.
root@am62xx-evm:/tmp/myusb#
root@am62xx-evm:/tmp/myusb# zcat /proc/config.gz | grep  BACKLIGH
CONFIG_BACKLIGHT_CLASS_DEVICE=y
# CONFIG_BACKLIGHT_KTD253 is not set
CONFIG_BACKLIGHT_PWM=m
# CONFIG_BACKLIGHT_QCOM_WLED is not set
# CONFIG_BACKLIGHT_ADP8860 is not set
# CONFIG_BACKLIGHT_ADP8870 is not set
# CONFIG_BACKLIGHT_LM3630A is not set
# CONFIG_BACKLIGHT_LM3639 is not set
CONFIG_BACKLIGHT_LP855X=m
# CONFIG_BACKLIGHT_GPIO is not set
# CONFIG_BACKLIGHT_LV5207LP is not set
# CONFIG_BACKLIGHT_BD6107 is not set
# CONFIG_BACKLIGHT_ARCXCNN is not set
# CONFIG_BACKLIGHT_LED is not set
# CONFIG_LEDS_TRIGGER_BACKLIGHT is not set
# CONFIG_CROS_KBD_LED_BACKLIGHT is not set
root@am62xx-evm:/tmp/myusb# zcat /proc/config.gz | grep  PANEL
# CONFIG_INPUT_IBM_PANEL is not set
CONFIG_DRM_PANEL=y
# CONFIG_DRM_PANEL_ABT_Y030XX067A is not set
# CONFIG_DRM_PANEL_ARM_VERSATILE is not set
# CONFIG_DRM_PANEL_ASUS_Z00T_TM5P5_NT35596 is not set
# CONFIG_DRM_PANEL_BOE_BF060Y8M_AJ0 is not set
# CONFIG_DRM_PANEL_BOE_HIMAX8279D is not set
CONFIG_DRM_PANEL_BOE_TV101WUM_NL6=m
# CONFIG_DRM_PANEL_DSI_CM is not set
CONFIG_DRM_PANEL_LVDS=m
CONFIG_DRM_PANEL_SIMPLE=m
CONFIG_DRM_PANEL_EDP=m
# CONFIG_DRM_PANEL_EBBG_FT8719 is not set
# CONFIG_DRM_PANEL_ELIDA_KD35T133 is not set
# CONFIG_DRM_PANEL_FEIXIN_K101_IM2BA02 is not set
# CONFIG_DRM_PANEL_FEIYANG_FY07024DI26A30D is not set
# CONFIG_DRM_PANEL_ILITEK_IL9322 is not set
# CONFIG_DRM_PANEL_ILITEK_ILI9341 is not set
# CONFIG_DRM_PANEL_ILITEK_ILI9881C is not set
# CONFIG_DRM_PANEL_INNOLUX_EJ030NA is not set
# CONFIG_DRM_PANEL_INNOLUX_P079ZCA is not set
# CONFIG_DRM_PANEL_JDI_LT070ME05000 is not set
# CONFIG_DRM_PANEL_JDI_R63452 is not set
# CONFIG_DRM_PANEL_KHADAS_TS050 is not set
# CONFIG_DRM_PANEL_KINGDISPLAY_KD097D04 is not set
# CONFIG_DRM_PANEL_LEADTEK_LTK050H3146W is not set
# CONFIG_DRM_PANEL_LEADTEK_LTK500HD1829 is not set
# CONFIG_DRM_PANEL_SAMSUNG_LD9040 is not set
# CONFIG_DRM_PANEL_LG_LB035Q02 is not set
# CONFIG_DRM_PANEL_LG_LG4573 is not set
# CONFIG_DRM_PANEL_NEC_NL8048HL11 is not set
# CONFIG_DRM_PANEL_NEWVISION_NV3052C is not set
# CONFIG_DRM_PANEL_NOVATEK_NT35510 is not set
# CONFIG_DRM_PANEL_NOVATEK_NT35560 is not set
# CONFIG_DRM_PANEL_NOVATEK_NT35950 is not set
# CONFIG_DRM_PANEL_NOVATEK_NT36672A is not set
# CONFIG_DRM_PANEL_NOVATEK_NT39016 is not set
CONFIG_DRM_PANEL_MANTIX_MLAF057WE51=m
# CONFIG_DRM_PANEL_OLIMEX_LCD_OLINUXINO is not set
# CONFIG_DRM_PANEL_ORISETECH_OTM8009A is not set
# CONFIG_DRM_PANEL_OSD_OSD101T2587_53TS is not set
# CONFIG_DRM_PANEL_PANASONIC_VVX10F034N00 is not set
# CONFIG_DRM_PANEL_RASPBERRYPI_TOUCHSCREEN is not set
CONFIG_DRM_PANEL_RAYDIUM_RM67191=m
# CONFIG_DRM_PANEL_RAYDIUM_RM68200 is not set
# CONFIG_DRM_PANEL_RONBO_RB070D30 is not set
# CONFIG_DRM_PANEL_SAMSUNG_ATNA33XC20 is not set
# CONFIG_DRM_PANEL_SAMSUNG_DB7430 is not set
# CONFIG_DRM_PANEL_SAMSUNG_S6D16D0 is not set
# CONFIG_DRM_PANEL_SAMSUNG_S6D27A1 is not set
# CONFIG_DRM_PANEL_SAMSUNG_S6E3HA2 is not set
# CONFIG_DRM_PANEL_SAMSUNG_S6E63J0X03 is not set
# CONFIG_DRM_PANEL_SAMSUNG_S6E63M0 is not set
# CONFIG_DRM_PANEL_SAMSUNG_S6E88A0_AMS452EF01 is not set
# CONFIG_DRM_PANEL_SAMSUNG_S6E8AA0 is not set
# CONFIG_DRM_PANEL_SAMSUNG_SOFEF00 is not set
# CONFIG_DRM_PANEL_SEIKO_43WVF1G is not set
# CONFIG_DRM_PANEL_SHARP_LQ101R1SX01 is not set
# CONFIG_DRM_PANEL_SHARP_LS037V7DW01 is not set
# CONFIG_DRM_PANEL_SHARP_LS043T1LE01 is not set
# CONFIG_DRM_PANEL_SHARP_LS060T1SX01 is not set
# CONFIG_DRM_PANEL_SITRONIX_ST7701 is not set
CONFIG_DRM_PANEL_SITRONIX_ST7703=m
# CONFIG_DRM_PANEL_SITRONIX_ST7789V is not set
# CONFIG_DRM_PANEL_SONY_ACX565AKM is not set
# CONFIG_DRM_PANEL_SONY_TULIP_TRULY_NT35521 is not set
# CONFIG_DRM_PANEL_TDO_TL070WSH30 is not set
# CONFIG_DRM_PANEL_TPO_TD028TTEC1 is not set
# CONFIG_DRM_PANEL_TPO_TD043MTEA1 is not set
# CONFIG_DRM_PANEL_TPO_TPG110 is not set
CONFIG_DRM_PANEL_TRULY_NT35597_WQXGA=m
# CONFIG_DRM_PANEL_VISIONOX_RM69299 is not set
# CONFIG_DRM_PANEL_WIDECHIPS_WS2401 is not set
# CONFIG_DRM_PANEL_XINPENG_XPP055C272 is not set
CONFIG_DRM_PANEL_BRIDGE=y
# CONFIG_DRM_PANEL_MIPI_DBI is not set
CONFIG_DRM_PANEL_ORIENTATION_QUIRKS=m
root@am62xx-evm:/tmp/myusb#

Thanks. 

Paul

  • Hi,

    Can you please check if following can help:

    1. 

    IMAGE_INSTALL:remove = "psplash"
    IMAGE_FEATURES:remove = "splash"

    Only remove splash, and let psplash remain.

    2. Remove splash by disabling this kconfig within yocto: CONFIG_SPL_VIDEO

  • Hello 

    Removing CONFIG_SPL_VIDEO in u-boot, it does not effect (also SPL related CONFIG_xx) as below.

    paul@43Server:~/300G_HDD/ti_am62x/build/arago-tmp-default-glibc/work/am62xx_evm_k3r5-oe-linux-gnueabi/u-boot-ti-staging/1_2023.04+gitAUTOINC+24098ea90d-r0.psdk3/git$ cat configs/am62x_evm_a53_defconfig | grep SPL
    CONFIG_SPL_GPIO=y
    CONFIG_SPL_LIBCOMMON_SUPPORT=y
    CONFIG_SPL_LIBGENERIC_SUPPORT=y
    CONFIG_SPL_DM_SPI=y
    CONFIG_SPL_TEXT_BASE=0x80080000
    CONFIG_SPL_MMC=y
    CONFIG_SPL_SERIAL=y
    CONFIG_SPL_DRIVERS_MISC=y
    CONFIG_SPL_STACK_R_ADDR=0x82000000
    CONFIG_SPL_SIZE_LIMIT=0x80000
    CONFIG_SPL_SIZE_LIMIT_PROVIDE_STACK=0x800
    CONFIG_SPL_FS_FAT=y
    CONFIG_SPL_LIBDISK_SUPPORT=y
    CONFIG_SPL_SPI_FLASH_SUPPORT=y
    CONFIG_SPL_SPI=y
    CONFIG_SPL_LOAD_FIT=y
    CONFIG_SPL_LOAD_FIT_ADDRESS=0x81000000
    CONFIG_SPL_MAX_SIZE=0x80000
    CONFIG_SPL_HAS_BSS_LINKER_SECTION=y
    CONFIG_SPL_BSS_START_ADDR=0x80c80000
    CONFIG_SPL_BSS_MAX_SIZE=0x80000
    CONFIG_SPL_SYS_REPORT_STACK_F_USAGE=y
    CONFIG_SPL_BOARD_INIT=y
    CONFIG_SPL_SYS_MALLOC_SIMPLE=y
    CONFIG_SPL_STACK_R=y
    CONFIG_SYS_SPL_MALLOC=y
    CONFIG_SPL_DMA=y
    CONFIG_SPL_ENV_SUPPORT=y
    CONFIG_SPL_ETH=y
    CONFIG_SPL_FS_LOAD_PAYLOAD_NAME="u-boot.img"
    CONFIG_SPL_I2C=y
    CONFIG_SPL_DM_MAILBOX=y
    CONFIG_SPL_DM_SPI_FLASH=y
    CONFIG_SPL_NET=y
    CONFIG_SPL_NET_VCI_STRING="AM62X U-Boot A53 SPL"
    CONFIG_SPL_POWER_DOMAIN=y
    CONFIG_SPL_RAM_SUPPORT=y
    CONFIG_SPL_RAM_DEVICE=y
    # CONFIG_SPL_SPI_FLASH_TINY is not set
    CONFIG_SPL_SPI_FLASH_SFDP_SUPPORT=y
    CONFIG_SPL_SPI_LOAD=y
    CONFIG_SPL_THERMAL=y
    CONFIG_SPL_USB_HOST=y
    CONFIG_SPL_USB_STORAGE=y
    CONFIG_SPL_USB_GADGET=y
    CONFIG_SPL_DFU=y
    CONFIG_SPL_YMODEM_SUPPORT=y
    CONFIG_SPL_BMP=y
    CONFIG_SPL_OF_CONTROL=y
    CONFIG_SPL_MULTI_DTB_FIT=y
    CONFIG_SPL_MULTI_DTB_FIT_NO_COMPRESSION=y
    CONFIG_SPL_DM=y
    CONFIG_SPL_DM_DEVICE_REMOVE=y
    CONFIG_SPL_DM_SEQ_ALIAS=y
    CONFIG_SPL_REGMAP=y
    CONFIG_SPL_SYSCON=y
    CONFIG_SPL_OF_TRANSLATE=y
    CONFIG_SPL_CLK=y
    CONFIG_SPL_DM_GPIO_LOOKUP_LABEL=y
    CONFIG_SPL_DM_PCA953X=y
    CONFIG_SPL_I2C_EEPROM=y
    CONFIG_SPL_MMC_IO_VOLTAGE=y
    CONFIG_SPL_MMC_UHS_SUPPORT=y
    CONFIG_SPL_MMC_HS200_SUPPORT=y
    CONFIG_SPL_MMC_SDHCI_ADMA=y
    CONFIG_SPL_PINCTRL=y
    CONFIG_SPL_DM_REGULATOR=y
    CONFIG_SPL_DM_REGULATOR_FIXED=y
    CONFIG_SPL_DM_REGULATOR_GPIO=y
    CONFIG_SPL_SYSRESET=y
    CONFIG_SPL_DM_USB_GADGET=y
    CONFIG_SPL_USB_DWC3_GENERIC=y
    CONFIG_SPL_USB_DWC3_AM62=y
    # CONFIG_SPL_VIDEO_TIDSS=y
    # CONFIG_SPL_VIDEO=y
    # CONFIG_SPLASH_SCREEN=y
    # CONFIG_SPL_SYS_WHITE_ON_BLACK=y
    # CONFIG_SPLASH_SCREEN_ALIGN=y
    # CONFIG_SPLASH_SOURCE=y
    # CONFIG_SPL_VIDEO_BMP_GZIP=y
    # CONFIG_SPL_BMP_24BPP=y
    # CONFIG_SPL_BMP_32BPP=y
    # CONFIG_SPL_GZIP=y
    paul@43Server:~/300G_HDD/ti_am62x/build/arago-tmp-default-glibc/work/am62xx_evm_k3r5-oe-linux-gnueabi/u-boot-ti-staging/1_2023.04+gitAUTOINC+24098ea90d-r0.psdk3/git$ cat configs/am62x_evm_a53_defconfig | grep VIDEO
    # CONFIG_VIDEO=y
    # CONFIG_VIDEO_LOGO=y
    # CONFIG_VIDEO_TIDSS=y
    # CONFIG_SPL_VIDEO_TIDSS=y
    # CONFIG_VIDEO_BMP_GZIP=y
    # CONFIG_SPL_VIDEO=y
    # CONFIG_SPL_VIDEO_BMP_GZIP=y
    paul@43Server:~/300G_HDD/ti_am62x/build/arago-tmp-default-glibc/work/am62xx_evm_k3r5-oe-linux-gnueabi/u-boot-ti-staging/1_2023.04+gitAUTOINC+24098ea90d-r0.psdk3/git$ cat configs/am62x_evm_a53_defconfig | grep LOGO
    # CONFIG_VIDEO_LOGO=y
    # CONFIG_HIDE_LOGO_VERSION=y
    paul@43Server:~/300G_HDD/ti_am62x/build/arago-tmp-default-glibc/work/am62xx_evm_k3r5-oe-linux-gnueabi/u-boot-ti-staging/1_2023.04+gitAUTOINC+24098ea90d-r0.psdk3/git$
    

  • Hi Paul, 

    Please try setting CONFIG_SPL_VIDEO=n instead of just commenting, you do not need to remove other SPL configs.
    I have tried this on my end, and it is able to remove the splash in u-boot proper stage.

  • Hello 

    We try to do the setting and made a clean build for our yocto SDK but still failed. May you help to check and clarify below?

    1. Below is our full patch of u-boot

    /usr/bin/psplash exists and it run when kernel starts.

    paul@44Server:~/300G_HDD/ti_am62x/build/arago-tmp-default-glibc/work/am62xx_evm_k3r5-oe-linux-gnueabi/u-boot-ti-staging/1_2023.04+gitAUTOINC+24098ea90d-r0.psdk3/git$ git status
    On branch ti-u-boot-2023.04
    Your branch is behind 'origin/ti-u-boot-2023.04' by 382 commits, and can be fast-forwarded.
      (use "git pull" to update your local branch)
    
    Changes not staged for commit:
      (use "git add <file>..." to update what will be committed)
      (use "git checkout -- <file>..." to discard changes in working directory)
    
            modified:   arch/arm/dts/k3-am62-main.dtsi
            modified:   arch/arm/dts/k3-am625-sk.dts
            modified:   arch/arm/dts/k3-am62x-sk-common-u-boot.dtsi
            modified:   configs/am62x_evm_a53_defconfig
            modified:   drivers/mmc/mmc.c
            modified:   include/configs/am62x_evm.h
    
    no changes added to commit (use "git add" and/or "git commit -a")
    paul@44Server:~/300G_HDD/ti_am62x/build/arago-tmp-default-glibc/work/am62xx_evm_k3r5-oe-linux-gnueabi/u-boot-ti-staging/1_2023.04+gitAUTOINC+24098ea90d-r0.psdk3/git$ grep -rn CONFIG_SPL_VIDEO
    drivers/Makefile:65:obj-$(CONFIG_SPL_VIDEO) +=video/
    drivers/pci/pci_rom.c:375:      if (IS_ENABLED(CONFIG_SPL_VIDEO) && spl_phase() > PHASE_SPL &&
    configs/am62x_evm_a53_defconfig:191:CONFIG_SPL_VIDEO_TIDSS=n
    configs/am62x_evm_a53_defconfig:195:CONFIG_SPL_VIDEO=n
    configs/am62x_evm_a53_defconfig:200:CONFIG_SPL_VIDEO_BMP_GZIP=n
    .pc/0314_42_uboot_add_quiet.patch/configs/am62x_evm_a53_defconfig:189:CONFIG_SPL_VIDEO_TIDSS=y
    .pc/0314_42_uboot_add_quiet.patch/configs/am62x_evm_a53_defconfig:193:CONFIG_SPL_VIDEO=y
    .pc/0314_42_uboot_add_quiet.patch/configs/am62x_evm_a53_defconfig:198:CONFIG_SPL_VIDEO_BMP_GZIP=y
    common/board_f.c:414:   if (IS_ENABLED(CONFIG_SPL_VIDEO) && spl_phase() > PHASE_SPL &&
    common/spl/spl.c:894:#if defined(CONFIG_SPL_VIDEO_REMOVE)
    paul@44Server:~/300G_HDD/ti_am62x/build/arago-tmp-default-glibc/work/am62xx_evm_k3r5-oe-linux-gnueabi/u-boot-ti-staging/1_2023.04+gitAUTOINC+24098ea90d-r0.psdk3/git$ git diff
    diff --git a/arch/arm/dts/k3-am62-main.dtsi b/arch/arm/dts/k3-am62-main.dtsi
    index bdfda77586e..839d342b894 100644
    --- a/arch/arm/dts/k3-am62-main.dtsi
    +++ b/arch/arm/dts/k3-am62-main.dtsi
    @@ -535,7 +535,7 @@
                    ti,itap-del-sel-sdr12 = <0xA>;
                    ti,itap-del-sel-sdr25 = <0x1>;
                    ti,clkbuf-sel = <0x7>;
    -               bus-width = <4>;
    +               bus-width = <1>;
                    status = "disabled";
            };
    
    diff --git a/arch/arm/dts/k3-am625-sk.dts b/arch/arm/dts/k3-am625-sk.dts
    index 859f038c376..9d8063efbe2 100644
    --- a/arch/arm/dts/k3-am625-sk.dts
    +++ b/arch/arm/dts/k3-am625-sk.dts
    @@ -141,7 +141,7 @@
                    regulator-boot-on;
                    enable-active-high;
                    vin-supply = <&vcc_3v3_sys>;
    -               gpio = <&exp1 3 GPIO_ACTIVE_HIGH>;
    +               //gpio = <&exp1 3 GPIO_ACTIVE_HIGH>;
            };
    
            vdd_sd_dv: regulator-4 {
    @@ -231,12 +231,12 @@
                    >;
            };
    
    -       main_i2c2_pins_default: main-i2c2-pins-default {
    -               pinctrl-single,pins = <
    -                       AM62X_IOPAD(0x0b0, PIN_INPUT_PULLUP, 1) /* (K22) GPMC0_CSn2.I2C2_SCL */
    -                       AM62X_IOPAD(0x0b4, PIN_INPUT_PULLUP, 1) /* (K24) GPMC0_CSn3.I2C2_SDA */
    -               >;
    -       };
    +       //main_i2c2_pins_default: main-i2c2-pins-default {
    +       //      pinctrl-single,pins = <
    +       //              AM62X_IOPAD(0x0b0, PIN_INPUT_PULLUP, 1) /* (K22) GPMC0_CSn2.I2C2_SCL */
    +       //              AM62X_IOPAD(0x0b4, PIN_INPUT_PULLUP, 1) /* (K24) GPMC0_CSn3.I2C2_SDA */
    +       //      >;
    +       //};
    
            main_mmc0_pins_default: main-mmc0-pins-default {
                    pinctrl-single,pins = <
    @@ -407,8 +407,8 @@
            status = "okay";
            pinctrl-names = "default";
            pinctrl-0 = <&main_i2c1_pins_default>;
    -       clock-frequency = <400000>;
    -
    +       clock-frequency = <100000>;
    +        /*
            exp1: gpio@22 {
                    compatible = "ti,tca6424";
                    reg = <0x22>;
    @@ -435,6 +435,7 @@
                    pinctrl-names = "default";
                    pinctrl-0 = <&main_gpio1_ioexp_intr_pins_default>;
            };
    +       */
    
     };
    
    @@ -455,6 +456,7 @@
            pinctrl-0 = <&main_mmc1_pins_default>;
            ti,driver-strength-ohm = <50>;
            disable-wp;
    +       sdhci-caps-mask = <0x00000007 0x00000000>; /* Limiting to SD SH speed mode */
     };
    
     &cpsw3g {
    diff --git a/arch/arm/dts/k3-am62x-sk-common-u-boot.dtsi b/arch/arm/dts/k3-am62x-sk-common-u-boot.dtsi
    index a408fd702a4..c35262023b8 100644
    --- a/arch/arm/dts/k3-am62x-sk-common-u-boot.dtsi
    +++ b/arch/arm/dts/k3-am62x-sk-common-u-boot.dtsi
    @@ -6,7 +6,8 @@
    
     / {
            chosen {
    -               stdout-path = "serial2:115200n8";
    +               stdout-path = "serial2:115200n8";
    +               bootargs = "console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 quiet";
                    tick-timer = &timer1;
            };
    
    @@ -224,9 +225,9 @@
            bootph-pre-ram;
     };
    
    -&exp1 {
    -       bootph-pre-ram;
    -};
    +//&exp1 {
    +//     bootph-pre-ram;
    +//};
    
     &vdd_mmc1 {
            bootph-pre-ram;
    diff --git a/configs/am62x_evm_a53_defconfig b/configs/am62x_evm_a53_defconfig
    index cc91adf496c..b2d2be27c1e 100644
    --- a/configs/am62x_evm_a53_defconfig
    +++ b/configs/am62x_evm_a53_defconfig
    @@ -32,6 +32,8 @@ CONFIG_SPL_LOAD_FIT=y
     CONFIG_SPL_LOAD_FIT_ADDRESS=0x81000000
     CONFIG_DISTRO_DEFAULTS=y
     CONFIG_BOOTCOMMAND="run envboot; run distro_bootcmd;"
    +CONFIG_BOOTDELAY=0
    +CONFIG_AUTOBOOT=y
     CONFIG_BOARD_LATE_INIT=y
     CONFIG_BLOBLIST=y
     CONFIG_BLOBLIST_ADDR=0x80D00000
    @@ -182,23 +184,23 @@ CONFIG_USB_GADGET_MANUFACTURER="Texas Instruments"
     CONFIG_USB_GADGET_VENDOR_NUM=0x0451
     CONFIG_USB_GADGET_PRODUCT_NUM=0x6165
     CONFIG_USB_GADGET_DOWNLOAD=y
    -CONFIG_VIDEO=y
    -# CONFIG_VIDEO_LOGO is not set
    -CONFIG_SYS_WHITE_ON_BLACK=y
    -CONFIG_VIDEO_TIDSS=y
    -CONFIG_SPL_VIDEO_TIDSS=y
    -CONFIG_VIDEO_BMP_GZIP=y
    -CONFIG_BMP_24BPP=y
    -CONFIG_BMP_32BPP=y
    -CONFIG_SPL_VIDEO=y
    -CONFIG_SPL_SPLASH_SCREEN=y
    -CONFIG_SPL_SYS_WHITE_ON_BLACK=y
    -CONFIG_SPL_SPLASH_SCREEN_ALIGN=y
    -CONFIG_SPL_SPLASH_SOURCE=y
    -CONFIG_SPL_VIDEO_BMP_GZIP=y
    -CONFIG_SPL_BMP_24BPP=y
    -CONFIG_SPL_BMP_32BPP=y
    -CONFIG_SPL_HIDE_LOGO_VERSION=y
    +CONFIG_VIDEO=n
    +CONFIG_VIDEO_LOGO=n
    +CONFIG_SYS_WHITE_ON_BLACK=n
    + CONFIG_VIDEO_TIDSS=n
    +CONFIG_SPL_VIDEO_TIDSS=n
    +CONFIG_VIDEO_BMP_GZIP=n
    +CONFIG_BMP_24BPP=n
    +CONFIG_BMP_32BPP=n
    +CONFIG_SPL_VIDEO=n
    +CONFIG_SPL_SPLASH_SCREEN=n
    +CONFIG_SPL_SYS_WHITE_ON_BLACK=n
    +CONFIG_SPL_SPLASH_SCREEN_ALIGN=n
    +CONFIG_SPL_SPLASH_SOURCE=n
    +CONFIG_SPL_VIDEO_BMP_GZIP=n
    +CONFIG_SPL_BMP_24BPP=n
    +CONFIG_SPL_BMP_32BPP=n
    +CONFIG_SPL_HIDE_LOGO_VERSION=n
     CONFIG_FS_FAT_MAX_CLUSTSIZE=16384
    -CONFIG_SPL_GZIP=y
    -CONFIG_OF_LIBFDT_OVERLAY=y
    +CONFIG_SPL_GZIP=n
    +CONFIG_OF_LIBFDT_OVERLAY=n
    diff --git a/drivers/mmc/mmc.c b/drivers/mmc/mmc.c
    index dde251c87bc..d382f6a443f 100644
    --- a/drivers/mmc/mmc.c
    +++ b/drivers/mmc/mmc.c
    @@ -2797,7 +2797,7 @@ static int mmc_power_cycle(struct mmc *mmc)
             * SD spec recommends at least 1ms of delay. Let's wait for 2ms
             * to be on the safer side.
             */
    -       udelay(2000);
    +       udelay(4000);
            return mmc_power_on(mmc);
     }
    
    diff --git a/include/configs/am62x_evm.h b/include/configs/am62x_evm.h
    index bdf0bec0981..c7aeeb3e89c 100644
    --- a/include/configs/am62x_evm.h
    +++ b/include/configs/am62x_evm.h
    @@ -33,4 +33,7 @@
     #define CFG_SYS_NAND_ECCBYTES        14
     /*-- end NAND config --*/
    
    +#define CONFIG_BOOTDELAY 0
    +#define CONFIG_AUTOBOOT
    +
     #endif /* __CONFIG_AM625_EVM_H */
    (END)
    

    2. psplash as below, it seems it is a part of kernel process (ref: log1_firstboot.txt), not u-boot?

    【68.316224] PVR_K: 213: RGX Device registered with BVNC 33.15.11.3
    Starting Start psplash boot splash screen...
    [ OK ] Started Start psplash boot splash screen.
    [ OK ] Started Start psplash-syst…progress communication helper.

    psplash boot logo and progress bar:

    3. We write our system image using balenaEthcher to a Micro SD card and boot from it.

    The first boot (as in  log1_firstboot.txt) we could see the psplash boot log and progress bar are shwon on LCD but in the next system boot,  it does not show. Please refer to log2_secondboot.txt below. 

    Our goal is to remove this psplash boot logo and progress bar, or it is ok to keep it but it must show in every reboot; not just only the first boot. 

    Please suggest. Thanks.

    log2_secondboot.txt

  • Hi,

    Please checkout the following file located in the Processor SDK:
    <SDK>/board-support/<ti-u-boot directory>/configs/am62x_evm_prune_splashscreen.config

    This will help disable the TI Logo, psplash along with progress bar.

    Do not forget to remove the psplash service from Yocto as you were doing earlier.