Tool/software:
Using the AWB plugin of TI's DCC tuning tool, a DCC file was generated and applied to the J721E evaluation board; however,
no changes were observed in the camera's video output.
The DCC file has been copied to the following folder on the SD card:
/roofs/opt/vision_apps/dcc/IMX390-UB953-DISCOVERY/wdr
What factors could be responsible for the changes not taking effect?
Additionally, the input image settings of the DCC tuning tool at that time are as follows: